This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

adc12_low_power_peripheral

Overview

The ADC Low Power Demo project is a demonstration program that uses the KSDK software. The microcontroller is set to a very low power stop (VLPS) mode, and every 500 ms an interrupt wakes up the ADC module and takes the current temperature sensor value of the microcontroller. While the temperature remains within boundaries, both LEDs are on. If the temperature is higher or lower than average, a led comes off. This demo provides an example to show how ADC works during a VLPS mode and a simple debugging.

Supported Boards