This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

adc16_low_power_async_edma

Overview

The ADC Low Power Async DMA demo application demonstrates the usage of the ADC and DMA peripheral while in a low power mode. The microcontroller is first set to very low power stop (VLPS) mode. Every 100 ms, low power timer trigger the ADC module convert value on ADC channel. After 16 times(1,6s) the DMA transfer finish interrupt wake up the CPU to process sampled data, print result to user and toggle LED.

Supported Boards