This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

adc16_low_power

Overview

The ADC Low Power demo application demonstrates the usage of the ADC peripheral while in a low power mode. The microcontroller is first set to very low power stop (VLPS) mode. Every 500 ms, an interrupt wakes up the ADC module and reads the current temperature of the microcontroller. While the temperature remains within boundaries, both LEDs are on. If the core temperature is higher or lower than average, the LEDs change state respectively.

Supported Boards