dev_audio_generator
Overview
The USB Audio Generator application is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as a recording device and users can record the sound from this device via the “Sound Recorder” in the Windows Accessories.
System Requirement
Hardware requirements
Mini/micro USB cable
USB A to micro AB cable
Hardware (Tower System/base module) for a specific device
Personal Computer(PC)
Software requirements
The project files for lite version examples are in the following path:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_audio_generator_lite/ / .
For non-lite version examples, the path is:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_audio_generator/ / .
The
is Bare Metal or FreeRTOS OS.
Getting Started
Hardware Settings
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example
Connect a USB cable between the PC host and the debugger USB port on the board to provide power supply (the example is self-powered).
Download the program to the target board via IDE.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Connect a USB cable between the PC host and the USB device port on the board.
Demo start log is printed.

For detailed instructions, see the appropriate board User’s Guide.
Run the example in Windows
The mentioned steps can be different for Recording settings as per different Windows OS version.
A USB AUDIO DEMO device shows up as enumerated in the Device Manager.

Right click on the sound control icon of the Start bar (close to the clock) and select the “Recording devices” option.

In the pop-up window, select the “Microphone” device with the description “USB Audio Device” and click on the “Properties” button.

On the new window, go to the “Levels” tab, and move the slide until 100%. Click “OK”.

Ensure that the selected “Microphone-USB AUDIO DEMO” is display as Default device if no other microphone device supported by the Windows system. If it’s not mention as default device then click on the “Set default” option to make “Microphone-USB AUDIO DEMO” as a default device.

Open the “Sound Recorder” application and record audio for about 5-10 seconds.
After recording, open the recorder file with any media player and verify it by listening on the speaker of Laptop/PC.
note
On Aruba which has DMIC module, please speaker to the DMIC when recording, the recorder file is the sound which is recorded by DMIC.
When connected to MacBook®, change the PCM format from (0x02,0x00,) to (0x01,0x00, ) in
g_config_descriptor[CONFIG_DESC_SIZE] in the usb_descriptor.c. Otherwise, it can’t be enumerated and noise is present when recording with the QuickTime® player because the sampling frequency and bit resolution do not match.USB audio class 2.0 is enabled by default.
When device functionality is changed, such as USB auido class 2.0 or UAC 5.1, please uninstall the previous PC driver to make sure the device with changed functionality can run normally.
If you’re having audio problems on Windows 10 for recorder, please disable signal enhancement as the following if it is enabled and have a try again.

Supported Boards
EVKB-IMXRT1050
MIMXRT1060-EVKB
MIMXRT1170-EVKB
MIMXRT1060-EVKC
EVK-MIMXRT1010
EVK-MIMXRT1015
EVK-MIMXRT1020
MIMXRT1024-EVK
MIMXRT1040-EVK
EVK-MIMXRT1064
MIMXRT1160-EVK
MIMXRT1180-EVK
EVK-MIMXRT685
FRDM-K22F
FRDM-K32L2B
FRDM-K32L3A6
FRDM-MCXA153
FRDM-MCXA156
FRDM-MCXA276
FRDM-MCXC242
FRDM-MCXC444
FRDM-MCXN236
FRDM-MCXN947
FRDM-RW612
LPCXpresso54628
LPCXpresso54S018
LPCXpresso54S018M
LPCXpresso55S28
LPCXpresso55S36
LPCXpresso55S69
MCX-N9XX-EVK
MIMXRT700-EVK
RD-RW612-BGA