dev_hid_mouse
Overview
The USB HID mouse application is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as a mouse. Users can see the mouse arrow moving on the PC screen according in a rectangular fashion.
System Requirements
Hardware requirements
Mini/micro USB cable
USB A to micro AB cable
Hardware (Tower module/base board, and so on) for a specific device
Personal Computer (PC)
Software requirements
The project files are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_hid_mouse/ / .
For lite version, the project files are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_hid_mouse_lite/ / .
The
is Bare Metal or FreeRTOS OS.
Getting Started
Hardware Settings
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example
Download the program to the target board.
Connect the target board to the external power source (the example is self-powered).
Power off the target board. Then power on again.
Connect a USB cable between the PC and the USB device port of the board.
For detailed instructions, see the appropriate board User’s Guide.
Run the example
Plug-in the device, which is running HID mouse example, into the PC. A HID-compliant mouse is enumerated in the Device Manager.
The mouse arrow is moving on PC screen in the rectangular rotation.
*/
Supported Boards
FRDM-K22F
FRDM-K32L3A6
FRDM-MCXA153
FRDM-MCXA156
FRDM-MCXA276
FRDM-MCXN236
LPCXpresso51U68
LPCXpresso54628
LPCXpresso54S018
LPCXpresso54S018M
LPCXpresso55S28
LPCXpresso55S36
LPCXpresso55S69