This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

usb_pd_charger_battery

Overview

The PD charger + battery example is a simple demonstration based on the MCUXpresso SDK PD stack.
The application simulate battery product (for example: laptop), it prints the battery percent continually.
The demo works as DRP. When connect, the board can be source or sink.

System Requirement

Hardware requirements

  • One or two Type-C shield board

  • One or two 9V DC power suppliers

  • Type-C Cable

  • One or two hardwares (Tower module/base board, and so on) for a specific device, for example: lpcxpresso54114 board

  • Personal Computer

Software requirements

  • The project files are in:
    <MCUXpresso_SDK_Install>/boards//usb_examples/usb_pd_charger_battery//.

The is Bare Metal or FreeRTOS OS.

  • Terminal tool.

Getting Started

Hardware Settings


For detailed instructions, see the appropriate board User’s Guide.

Set the hardware jumpers (Tower system/base module) to default settings.

Prepare the example

  1. Download the program to the target board.

  2. Power on Type-C shield board then power on development board.

Run the example

  1. Connect the board to one charger or another shield board + development board (download this program too) with Type-C cable.

  2. Connect the OpenSDA USB port to the PC and open terminal.

  3. If running as source after connect.

    • If battery is (30%, 100%]: source caps are high power (5V/9V).

    • If battery is (0%, 30%]: source caps are low power (only 5V).

    • If partner request power role swap: accept.

    • prefer to work as sink.

      • get partner source cap, and judge whether to swap (if partner is external powered and satisfy self request).

        • if get partner source cap fail, retry one more time.

        • if can swap, then start power role swap.

        • if cannot swap or get source cap fail. still work as source.

      • do power role swap.

        • if fail, re-try one more time, if still fail, still work as source.

        • if success, please reference to sink description.

    • battery will decrease (if battery decrease to [0%, 20%]):

      • get partner source cap, and judge whether to swap (source cap satisfy self request).

        • if get partner source cap fail, retry one more time.

        • if can swap, then start power role swap.

        • if cannot swap or get source cap fail, send low power source caps.

      • do power role swap.

        • if fail, re-try one more time, if still fail send low power source caps.

        • if success, please reference to sink description.

      • if swap fail, after send low power source caps to trigger source capabilities change.

        • retry swap with interval 10s.

      • if battery decrease to 5%:

        • stop provide vbus.

        • set Try.SNK

  4. Running as sink after connect.

    • when connect:

      • if battery is less than 100%: request high power (9V).

      • if battery is 100%: request low power (5V).

    • when battery increase to 100%, request low power (5V).

    • If partner request power role swap

      • if battery is (30%, 100%]: accept.

      • if battery is [0%, 30%]: reject.

    • when battery increase to (30%, 100%]:

      • update self source caps as high power.

Supported Boards

  • LPCXpresso55S69