host_audio_speaker
Overview
The Host Audio example supports the audio speaker device.
The application prints the audio speaker information when the USB speaker device is attached.
System Requirement
Hardware requirements
Mini/micro USB cable
USB A to micro AB cable
Hardware (Tower module/base board, and so on) for a specific device
Personal Computer
Software requirements
The project files are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_host_audio_speaker/ / .
The
is Bare Metal or FreeRTOS OS.
Getting Started
Hardware Settings
For detailed instructions, see the appropriate board User’s Guide.
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example
Download the program to the target board.
Power off the target board, and then power on again or press the reset button on your board.
Connect the USB audio speaker devices to the board.
For detailed instructions, see the appropriate board User’s Guide.
Run the example
Connect the board UART to the PC and open the COM port in a terminal tool.
Plug in the USB audio speaker device to the board and attach the information print out in the terminal.
The USB audio speaker information prints in the terminal when USB speaker device is attached.
After the USB speaker device is plugged into the host, the USB application automatically transfers the audio data to the USB audio speaker device and the sound can be heard from the audio speaker device.
The following image shows how to attach a USB audio speaker device.
Known issue for FreeRTOS Host Audio Speaker Example
The FreeRTOS OS version example attach/detached printed debug message displays jumbled instructions to perform the hot plug test many times. Because the example handles different interfaces in different tasks, one task printing the debug message may be broken by another task and cause the debug message to be jumbled.
A noise occurs when a song is playing on some boards with The FreeRTOS version example. Because there is no software timer to ensure that one ISO transfer is sent per one SOF timer without the hardware PIT timer enablement, the issue also is effected by the KHCI hardware SOF Threshold feature. The host sends less audio data to the device after a while. As a result, the buffer on the device side experiences an underrun error. If the device doesn’t have an appropriate method to deal with it, some noise will occur.
Supported Boards
EVKB-IMXRT1050
MIMXRT1060-EVKB
MIMXRT1170-EVKB
MIMXRT1060-EVKC
EVK-MIMXRT1010
EVK-MIMXRT1015
EVK-MIMXRT1020
MIMXRT1024-EVK
MIMXRT1040-EVK
EVK-MIMXRT1064
MIMXRT1160-EVK
MIMXRT1180-EVK
EVK-MIMXRT595
EVK-MIMXRT685
FRDM-MCXN236
FRDM-RW612
LPCXpresso55S36
MIMXRT685-AUD-EVK
MIMXRT700-EVK
RD-RW612-BGA