Hardware Rework Guide for MIMXRT595-EVK and AW-AM510MA

This section is a brief hardware rework guidance of the EdgeFast Bluetooth PAL on the NXP i.MX MIMXRT595-EVK board and AW-AM510MA. The AW-AM510MA user guide is available here. The hardware rework has one part:

  • Debug console serial rework

Hardware rework

Debug console serial rework:

No special rework is required, except the following to enable the debug port.

  • Connect J39 with external power.

  • Connect JP4 1-2.

  • J27 1 — TX of USB to serial converter.

  • J27 2 — RX of USB to serial converter.

Parent topic:Hardware Rework Guide for MIMXRT595-EVK and AW-AM510MA