Hardware Rework Guide for MIMXRT685-EVK and Murata uSD-M.2 Adapter

This section is a brief hardware rework guidance of the EdgeFast Bluetooth PAL on the NXP i.MX MIMXRT685-EVK board and the Murata uSD-M.2 adapter. For details on the Murata uSD-M.2 Adapter, see Murata’s uSD-M.2 webpage.

The hardware rework has one part:

  • HCI UART rework

Hardware rework

HCI UART rework :

  • JP12 2-3

  • Connect the pins of two boards as the following table using jumper cables included in Murata’s uSD-M.2 Adapter kit.

Pin name

uSD-M.2 adapter pin

i.MX RT685 pin

Pin name of RT685

GPIO name of RT685

BT_UART_TXD_HOST

J9 (pin 1)

J27 (pin 1)

USART4_RXD

FC4_RXD_SDA_MOSI_DATA

BT_UART_RXD_HOST

J9 (pin 2)

J27 (pin 2)

USART4_TXD

FC4_TXD_SCL_MISO_WS

BT_UART_RTS_HOST

J8 (pin 3)

J47 (pin 9)

USART4_CTS

FC4_CTS_SDA_SSEL0

BT_UART_CTS_HOST

J8 (pin 4)

J27 (pin 5)

USART4_RTS

FC4_RTS_SCL_SSEL1

Murata uSD-M.2 jumper settings:

  • Both J12 and J13 = 1-2 (WLAN-SDIO = 1.8 V; and BT-UART and WLAN/BT-CTRL = 3.3 V)

  • J1 = 2-3 (3.3 V from uSD connector)

Parent topic:Hardware Rework Guide for MIMXRT685-EVK and Murata uSD-M.2 Adapter