Organization of this manual
This manual is divided into four parts:
Part I: Concept and Operational Information consists of six chapters:
Chapter 1: Preface provides an overview of the document contents, conventions, support resources, and compatibility information.
Chapter 2: ZigBee overview introduces the ZigBee 3.0 wireless network protocol.
Chapter 3: ZigBee PRO architecture and operation describes the architecture and features of ZigBee 3.0.
Chapter 4: ZigBee Stack Software introduces the NXP ZigBee PRO stack software.
Chapter 5: Application development overview provides an overview of the ZigBee 3.0 application development environment and process.
Chapter 6: Application coding with ZigBee PRO APIs describes how to perform common wireless network operations using the functions of the NXP ZigBee 3.0 APIs.
Part II: Reference Information consists of six chapters:
Chapter 7: ZigBee Device Objects (ZDO) API details the functions and associated resources of the ZigBee Device Objects (ZDO) API.
Chapter 8: Application Framework (AF) API details the functions and associated resources of the Application Framework (AF) API.
Chapter 9: ZigBee Device Profile (ZDP) API details the functions and associated resources of the ZigBee Device Profile (ZDP) API.
Chapter 10: General ZPS Resources details the general functions and associated resources provided with the NXP ZigBee PRO stack.
Chapter 11: Event and Status Codes details the stack events and the return/status codes used by the ZigBee PRO APIs.
Chapter 12: ZigBee network parameters details the ZigBee network parameters.
Part III: Network Configuration consists of one chapter:
Chapter 13: ZPS Configuration Editor describes how to use the ZPS Configuration Editor.
Part IV: contains various ancillary information that include the following:
Appendix A: Appendix A: Handling stack events: a description of the handling of ZigBee PRO stack events.
Appendix B: Appendix B: Application design notes: a set of design application notes.
Appendix C: Appendix C: Implementation of frame counters: a description of frame counters.
Appendix D: Appendix D: storing applications in device flash memory: a description of application storage in Flash memory.
Appendix E: a glossary of terms used in ZigBee 3.0 networks.
Appendix F: Revision History for the document.
Parent topic:Preface