MCUXpresso SDK Release Notes#
Overview#
The MCUXpresso SDK is a comprehensive software enablement package designed to simplify and accelerate application development with Arm Cortex-M-based devices from NXP, including its general purpose, crossover and Bluetooth-enabled MCUs. MCUXpresso SW and Tools for DSC further extends the SDK support to current 32-bit Digital Signal Controllers. The MCUXpresso SDK includes production-grade software with integrated RTOS (optional), integrated enabling software technologies (stacks and middleware), reference software, and more.
In addition to working seamlessly with the MCUXpresso IDE, the MCUXpresso SDK also supports and provides example projects for various toolchains. The Development tools chapter in the associated Release Notes provides details about toolchain support for your board. Support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
Underscoring our commitment to high quality, the MCUXpresso SDK is MISRA compliant and checked with Coverity static analysis tools. For details on MCUXpresso SDK, see MCUXpresso-SDK: Software Development Kit for MCUXpresso.
MCUXpresso SDK#
As part of the MCUXpresso software and tools, MCUXpresso SDK is the evolution of Kinetis SDK, includes support for LPC, DSC,PN76, and i.MX System-on-Chip (SoC). The same drivers, APIs, and middleware are still available with support for Kinetis, LPC, DSC, and i.MX silicon. The MCUXpresso SDK adds support for the MCUXpresso IDE, an Eclipse-based toolchain that works with all MCUXpresso SDKs. Easily import your SDK into the new toolchain to access to all of the available components, examples, and demos for your target silicon. In addition to the MCUXpresso IDE, support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
In order to maintain compatibility with legacy Freescale code, the filenames and source code in MCUXpresso SDK containing the legacy Freescale prefix FSL has been left as is. The FSL prefix has been redefined as the NXP Foundation Software Library.
Development tools#
The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.
IAR 9.70.2 does not yet support the MIMXRT1186 device. If you need to build your project using IAR 9.70.2, you must install the corresponding IAR patch.
IAR patch is distributed via iar_segger_support_patch_rt1186.
Segger J‑Link v9.10 has been verified to support MIMXRT1186 devices, and using J‑Link version 9.10 or later is strongly recommended.
MCUXpresso IDE, Rev. 25.06.xx
IAR Embedded Workbench for Arm, version is 9.70.4
Keil MDK, version is 5.43a
MCUXpresso for VS Code v26.06
GCC Arm Embedded Toolchain 14.2.x
Supported development systems#
This release supports board and devices listed in following table. The board and devices in bold were tested in this release.
Development boards |
MCU devices |
|---|---|
FRDM-IMXRT1186 |
MIMXRT1186CVJ8C, MIMXRT1186XVJ8C, MIMXRT1185CVJ8C, |
MCUXpresso SDK release package#
The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.
Device support#
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.
Board support#
The boards folder provides the board-specific demo applications, driver examples, and middleware examples.
Demo application and other examples#
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
RTOS#
FreeRTOS#
Real-time operating system for microcontrollers from Amazon
Middleware#
CMSIS DSP Library#
The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.
MCU Boot#
MCU Boot (formerly KBOOT) NXP/Freescale proprietary loader
Ethermind BT/BLE Stack#
nxp_bt_ble_stack
coreHTTP#
coreHTTP
USB Host, Device, OTG Stack#
See the MCUXpresso SDK USB Stack User’s Guide (document MCUXSDKUSBSUG) for more information.
Peripheral devices tested with USB Host stack#
Table 1 provides a list of USB devices tested with the USB Host stack.
Device type |
Device |
|---|---|
USB HUB |
BELKIN F5U233BELKIN F5U304BELKIN F5U307BELKIN F4U040UNITEK Y-2151Z-TEK ZK032AHYUNDAI HY-HB608 |
USB flash drive |
ADATA C008 32 GBADATA S102 8 GADATA S102 16 GVerbatim STORE N GO USB Device 8 GKingston DataTraveler DT101 G2SanDisk Cruzer Blade 8 GBUnisplendour 1 GImation 2 GBV-mux 2 GBSanmina-SCI 128 MCorporate Express 1 GTOSHIBA THUHYBS-008G 8 GTranscend JF700 8 GNetac U903 16 GSSK SFD205 8 GBRex 4 GBSAMSUNG USB3.0 16GB |
USB card reader/adapter |
SSK TF adapterKawau Multi Card ReaderKawau TF adapterKawau SDHC cardUSB Mouse DELL MS111-PDELL M066U0ADELL MUAVDEL8TARGUS AMU76APDELL MD56U0DELL MS111-TRAPOO M110 |
USB Keyboard |
DELL SK8135DELL SK8115 |
TinyCBOR#
Concise Binary Object Representation (CBOR) Library
Simple Open EtherCAT Master#
Simple Open EtherCAT Master (SOEM) is an open source EtherCAT master stack that is used to write custom EtherCAT Master applications. For more information on how to use SOEM, see the Getting Started with MCUXpresso SDK for SOEM document.
SDMMC stack#
The SDMMC software is integrated with MCUXpresso SDK to support SD/MMC/SDIO standard specification. This also includes a host adapter layer for bare-metal/RTOS applications.
PKCS#11#
The PKCS#11 standard specifies an application programming interface (API), called “Cryptoki,” for devices that hold cryptographic information and perform cryptographic functions. Cryptoki follows a simple object based approach, addressing the goals of technology independence (any kind of device) and resource sharing (multiple applications accessing multiple devices), presenting to applications a common, logical view of the device called a “cryptographic token”.
Multicore#
Multicore Software Development Kit
Motor Control Software (ACIM, BLDC, PMSM)#
Motor control examples.
MCU Boot#
Open source MCU Bootloader.
mbedTLS#
mbedtls SSL/TLS library v3.x
mbedTLS#
mbedtls SSL/TLS library v2.x
lwIP#
The lwIP TCP/IP stack is pre-integrated with MCUXpresso SDK and runs on top of the MCUXpresso SDK Ethernet driver with Ethernet-capable devices/boards.
For details, see the lwIP TCPIP Stack and MCUXpresso SDK Integration User’s Guide (document MCUXSDKLWIPUG).
lwIP is a small independent implementation of the TCP/IP protocol suite.
eIQ#
The package contains several example applications using the eIQ TensorFlow Lite for Microcontrollers library.
eIQ machine learning SDK containing:
Arm CMSIS-NN library (neural network kernels optimized for Cortex-M cores)
Inference engines:
TensorFlow Lite Micro
DeepView RT
Example code for TensorFlow Lite Micro, Glow, and DeepView RT
llhttp#
HTTP parser llhttp
LittleFS#
LittleFS filesystem stack
FreeMASTER#
FreeMASTER communication driver for 32-bit platforms.
File systemFatfs#
The FatFs file system is integrated with the MCUXpresso SDK and can be used to access either the SD card or the USB memory stick when the SD card driver or the USB Mass Storage Device class implementation is used.
NAND Flash Management Stack#
NAND Flash Management Stack
NXP PSA CRYPTO DRIVER#
PSA crypto driver for crypto library integration via driver wrappers
ELE Crypto#
Crypto functionality provided Edgelock Core
Release contents#
Provides an overview of the MCUXpresso SDK release package contents and locations.
Deliverable |
Location |
|---|---|
Boards |
INSTALL_DIR/boards |
Demo Applications |
INSTALL_DIR/boards/<board_name>/demo_apps |
Driver Examples |
INSTALL_DIR/boards/<board_name>/driver_examples |
eIQ examples |
INSTALL_DIR/boards/<board_name>/eiq_examples |
Board Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/boards/<board_name>/project_template |
Driver, SoC header files, extension header files and feature header files, utilities |
INSTALL_DIR/devices/<device_name> |
CMSIS drivers |
INSTALL_DIR/devices/<device_name>/cmsis_drivers |
Peripheral drivers |
INSTALL_DIR/devices/<device_name>/drivers |
Toolchain linker files and startup code |
INSTALL_DIR/devices/<device_name>/<toolchain_name> |
Utilities such as debug console |
INSTALL_DIR/devices/<device_name>/utilities |
Device Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/devices/<device_name>/project_template |
CMSIS Arm Cortex-M header files, DSP library source |
INSTALL_DIR/CMSIS |
Components and board device drivers |
INSTALL_DIR/components |
RTOS |
INSTALL_DIR/rtos |
Release Notes, Getting Started Document and other documents |
INSTALL_DIR/docs |
Tools such as shared cmake files |
INSTALL_DIR/tools |
Middleware |
INSTALL_DIR/middleware |
Known Issues#
This section lists the known issues, limitations, and/or workarounds.
[config_tool][importProject.board_FRDM-IMXRT1186] No processor detected in IAR project#
Summary#
Import issues of importProject.board_FRDM-IMXRT1186: No processor detected in IAR project