dev_phdc_weighscale_lite_bm#
Overview#
The USB PHDC WeighScale application is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as a weight scale device and the HealthLink software is used to interact with this device to simulate the personal weight scale data, such as body mass and body mass index.
System Requirement#
Hardware requirements#
Mini/micro USB cable
USB A to micro AB cable
Hardware (Tower module/base board, and so on) for a specific device
Personal Computer (PC)
Software requirements#
The project files for lite version example are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_phdc_weighscale_lite/ / .
For non-lite version example, the path is:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_phdc_weighscale/ / .
The
is Bare Metal or FreeRTOS OS.
The HealthLink software installed in Personal Computer(PC)
Getting Started#
Hardware Settings#
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example#
Download the program to the target board.
Connect the target board to the external power source (the example is self-powered).
Power off the target board. And then power on again.
Connect a USB cable between the Host and the USB device port of the board.
For detailed instructions, see the appropriate board User’s Guide. this example could be tested with the “usb_host_phdc_manager” example in pairs.
Run the example in Windows#
Prepare one board that run usb_host_phdc_manager example work as host.
Prepare one target board which is running the “usb_device_phdc_weighscale” example to work as device, plug into the host . The state of the device and the received data will show up on host phdc serial terminal.Open the host serial terminal, the data received from device phdc will be printed as following.

*/
Supported Boards#
MIMXRT1170-EVKB
FRDM-MCXC444
FRDM-K22F
LPCXpresso55S69
EVK-MIMXRT1064
FRDM-MCXA153
MIMXRT685-AUD-EVK
LPCXpresso51U68
LPCXpresso54S018
LPCXpresso55S16
FRDM-K32L2B
LPCXpresso54S018M
MIMXRT1060-EVKB
EVK-MIMXRT1010
MIMXRT1040-EVK
FRDM-MCXN947
MIMXRT1024-EVK
LPCXpresso55S28
LPCXpresso54628
LPCXpresso55S36
MCX-N5XX-EVK
MIMXRT1060-EVKC
MIMXRT1160-EVK
MIMXRT1180-EVK
FRDM-K32L2A4S
EVK-MIMXRT1020
MIMXRT700-EVK
FRDM-IMXRT700
FRDM-MCXA156
EVK-MIMXRT595
EVK-MIMXRT685
FRDM-MCXC242
MCX-N9XX-EVK
EVKB-IMXRT1050
RD-RW612-BGA
FRDM-K32L3A6
EVK-MIMXRT1015
FRDM-MCXN236
FRDM-RW612