itrc#
Overview#
The ITRC Example project is a demonstration program that uses the MCUX SDK software to set up Intrusion and Tamper Response Controller. Then tests the expected behaviour.
Running the demo#
When the demo runs successfully, the terminal displays similar information like the following:
ITRC Peripheral Driver Example
Pass: No Event/Action triggered in STATUS after Init
Enable ITRC IRQ Action response to SW Event 0
Trigger SW Event 0
ITRC IRQ Reached!
ITRC STATUS: SW Event 0 occured!
Clear ITRC IRQ and SW Event 0 STATUS
Disable ITRC IRQ Action response to SW Event 0
Trigger SW Event 0
Pass: No Action triggered
End of example