MCUXpresso SDK Documentation

tflm_label_image#

Overview#

This example demonstrates a TensorFlow Lite Micro model for image classification on MCUs. It is based on the TensorFlow Lite Label Image example adjusted to run on MCUs.

In this example, a static test image (“stopwatch”) is evaluated for classification into one of 1000 ImageNet classes.

Key Features#

  • Model Architecture: Mobilenet V1 0.25 128 quantized convolutional neural network

  • Input: 3-channel color image (128×128 pixels)

  • Output: Classification into 1000 classes

  • Detection Threshold: 23%

  • Neutron Software Version: MCU SDK 26.06.00 comes with a default Neutron Software Version of 3.1.1

Network Structure#

The neural network is based on Mobilenet V1 architecture:

  • Depthwise separable convolutions for efficient computation

  • Quantized model optimized for MCU deployment

Model Origin#


Project Files#

File

Description

main.cpp

Example main function

stopwatch.bmp

Static test image (source: Wikimedia Commons)

image_data.h

Image converted to C array (RGB values)

labels.h

Names of object classes

timer.c

Timer source code

image/*

Image capture and pre-processing code

video/*

Camera and display handling

get_top_n.cpp

Top-N results retrieval

model.cpp

Model initialization and inference

model_mobilenet_ops.cpp

Model operations registration

output_postproc.cpp

Output post-processing

model_data.h

Model data from .tflite converted to C array

Project Structure in MCU SDK#

Only primary files are listed here:

Path_to_MCUSDK/mcuxsdk/examples/
├── eiq_examples/
│   ├── common/                # Common utilities for eIQ examples
│   │   ├── image/*            # Image capture and pre-processing module
│   │   └── video/*            # Camera and display handling module
│   └── tflm_cifar10/          
│       ├── CMakeLists.txt
│       ├── image_data.h
│       ├── labels.h
│       ├── labels.txt
│       ├── main.cpp
│       ├── readme.md
│       └── stopwatch.bmp
└── _boards/
    └── <board_name>/
        └── eiq_examples/
            └── tflm_label_image/
                ├── example_board_readme.md
                └── pcq_npu    # NPU version of the model files
                    ├── mobilenet_v1_0.25_128_quant_int8_npu.tflite
                    ├── model_mobilenet_ops_npu.cpp
                    └── model_data.h

(For the boards without NPU hardware, the CPU version of the model files is located in the pcq/ folder.)

Project Structure in IDE#

(1) Project Structure in MCUXpresso IDE

Only primary files are listed here:

.
├── eiq
│   ├── neutron       # Neutron-Software files
│   │   ├── common
│   │   │   └── include
│   │   │       └── NeutronErrors.h
│   │   ├── driver
│   │   │   └── include
│   │   │       └── NeutronDriver.h
│   │   └── rt700
│   │       └── cm33
│   │           ├── libNeutronDriver.a
│   │           └── libNeutronFirmware.a
│   └── tensorflow-lite/     
source
│   ├── board_init.h
│   ├── demo_config.h
│   ├── demo_info.cpp
│   ├── demo_info.h
│   ├── image/*
│   ├── labels.h
│   ├── main.cpp
│   ├── mcux_config.h
│   ├── mcuxsdk_version.h
│   ├── model
│   │   ├── get_top_n.cpp
│   │   ├── get_top_n.h
│   │   ├── model.cpp
│   │   ├── model.h
│   │   ├── model_data.h    # Model data file
│   │   ├── model_mobilenet_ops_npu.cpp
│   │   ├── output_postproc.cpp
│   │   └── output_postproc.h
│   ├── pmic_support.c
│   ├── pmic_support.h
│   ├── semihost_hardfault.c
│   ├── timer.c
│   └── timer.h
└── doc/                     # Documentation
    └── readme.md

The library files and header files in the eiq/neutron/ folder are Neutron-Software related files.

Users can update the Neutron-Software version in this project by replacing these four files in the eiq/neutron/ folder: NeutronDriver.h, NeutronErrors.h, libNeutronDriver.a, and libNeutronFirmware.a.

(2) Project Structure in MCUXpresso for VScode

Please select the following two options in the MCUXpresso for VS Code extension settings:

  • [✓] Mcuxpresso > Experimental: Enable Add Files To Project

  • [✓] Mcuxpresso > Experimental: Enable Freestanding Copy Board

After importing a Freestanding project from the MCU SDK, the project structure is as follows (only primary files are listed here):

.
├── CMakeLists.txt
├── labels.h
├── main.cpp
├── stopwatch.bmp
├── image_data.h
├── image/*
├── common
│   ├── timer.c
│   ├── timer.h
│   └── timer_xtensa.h
├── model
│   ├── get_top_n.cpp
│   ├── get_top_n.h
│   ├── model.h
│   ├── output_postproc.cpp
│   └── output_postproc.h
├── pcq_npu
│   ├── mobilenet_v1_0.25_128_quant_int8_npu.tflite
│   ├── model_data.h             # Model data file
│   └── model_mobilenet_ops_npu.cpp
├── <board_name_folder> (e.g. mimxrt700evk_cm33_core0) 
│   └── middleware_eiq_neutron   # Neutron-Software files
│       ├── NeutronDriver.h
│       ├── NeutronErrors.h
│       └── cm33
│           ├── libNeutronDriver.a
│           └── libNeutronFirmware.a
└── tflm
    ├── demo_info.cpp
    └── model.cpp

For the boards with NPU hardware, the NPU model file is located in the pcq_npu/ folder. (For the boards without NPU hardware, the CPU version of the model file is located in the pcq/ folder.)

The header files and library files in the <board_name_folder>/middleware_eiq_neutron folder are Neutron-Software related files.

Users can update the Neutron-Software version in this project by replacing these four files: NeutronDriver.h, NeutronErrors.h, libNeutronDriver.a, and libNeutronFirmware.a.

Replace the model file#

If you need to replace the model file with your own model, please follow two main steps:

  • Step 1: Modify the model_data.h file.

  • Step 2: Modify the model_mobilenet_ops_npu.cpp file.

Step 1: Modify the model_data.h file.#

(1) Use NPU model

For NPU boards, you can use the Neutron Converter tool to convert your .tflite model into an NPU-optimized version, which simultaneously generates an NPU-specific .tflite file and a corresponding .h header file.

  • You can obtain the Neutron Converter tool from the eIQ Neutron SDK.

  • After downloading and extracting the Neutron SDK Zip package, you can find the Neutron Converter tool at the following path: /eiq-neutron-sdk-linux-x.x.x/bin/neutron-converter.

# Set environment variables
export NEUTRON_SDK_PATH="/path/to/eiq-neutron-sdk-linux-x.x.x"
export LD_LIBRARY_PATH="${NEUTRON_SDK_PATH}/lib:${LD_LIBRARY_PATH}"
export PATH="${NEUTRON_SDK_PATH}/bin:${PATH}"

# Convert for mcxn94x target
neutron-converter --input model_name.tflite --output model_name_mcxn94x.tflite --target mcxn94x --dump-header-file-output

# Convert for imxrt700 target
neutron-converter --input model_name.tflite --output model_name_rt700.tflite --target imxrt700 --dump-header-file-output

Neutron Converter Target Platforms:

Target

Description

Boards

mcxn94x

MCXN94x series

frdmmcxn947, mcxn5xxevk, mcxn9xxevk

imxrt700

i.MX RT700 series

mimxrt700evk

Modify the model_data.h file in the project:

  • Replace the original model data with model_data array and model_data_len from your model’s .h file.

  • Refer to the “Total data” value for graph “main” shown in the terminal output of neutron converter, and adjust the kTensorArenaSize value in the model_data.h file accordingly. Typically, kTensorArenaSize should be set to 105% or more of the “Total data” value.

# Example terminal output from neutron converter:
# The "Total data" value for graph "main" is 16,512 (bytes), so the kTensorArenaSize should be set to about 17,338 (bytes) (16,512 * 1.05)

Overall statistics for graph "main":
  Operators:
    ...<operator details>...
  Memory:
    Total data    = 16,512 (bytes) (Inputs + Outputs + Intermediate Variable Tensors)
    Total weights = 30,400 (bytes) (Weights)
    Total size    = 46,912 (bytes) (All)
// Modify the model_data.h file:

constexpr int kTensorArenaSize = <Total data * 1.05>;  // TensorArenaSize in (bytes)

static const uint8_t model_data[] __ALIGNED(16) __PLACEMENT = {
...<your model array>...
}

static const unsigned int model_data_len = <your model length>;

If the following error occurs while running the example, it is caused by the kTensorArenaSize being too small. Please increase the kTensorArenaSize accordingly.

Failed to resize buffer. Requested:16544, available 15928, missing:616
AllocateTensors() failed

(2) Use CPU model

You can use the following workflow to run a CPU-version model in this example.

The xxd tool can convert your .tflite model file into a .h header file. The command is as follows:

xxd -i model_name.tflite > model_name.h

Or you can also use Neutron Converter (Recommend) to generate the .h file by using the --dump-header-file-input option. This will convert your input CPU-version .tflite model into a CPU-version .h file.

neutron-converter --input model_name.tflite  --output model_name_imxrt700.tflite --target imxrt700  --dump-header-file-input

Modify the model_data.h file in the project: replace the original model data with model_data array and model_data_len from your model’s .h file.

# Modify the model_data.h file:

static const uint8_t model_data[] __ALIGNED(16) __PLACEMENT = {
...<your model array>...
}

static const unsigned int model_data_len = <your model length>;

Step 2: Modify the model_mobilenet_ops_npu.cpp file.#

In step 2, you need to refer to the .h file generated by the Neutron Converter in step 1 and modify the model operators in the model_mobilenet_ops_npu.cpp file.

Typically, the .h file output by the Neutron Converter contains content similar to the following:

/*
// Register operators for TFLite Micro.
static tflite::MicroMutableOpResolver<4> s_microOpResolver;
s_microOpResolver.AddQuantize();
s_microOpResolver.AddSoftmax();
s_microOpResolver.AddDequantize();
s_microOpResolver.AddCustom(tflite::GetString_NEUTRON_GRAPH(), tflite::Register_NEUTRON_GRAPH());
*/

Copy the operator registration code from the .h file generated by the Neutron Converter into the model_mobilenet_ops_npu.cpp file.

Image Conversion Script#

The image_data.h file is generated using Python with OpenCV and NumPy:

import cv2
import numpy as np

img = cv2.imread('stopwatch.bmp')
img = cv2.resize(img, (128, 128))
img = cv2.cvtColor(img, cv2.COLOR_BGR2RGB)

with open('image_data.h', 'w') as fout:
    print('#define STATIC_IMAGE_NAME "stopwatch"', file=fout)
    print('static const uint8_t image_data[] = {', file=fout)
    img.tofile(fout, ', ', '0x%02X')
    print('};\n', file=fout)

Note: For more details on model quantization and conversion, refer to the eIQ TensorFlow Lite User’s Guide included in the MCUXpresso SDK package.


Running the Demo#

Run result on MIMXRT700-EVK board with ARM GCC toolchain (NPU version):

Label image example using a TensorFlow Lite Micro model.
Detection threshold: 23%
Model: mobilenet_v1_0.25_128_quant_int8_npu
Core/NPU Frequency: 324 MHz
TensorArena Addr: 0x20000000 - 0x20040000
TensorArena Size: Total 0x40000 (262144 B); Used 0x246c0 (149184 B)
Model Addr: 0x20400000 - 0x2047b760
Model Size: 0x7b760 (505696 B)
Total Size Used: 654880 B (Model (505696 B) + TensorArena (149184 B))

Static data processing:
----------------------------------------
     Inference time: 2759 us
     Detected: stopwatch (87%)
----------------------------------------

Supported Boards with NPU#

Supported Boards with CPU Only#

  • MIMXRT1040-EVK

  • EVKB-IMXRT1050

  • MIMXRT1060-EVKB

  • MIMXRT1060-EVKC

  • EVK-MIMXRT1064

  • MIMXRT1160-EVK

  • MIMXRT1170-EVKB

  • MIMXRT1180-EVK

  • FRDM-IMXRT1186

  • EVK-MIMXRT595

  • EVK-MIMXRT685

  • MIMXRT685-AUD-EVK