MCUXpresso SDK Documentation

tsi_v5_selfmode

tsi_v5_selfmode#

Overview#

The tsi_v5_selfmode demo shows how to use TSI_V5 driver in self-cap mode:

In this example , available electrodes on board is used to show how to realize touch key.

  1. Firstly, get the non-touch calibration results as baseline electrode counter;

  2. Then, start the periodical Software-Trigger scan using polling method to detect finger touch;

  3. Wait for the electrodes touched and deal with the event.

Running the demo#

When running successfully, LED will be turn on when the electrode on board touched and will be turn off when released. The log output in terminal shall be similar as below:

TSI self mode demo.
TSI key touched.
TSI key released.
TSI key touched.
TSI key released.

Supported Boards#

FRDM-KE15Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE15Z board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When running successfully, LED will be turn on when the electrode on board touched and will be turn off when released. The log output in terminal shall be similar as below:

TSI self mode demo.
TSI key touched.
TSI key released.
TSI key touched.
TSI key released.
FRDM-KE16Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE16Z board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When running successfully, LED will be turn on when the electrode on board touched and will be turn off when released. The log output in terminal shall be similar as below:

TSI self mode demo.
TSI key touched.
TSI key released.
TSI key touched.
TSI key released.
FRDM-KE17Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE17Z board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When running successfully, LED will be turn on when the electrode on board touched and will be turn off when released. The log output in terminal shall be similar as below:

TSI self mode demo.
TSI key touched.
TSI key released.
TSI key touched.
TSI key released.
FRDM-KE17Z512
Hardware requirements
  • Micro USB cable

  • FRDM-KE17Z512 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When running successfully, LED will be turn on when the electrode on board touched and will be turn off when released. The log output in terminal shall be similar as below:

TSI self mode demo.
TSI key touched.
TSI key released.
TSI key touched.
TSI key released.