![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The frdm_k22f.h file defines GPIO pins for FRDM-K22F board. More...
#include "pin_mux.h"#include "fsl_smc.h"#include "MK22F51212.h"#include "RTE_Device.h"#include "gpio_driver.h"

Go to the source code of this file.
Macros | |
| #define | I2C_S1_SCL_PIN A5 |
| #define | I2C_S1_SDA_PIN A4 |
| #define | I2C_S1_DRIVER Driver_I2C0 |
| #define | I2C_S1_DEVICE_INDEX I2C0_INDEX |
| #define | I2C_S1_SIGNAL_EVENT I2C0_SignalEvent_t |
| #define | I2C_S2_SCL_PIN D15 |
| #define | I2C_S2_SDA_PIN D14 |
| #define | I2C_S2_DRIVER Driver_I2C1 |
| #define | I2C_S2_DEVICE_INDEX I2C1_INDEX |
| #define | I2C_S2_SIGNAL_EVENT I2C1_SignalEvent_t |
| #define | I2C_BB_SCL_PIN A5 |
| #define | I2C_BB_SDA_PIN A4 |
| #define | I2C_BB_DRIVER Driver_I2C0 |
| #define | I2C_BB_DEVICE_INDEX I2C0_INDEX |
| #define | I2C_BB_SIGNAL_EVENT I2C0_SignalEvent_t |
| #define | SPI_S_SCLK D13 |
| #define | SPI_S_MOSI D11 |
| #define | SPI_S_MISO D12 |
| #define | SPI_S_DRIVER Driver_SPI1 |
| #define | SPI_S_BAUDRATE 500000U |
| Transfer baudrate - 500k. More... | |
| #define | SPI_S_DEVICE_INDEX SPI1_INDEX |
| #define | SPI_S_SIGNAL_EVENT SPI1_SignalEvent_t |
| #define | HOST_S_DRIVER Driver_USART1 |
| #define | HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | HOST_B_DRIVER Driver_USART2 |
| #define | HOST_B_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | FXOS8700_BB_I2C_ADDR 0x1C |
| #define | FXOS8700_BB_INT1 INT1 |
| #define | FXOS8700_BB_INT2 INT2 |
| #define | ASK_USER_TO_RESUME(x) |
Wired UART Parameters | |
Sensor Fusion aliases are defined in terms of specific hardware features defined in MK22F51212.h. | |
| #define | WIRED_UART UART1 |
| KSDK instance name for the debug UART. More... | |
| #define | WIRED_UART_PORT_CLKEN kCLOCK_PortE |
| KDSK handle for the pin port clock enable. More... | |
| #define | WIRED_UART_PORT PORTE |
| KDSK handle for the pin port associated with this UART. More... | |
| #define | WIRED_UART_RX_PIN 1U |
| The port number associated with RX. More... | |
| #define | WIRED_UART_TX_PIN 0U |
| The port number associated with TX. More... | |
| #define | WIRED_UART_MUX kPORT_MuxAlt3 |
| If Using Orient App then use Host I/O. More... | |
| #define | WIRED_UART_IRQHandler UART1_RX_TX_IRQHandler |
| KDSK-specified IRQ handler name. More... | |
| #define | WIRED_UART_IRQn UART1_RX_TX_IRQn |
| The interrupt number associated with this IRQ. More... | |
| #define | WIRED_UART_CLKSRC UART1_CLK_SRC |
| KSDK instance name for the clock feeding this module. More... | |
| #define | WIRED_UART_IRQn UART1_RX_TX_IRQn |
| The interrupt number associated with this IRQ. More... | |
Wireless UART Parameters | |
Sensor Fusion aliases are defined in terms of specific hardware features defined in MK22F51212.h. | |
| #define | WIRELESS_UART UART2 |
| KSDK instance name for the debug UART. More... | |
| #define | WIRELESS_UART_PORT_CLKEN kCLOCK_PortD |
| KDSK handle for the pin port clock enable. More... | |
| #define | WIRELESS_UART_PORT PORTD |
| KDSK handle for the pin port associated with this UART. More... | |
| #define | WIRELESS_UART_RX_PIN 2U |
| The port number associated with RX. More... | |
| #define | WIRELESS_UART_TX_PIN 3U |
| The port number associated with TX. More... | |
| #define | WIRELESS_UART_MUX kPORT_MuxAlt3 |
| KDSK pin mux selector. More... | |
| #define | WIRELESS_UART_IRQHandler UART2_RX_TX_IRQHandler |
| KDSK-specified IRQ handler name. More... | |
| #define | WIRELESS_UART_IRQn UART2_RX_TX_IRQn |
| The interrupt number associated with this IRQ. More... | |
| #define | WIRELESS_UART_CLKSRC UART2_CLK_SRC |
| KSDK instance name for the clock feeding this module. More... | |
| #define | WIRELESS_UART_IRQn UART2_RX_TX_IRQn |
| The interrupt number associated with this IRQ. More... | |
Miscellaneous Hardware Configuration Parameters | |
| #define | THIS_BOARD 9 |
| FRDM_K22F. More... | |
| #define | CORE_SYSTICK_HZ 80000000 |
| core and systick clock rate (Hz) More... | |
| #define | CALIBRATION_NVM_ADDR 0x0007F800 |
| start of final 2K (sector size) of 512K flash More... | |
| #define | ADS_NVM_ADDR 0x0007F000 |
| start of the next to last 2K (sector size) of the 512K flash More... | |
| #define | FLASH_SECTOR_SIZE_PROPERTY kFLASH_PropertyPflashSectorSize |
| #define | FLASH_ERASE_KEY kFLASH_ApiEraseKey |
| #define | MAG_NVM_OFFSET 0 |
| #define | GYRO_NVM_OFFSET 100 |
| #define | ACCEL_NVM_OFFSET 140 |
The frdm_k22f.h file defines GPIO pins for FRDM-K22F board.
Definition in file frdm_k22f.h.
| #define ACCEL_NVM_OFFSET 140 |
Definition at line 186 of file frdm_k22f.h.
| #define ADS_NVM_ADDR 0x0007F000 |
start of the next to last 2K (sector size) of the 512K flash
Definition at line 179 of file frdm_k22f.h.
| #define ASK_USER_TO_RESUME | ( | x | ) |
Definition at line 130 of file frdm_k22f.h.
| #define CALIBRATION_NVM_ADDR 0x0007F800 |
start of final 2K (sector size) of 512K flash
Definition at line 178 of file frdm_k22f.h.
| #define CORE_SYSTICK_HZ 80000000 |
core and systick clock rate (Hz)
Definition at line 177 of file frdm_k22f.h.
| #define FLASH_ERASE_KEY kFLASH_ApiEraseKey |
Definition at line 181 of file frdm_k22f.h.
| #define FLASH_SECTOR_SIZE_PROPERTY kFLASH_PropertyPflashSectorSize |
Definition at line 180 of file frdm_k22f.h.
| #define FXOS8700_BB_I2C_ADDR 0x1C |
Definition at line 125 of file frdm_k22f.h.
| #define FXOS8700_BB_INT1 INT1 |
Definition at line 126 of file frdm_k22f.h.
| #define FXOS8700_BB_INT2 INT2 |
Definition at line 127 of file frdm_k22f.h.
| #define GYRO_NVM_OFFSET 100 |
Definition at line 185 of file frdm_k22f.h.
| #define HOST_B_DRIVER Driver_USART2 |
Definition at line 121 of file frdm_k22f.h.
| #define HOST_B_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 122 of file frdm_k22f.h.
| #define HOST_S_DRIVER Driver_USART1 |
Definition at line 117 of file frdm_k22f.h.
| #define HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 118 of file frdm_k22f.h.
| #define I2C_BB_DEVICE_INDEX I2C0_INDEX |
Definition at line 104 of file frdm_k22f.h.
| #define I2C_BB_DRIVER Driver_I2C0 |
Definition at line 103 of file frdm_k22f.h.
| #define I2C_BB_SCL_PIN A5 |
Definition at line 101 of file frdm_k22f.h.
| #define I2C_BB_SDA_PIN A4 |
Definition at line 102 of file frdm_k22f.h.
| #define I2C_BB_SIGNAL_EVENT I2C0_SignalEvent_t |
Definition at line 105 of file frdm_k22f.h.
| #define I2C_S1_DEVICE_INDEX I2C0_INDEX |
Definition at line 89 of file frdm_k22f.h.
| #define I2C_S1_DRIVER Driver_I2C0 |
Definition at line 88 of file frdm_k22f.h.
| #define I2C_S1_SCL_PIN A5 |
Definition at line 86 of file frdm_k22f.h.
| #define I2C_S1_SDA_PIN A4 |
Definition at line 87 of file frdm_k22f.h.
| #define I2C_S1_SIGNAL_EVENT I2C0_SignalEvent_t |
Definition at line 90 of file frdm_k22f.h.
| #define I2C_S2_DEVICE_INDEX I2C1_INDEX |
Definition at line 97 of file frdm_k22f.h.
| #define I2C_S2_DRIVER Driver_I2C1 |
Definition at line 96 of file frdm_k22f.h.
| #define I2C_S2_SCL_PIN D15 |
Definition at line 94 of file frdm_k22f.h.
| #define I2C_S2_SDA_PIN D14 |
Definition at line 95 of file frdm_k22f.h.
| #define I2C_S2_SIGNAL_EVENT I2C1_SignalEvent_t |
Definition at line 98 of file frdm_k22f.h.
| #define MAG_NVM_OFFSET 0 |
Definition at line 184 of file frdm_k22f.h.
| #define SPI_S_BAUDRATE 500000U |
Transfer baudrate - 500k.
Definition at line 112 of file frdm_k22f.h.
| #define SPI_S_DEVICE_INDEX SPI1_INDEX |
Definition at line 113 of file frdm_k22f.h.
| #define SPI_S_DRIVER Driver_SPI1 |
Definition at line 111 of file frdm_k22f.h.
| #define SPI_S_MISO D12 |
Definition at line 110 of file frdm_k22f.h.
| #define SPI_S_MOSI D11 |
Definition at line 109 of file frdm_k22f.h.
| #define SPI_S_SCLK D13 |
Definition at line 108 of file frdm_k22f.h.
| #define SPI_S_SIGNAL_EVENT SPI1_SignalEvent_t |
Definition at line 114 of file frdm_k22f.h.
| #define THIS_BOARD 9 |
FRDM_K22F.
Definition at line 176 of file frdm_k22f.h.
| #define WIRED_UART UART1 |
KSDK instance name for the debug UART.
Definition at line 144 of file frdm_k22f.h.
| #define WIRED_UART_CLKSRC UART1_CLK_SRC |
KSDK instance name for the clock feeding this module.
Definition at line 154 of file frdm_k22f.h.
| #define WIRED_UART_IRQHandler UART1_RX_TX_IRQHandler |
KDSK-specified IRQ handler name.
Definition at line 151 of file frdm_k22f.h.
| #define WIRED_UART_IRQn UART1_RX_TX_IRQn |
The interrupt number associated with this IRQ.
KSDK interrupt vector number.
Definition at line 155 of file frdm_k22f.h.
| #define WIRED_UART_IRQn UART1_RX_TX_IRQn |
The interrupt number associated with this IRQ.
KSDK interrupt vector number.
Definition at line 155 of file frdm_k22f.h.
| #define WIRED_UART_MUX kPORT_MuxAlt3 |
If Using Orient App then use Host I/O.
KDSK pin mux selector
Definition at line 149 of file frdm_k22f.h.
| #define WIRED_UART_PORT PORTE |
KDSK handle for the pin port associated with this UART.
Definition at line 146 of file frdm_k22f.h.
| #define WIRED_UART_PORT_CLKEN kCLOCK_PortE |
KDSK handle for the pin port clock enable.
Definition at line 145 of file frdm_k22f.h.
| #define WIRED_UART_RX_PIN 1U |
The port number associated with RX.
Definition at line 147 of file frdm_k22f.h.
| #define WIRED_UART_TX_PIN 0U |
The port number associated with TX.
Definition at line 148 of file frdm_k22f.h.
| #define WIRELESS_UART UART2 |
KSDK instance name for the debug UART.
Definition at line 162 of file frdm_k22f.h.
| #define WIRELESS_UART_CLKSRC UART2_CLK_SRC |
KSDK instance name for the clock feeding this module.
Definition at line 170 of file frdm_k22f.h.
| #define WIRELESS_UART_IRQHandler UART2_RX_TX_IRQHandler |
KDSK-specified IRQ handler name.
Definition at line 168 of file frdm_k22f.h.
| #define WIRELESS_UART_IRQn UART2_RX_TX_IRQn |
The interrupt number associated with this IRQ.
KSDK interrupt vector number.
Definition at line 171 of file frdm_k22f.h.
| #define WIRELESS_UART_IRQn UART2_RX_TX_IRQn |
The interrupt number associated with this IRQ.
KSDK interrupt vector number.
Definition at line 171 of file frdm_k22f.h.
| #define WIRELESS_UART_MUX kPORT_MuxAlt3 |
KDSK pin mux selector.
Definition at line 167 of file frdm_k22f.h.
| #define WIRELESS_UART_PORT PORTD |
KDSK handle for the pin port associated with this UART.
Definition at line 164 of file frdm_k22f.h.
| #define WIRELESS_UART_PORT_CLKEN kCLOCK_PortD |
KDSK handle for the pin port clock enable.
Definition at line 163 of file frdm_k22f.h.
| #define WIRELESS_UART_RX_PIN 2U |
The port number associated with RX.
Definition at line 165 of file frdm_k22f.h.
| #define WIRELESS_UART_TX_PIN 3U |
The port number associated with TX.
Definition at line 166 of file frdm_k22f.h.
Definition at line 114 of file frdm_k64f.c.
Definition at line 121 of file frdm_k64f.c.
Definition at line 128 of file frdm_k64f.c.
Definition at line 135 of file frdm_k64f.c.
Definition at line 66 of file frdm_k64f.c.
Definition at line 59 of file frdm_k64f.c.
| gpioHandleKSDK_t BLUE_LED |
Definition at line 221 of file frdm_k64f.c.
Definition at line 98 of file frdm_k64f.c.
Definition at line 105 of file frdm_k64f.c.
| gpioHandleKSDK_t D10 |
Definition at line 198 of file frdm_k64f.c.
| gpioHandleKSDK_t D11 |
Definition at line 82 of file frdm_k64f.c.
| gpioHandleKSDK_t D12 |
Definition at line 89 of file frdm_k64f.c.
| gpioHandleKSDK_t D13 |
Definition at line 75 of file frdm_k64f.c.
| gpioHandleKSDK_t D14 |
Definition at line 50 of file frdm_k64f.c.
| gpioHandleKSDK_t D15 |
Definition at line 43 of file frdm_k64f.c.
Definition at line 142 of file frdm_k64f.c.
Definition at line 149 of file frdm_k64f.c.
Definition at line 156 of file frdm_k64f.c.
Definition at line 163 of file frdm_k64f.c.
Definition at line 170 of file frdm_k64f.c.
Definition at line 177 of file frdm_k64f.c.
Definition at line 184 of file frdm_k64f.c.
Definition at line 191 of file frdm_k64f.c.
| gpioHandleKSDK_t GREEN_LED |
Definition at line 214 of file frdm_k64f.c.
| gpioHandleKSDK_t INT1 |
Definition at line 230 of file frdm_k64f.c.
| gpioHandleKSDK_t INT2 |
Definition at line 237 of file frdm_k64f.c.
| gpioHandleKSDK_t RED_LED |
Definition at line 207 of file frdm_k64f.c.