41 #ifndef __DRIVER_GPIO_H__ 42 #define __DRIVER_GPIO_H__ 44 #include "Driver_Common.h" 46 #include "fsl_common.h" 74 clock_ip_name_t clockName;
90 #define MAKE_GPIO_HANDLE(PortName, Base, PinNumber, ClockName, PortNumber) \ 91 static gpioHandleKSDK_t PortName##PinNumber = {.base = Base, \ 92 .pinNumber = PinNumber, \ 93 .mask = 1 << (PinNumber), \ 94 .clockName = ClockName, \ 95 .portNumber = PortNumber}; 97 #define GPIO_PIN_ID(PortName, PinNumber) &(PortName##PinNumber) 100 #endif // __DRIVER_GPIO_H__ enum _gint_interrupt gint_interrupt_t
The GPIO pin handle for KSDK.
The GPIO Configuration KSDK.
void(* gpio_isr_handler_t)(void *apUserData)
gint_trig_t interruptMode
struct gpioHandleKSDK gpioHandleKSDK_t
The GPIO pin handle for KSDK.
gpio_pin_config_t pinConfig
Access structure of the GPIO Driver.
gint_interrupt_t interruptPolarity
struct gpioConfigKSDK gpioConfigKSDK_t
The GPIO Configuration KSDK.
The Driver_GPIO.h file contains the definitions for GPIO Driver direction.
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
struct gpioIsrObj gpioIsrObj_t
The gpio isr object.