ISSDK  1.8
IoT Sensing Software Development Kit
Functions | Variables
fxlc95000_drv.c File Reference

The fxlc95000_drv.c file implements the FXLC95000 sensor driver interface. More...

#include "gpio_driver.h"
#include "fxlc95000_drv.h"
#include "systick_utils.h"
Include dependency graph for fxlc95000_drv.c:

Go to the source code of this file.

Functions

void FXLC95000_SPI_ReadPreprocess (void *pCmdOut, uint32_t offset, uint32_t size)
 The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. More...
 
void FXLC95000_SPI_WritePreprocess (void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
 The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. More...
 
int32_t FXLC95000_SPI_Initialize (fxlc95000_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSpiSelect, void *pSlaveSelect, void *pReset, uint16_t buildId)
 The interface function to initialize the sensor. More...
 
void FXLC95000_SPI_SetIdleTask (fxlc95000_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the SPI Idle Task. More...
 
int32_t FXLC95000_SPI_CommandResponse (fxlc95000_spi_sensorhandle_t *pSensorHandle, const registercommandlist_t *pCommandList, const registerreadlist_t *pResponseList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 
int32_t FXLC95000_I2C_CheckRomMode (ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress)
 The interface function to check if the sensor is in ROM CI Mode. More...
 
int32_t FXLC95000_I2C_FlashCommands (ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, const registercommandlist_t *pCommandList)
 The interface function to write ROM CI Commands. More...
 
int32_t FXLC95000_I2C_FlashPayload (ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t *pFlashBytes, uint8_t numBytes)
 The interface function to write ROM CI Data Payload. More...
 
int32_t FXLC95000_I2C_Initialize (fxlc95000_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint16_t buildId)
 The interface function to initialize the sensor. More...
 
void FXLC95000_I2C_SetIdleTask (fxlc95000_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the I2C Idle Task. More...
 
int32_t FXLC95000_I2C_CommandResponse (fxlc95000_i2c_sensorhandle_t *pSensorHandle, const registercommandlist_t *pCommandList, const registerreadlist_t *pResponseList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 

Variables

uint8_t fxlc95000_spiRead_CmdBuffer [FXLC95000_SPI_MAX_MSG_SIZE] = {0}
 
uint8_t fxlc95000_spiRead_DataBuffer [FXLC95000_SPI_MAX_MSG_SIZE] = {0}
 
uint8_t fxlc95000_spiWrite_CmdDataBuffer [FXLC95000_SPI_MAX_MSG_SIZE] = {0}
 

Detailed Description

The fxlc95000_drv.c file implements the FXLC95000 sensor driver interface.

Definition in file fxlc95000_drv.c.

Function Documentation

◆ FXLC95000_I2C_CheckRomMode()

int32_t FXLC95000_I2C_CheckRomMode ( ARM_DRIVER_I2C *  pBus,
uint8_t  index,
uint16_t  sAddress 
)

The interface function to check if the sensor is in ROM CI Mode.

This function checks the Response of Version Info command to determine if Sensor is in ROM CI Mode.

Parameters
[in]pBuspointer to the CMSIS API compatible I2C bus object.
[in]indexthe I2C device number.
[in]sAddressslave address of the device on the bus.
Constraints:
This can be called any time. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLC95000_I2C_CheckRomMode() returns the status.

Definition at line 190 of file fxlc95000_drv.c.

References registerDeviceInfo_t::deviceInstance, int32_t(), Register_I2C_BlockWrite(), and status.

Referenced by process_host_command().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLC95000_I2C_CommandResponse()

int32_t FXLC95000_I2C_CommandResponse ( fxlc95000_i2c_sensorhandle_t *  pSensorHandle,
const registercommandlist_t *  pCommandList,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pCommandListpointer to the command read list.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called any number of times only after FXLC95000_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLC95000_I2C_CommandResponse() returns the status .

Validate for the correct handle and register read list.

Check whether sensor handle is initialized before reading sensor data.

Definition at line 389 of file fxlc95000_drv.c.

References fxlc95000_i2c_sensorhandle_t::deviceInfo, FXLC95000_COCO_ERROR_MASK, int32_t(), fxlc95000_i2c_sensorhandle_t::isInitialized, fxlc95000_i2c_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, SENSOR_ERROR_WRITE, Sensor_I2C_BlockWrite(), Sensor_I2C_Read(), fxlc95000_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by fxlc95000_enSensor(), and main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLC95000_I2C_FlashCommands()

int32_t FXLC95000_I2C_FlashCommands ( ARM_DRIVER_I2C *  pBus,
uint8_t  index,
uint16_t  sAddress,
const registercommandlist_t *  pCommandList 
)

The interface function to write ROM CI Commands.

This function Writes ROM CI commands over I2C to the Sensor.

Parameters
[in]pBuspointer to the CMSIS API compatible I2C bus object.
[in]indexthe I2C device number.
[in]sAddressslave address of the device on the bus.
[in]pCommandListpointer to the command read list.
Constraints:
This can be called only if Sensor is in ROM CI Mode. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLC95000_I2C_FlashCommands() returns the status.

Validate for the correct handle and register write list.

Definition at line 211 of file fxlc95000_drv.c.

References registerDeviceInfo_t::deviceInstance, FXLC95000_COCO_ERROR_MASK, int32_t(), SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_I2C_BlockWrite(), and status.

Referenced by FXLC95000_I2C_FlashPayload(), and process_host_command().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLC95000_I2C_FlashPayload()

int32_t FXLC95000_I2C_FlashPayload ( ARM_DRIVER_I2C *  pBus,
uint8_t  index,
uint16_t  sAddress,
uint8_t *  pFlashBytes,
uint8_t  numBytes 
)

The interface function to write ROM CI Data Payload.

This function Writes ROM CI Payload Bytes by creating formatted Commands and writing over I2C to the Sensor.

Parameters
[in]pBuspointer to the CMSIS API compatible I2C bus object.
[in]indexthe I2C device number.
[in]sAddressslave address of the device on the bus.
[in]pFlashBytespointer to payload bytes of flash data.
[in]numBytesthe number of bytes of flash data to be written.
Constraints:
This can be called only if Sensor is in ROM CI Mode. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLC95000_I2C_FlashPayload() returns the status.

Definition at line 235 of file fxlc95000_drv.c.

References __END_WRITE_CMD__, FXLC95000_FLASH_PAYLOAD_ADDR_LEN, FXLC95000_I2C_FlashCommands(), FXLC95000_ROM_CI_READ_WRITE_ADDR_LEN, FXLC95000_ROM_CI_READ_WRITE_HDR_LEN, FXLC95000_ROM_CI_READ_WRITE_MAX_LEN, FXLC95000_ROM_CI_WRITE_MAX_LEN, FXLC95000_ROM_CI_WRITE_MIN_LEN, int32_t(), SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, and status.

Referenced by process_host_command().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLC95000_I2C_Initialize()

int32_t FXLC95000_I2C_Initialize ( fxlc95000_i2c_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_I2C *  pBus,
uint8_t  index,
uint16_t  sAddress,
uint16_t  buildId 
)

The interface function to initialize the sensor.

This function initialize the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible I2C bus object.
[in]indexthe I2C device number.
[in]sAddressslave address of the device on the bus.
[in]buildIdFXLC95000 firmware buid number.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLC95000_I2C_Initialize() returns the status .

Check the input parameters.

Definition at line 338 of file fxlc95000_drv.c.

References fxlc95000_i2c_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, registerDeviceInfo_t::functionParam, registerDeviceInfo_t::idleFunction, int32_t(), Register_I2C_BlockWrite(), SENSOR_ERROR_INVALID_PARAM, and status.

Referenced by fxlc95000_enSensor(), and main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLC95000_I2C_SetIdleTask()

void FXLC95000_I2C_SetIdleTask ( fxlc95000_i2c_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the I2C Idle Task.

Parameters
[in]fxlc95000_i2c_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on I2C Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after FXLC95000_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 381 of file fxlc95000_drv.c.

References fxlc95000_i2c_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by fxlc95000_enSensor(), and main().

Here is the caller graph for this function:

◆ FXLC95000_SPI_CommandResponse()

int32_t FXLC95000_SPI_CommandResponse ( fxlc95000_spi_sensorhandle_t *  pSensorHandle,
const registercommandlist_t *  pCommandList,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pCommandListpointer to the command read list.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called any number of times only after FXLC95000_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLC95000_SPI_CommandResponse() returns the status .

Validate for the correct handle and command list.

Check whether sensor handle is initialized before reading sensor data.

Parse through the read list and read the data one by one.

Definition at line 147 of file fxlc95000_drv.c.

References fxlc95000_spi_sensorhandle_t::deviceInfo, FXLC95000_COCO_ERROR_MASK, int32_t(), fxlc95000_spi_sensorhandle_t::isInitialized, fxlc95000_spi_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, SENSOR_ERROR_WRITE, Sensor_SPI_BlockWrite(), Sensor_SPI_Read(), fxlc95000_spi_sensorhandle_t::slaveParams, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLC95000_SPI_Initialize()

int32_t FXLC95000_SPI_Initialize ( fxlc95000_spi_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_SPI *  pBus,
uint8_t  index,
void *  pSpiSelect,
void *  pSlaveSelect,
void *  pReset,
uint16_t  buildId 
)

The interface function to initialize the sensor.

This function initializes the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible SPI bus object.
[in]indexthe I2C device number.
[in]pSlaveSelectslave select hndle of the device on the bus.
[in]pResetreset handle of the device on the bus.
[in]buildIdFXLC95000 firmware buid number.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLC95000_SPI_Initialize() returns the status .

Check the input parameters.

Initialize the sensor handle.

Definition at line 68 of file fxlc95000_drv.c.

References BOARD_DELAY_ms(), GENERIC_DRIVER_GPIO::clr_pin, fxlc95000_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, Driver_GPIO_KSDK, registerDeviceInfo_t::functionParam, FXLC95000_SPI_CMD_LEN, FXLC95000_SPI_ReadPreprocess(), FXLC95000_SPI_WritePreprocess(), FXLC95000_SS_ACTIVE_VALUE, GPIO_DIRECTION_OUT, registerDeviceInfo_t::idleFunction, int32_t(), fxlc95000_spi_sensorhandle_t::pCommDrv, pGPIODriver, GENERIC_DRIVER_GPIO::pin_init, spiSlaveSpecificParams_t::pReadPreprocessFN, spiSlaveSpecificParams_t::pTargetSlavePinID, spiSlaveSpecificParams_t::pWritePreprocessFN, Register_SPI_BlockWrite(), SENSOR_ERROR_INVALID_PARAM, GENERIC_DRIVER_GPIO::set_pin, fxlc95000_spi_sensorhandle_t::slaveParams, spiSlaveSpecificParams_t::spiCmdLen, spiSlaveSpecificParams_t::ssActiveValue, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLC95000_SPI_ReadPreprocess()

void FXLC95000_SPI_ReadPreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size 
)

The SPI Read Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Read Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start reading from.
[in]sizenumber of bytes to read.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 31 of file fxlc95000_drv.c.

References FXLC95000_SPI_CMD_LEN, fxlc95000_spiRead_CmdBuffer, fxlc95000_spiRead_DataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by FXLC95000_SPI_Initialize().

Here is the caller graph for this function:

◆ FXLC95000_SPI_SetIdleTask()

void FXLC95000_SPI_SetIdleTask ( fxlc95000_spi_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the SPI Idle Task.

Parameters
[in]fxlc95000_spi_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on SPI Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after FXLC95000_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 139 of file fxlc95000_drv.c.

References fxlc95000_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by main().

Here is the caller graph for this function:

◆ FXLC95000_SPI_WritePreprocess()

void FXLC95000_SPI_WritePreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size,
void *  pWritebuffer 
)

The SPI Write Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Write Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start writing from.
[in]sizenumber of bytes to write.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 48 of file fxlc95000_drv.c.

References FXLC95000_SPI_CMD_LEN, fxlc95000_spiWrite_CmdDataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by FXLC95000_SPI_Initialize().

Here is the caller graph for this function:

Variable Documentation

◆ fxlc95000_spiRead_CmdBuffer

uint8_t fxlc95000_spiRead_CmdBuffer[FXLC95000_SPI_MAX_MSG_SIZE] = {0}

Definition at line 24 of file fxlc95000_drv.c.

Referenced by FXLC95000_SPI_ReadPreprocess().

◆ fxlc95000_spiRead_DataBuffer

uint8_t fxlc95000_spiRead_DataBuffer[FXLC95000_SPI_MAX_MSG_SIZE] = {0}

Definition at line 25 of file fxlc95000_drv.c.

Referenced by FXLC95000_SPI_ReadPreprocess().

◆ fxlc95000_spiWrite_CmdDataBuffer

uint8_t fxlc95000_spiWrite_CmdDataBuffer[FXLC95000_SPI_MAX_MSG_SIZE] = {0}

Definition at line 26 of file fxlc95000_drv.c.

Referenced by FXLC95000_SPI_WritePreprocess().