14 #ifndef FXLS8962_AF_H_    15 #define FXLS8962_AF_H_    61 #define FXLS8962_SPI_MAX_MSG_SIZE (64)    65 #define FXLS8962_SPI_CMD_LEN (2)    69 #define FXLS8962_SS_ACTIVE_VALUE SPI_SS_ACTIVE_LOW   151                                 ARM_DRIVER_SPI *pBus,
   231 #endif // FXLS8962_AF_H_ 
This structure defines the fxls8962 raw data buffer. 
This structure defines the device specific info required by register I/O. 
int32_t FXLS8962_I2C_DeInit(fxls8962_i2c_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
This structure defines the Write command List. 
The sensor_io_spi.h file declares low-level interface functions for reading and writing sensor regist...
void FXLS8962_I2C_SetIdleTask(fxls8962_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
void FXLS8962_SPI_ReadPreprocess(void *pCmdOut, uint32_t offset, uint32_t size)
The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. ...
The register_io_spi.h file declares low-level interface functions for reading and writing sensor regi...
This structure defines the spi slave command format. 
void FXLS8962_SPI_WritePreprocess(void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
int32_t FXLS8962_SPI_Deinit(fxls8962_spi_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
This defines the sensor specific information for I2C. 
The register_io_i2c.h file declares low-level interface functions for reading and writing sensor regi...
int32_t FXLS8962_SPI_ReadData(fxls8962_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
This defines the sensor specific information for SPI. 
ARM_DRIVER_SPI * pCommDrv
int32_t FXLS8962_I2C_Initialize(fxls8962_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t *whoAmi)
The interface function to initialize the sensor. 
void FXLS8962_SPI_SetIdleTask(fxls8962_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the SPI Idle Task. 
registerDeviceInfo_t deviceInfo
int32_t FXLS8962_I2C_ReadData(fxls8962_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
int32_t FXLS8962_SPI_Configure(fxls8962_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
ARM_DRIVER_I2C * pCommDrv
int32_t FXLS8962_I2C_Configure(fxls8962_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
This structure defines the Read command List. 
spiSlaveSpecificParams_t slaveParams
This file contains the FXLS8962 Accelerometer register definitions, access macros, and device access functions. 
The sensor_io_i2c.h file declares low-level interface functions for reading and writing sensor regist...
registerDeviceInfo_t deviceInfo
int32_t FXLS8962_SPI_Initialize(fxls8962_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t *whoAmi)
The interface function to initialize the sensor.