14 #ifndef FXOS8700_DRV_H_    15 #define FXOS8700_DRV_H_    69 #define FXOS8700_SPI_MAX_MSG_SIZE (64)    73 #define FXOS8700_SPI_CMD_LEN (2)    77 #define FXOS8700_SS_ACTIVE_VALUE SPI_SS_ACTIVE_LOW   160                                 ARM_DRIVER_SPI *pBus,
   240 #endif // FXOS8700_DRV_H_ int32_t FXOS8700_SPI_ReadData(fxos8700_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
This structure defines the fxos8700 raw data buffer. 
 
This structure defines the device specific info required by register I/O. 
 
This structure defines the Write command List. 
 
The sensor_io_spi.h file declares low-level interface functions for reading and writing sensor regist...
 
ARM_DRIVER_I2C * pCommDrv
 
void FXOS8700_SPI_WritePreprocess(void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. 
 
The register_io_spi.h file declares low-level interface functions for reading and writing sensor regi...
 
int32_t FXOS8700_SPI_Configure(fxos8700_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
void FXOS8700_SPI_SetIdleTask(fxos8700_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the SPI Idle Task. 
 
This structure defines the spi slave command format. 
 
spiSlaveSpecificParams_t slaveParams
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
The register_io_i2c.h file declares low-level interface functions for reading and writing sensor regi...
 
This defines the sensor specific information for I2C. 
 
int32_t FXOS8700_SPI_Deinit(fxos8700_spi_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
int32_t FXOS8700_I2C_Initialize(fxos8700_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
void FXOS8700_I2C_SetIdleTask(fxos8700_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
This structure defines the fxos8700 raw accel data buffer. 
 
This defines the sensor specific information for SPI. 
 
registerDeviceInfo_t deviceInfo
 
int32_t FXOS8700_SPI_Initialize(fxos8700_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
int32_t FXOS8700_I2C_Deinit(fxos8700_i2c_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
 
This structure defines the Read command List. 
 
int32_t FXOS8700_I2C_ReadData(fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
The fxos8700.h file contains the register definitions for FXOS8700 sensor driver. ...
 
void FXOS8700_SPI_ReadPreprocess(void *pCmdOut, uint32_t offset, uint32_t size)
The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. ...
 
int32_t FXOS8700_I2C_Configure(fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
The sensor_io_i2c.h file declares low-level interface functions for reading and writing sensor regist...
 
ARM_DRIVER_SPI * pCommDrv
 
registerDeviceInfo_t deviceInfo