ISSDK  1.8
IoT Sensing Software Development Kit
Data Structures | Macros | Functions
fxos8700_drv.h File Reference

The fxos8700_drv.h file describes the fxos8700 driver interface and structures. More...

#include <stdint.h>
#include "fxos8700.h"
#include "sensor_io_i2c.h"
#include "sensor_io_spi.h"
#include "register_io_i2c.h"
#include "register_io_spi.h"
Include dependency graph for fxos8700_drv.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  fxos8700_spi_sensorhandle_t
 This defines the sensor specific information for SPI. More...
 
struct  fxos8700_i2c_sensorhandle_t
 This defines the sensor specific information for I2C. More...
 
struct  fxos8700_accelmagdata_t
 This structure defines the fxos8700 raw data buffer. More...
 
struct  fxos8700_acceldata_t
 This structure defines the fxos8700 raw accel data buffer. More...
 

Macros

#define FXOS8700_SPI_MAX_MSG_SIZE   (64)
 The MAX size of SPI message. More...
 
#define FXOS8700_SPI_CMD_LEN   (2)
 The size of the Sensor specific SPI Header. More...
 
#define FXOS8700_SS_ACTIVE_VALUE   SPI_SS_ACTIVE_LOW
 Is the Slave Select Pin Active Low or High. More...
 

Functions

int32_t FXOS8700_I2C_Initialize (fxos8700_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
 The interface function to initialize the sensor. More...
 
void FXOS8700_I2C_SetIdleTask (fxos8700_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the I2C Idle Task. More...
 
int32_t FXOS8700_I2C_Configure (fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
 The interface function to configure he sensor. More...
 
int32_t FXOS8700_I2C_ReadData (fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 
int32_t FXOS8700_I2C_Deinit (fxos8700_i2c_sensorhandle_t *pSensorHandle)
 The interface function to De Initialize sensor.. More...
 
int32_t FXOS8700_SPI_Initialize (fxos8700_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t whoAmi)
 The interface function to initialize the sensor. More...
 
void FXOS8700_SPI_SetIdleTask (fxos8700_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the SPI Idle Task. More...
 
int32_t FXOS8700_SPI_Configure (fxos8700_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
 The interface function to configure he sensor. More...
 
int32_t FXOS8700_SPI_ReadData (fxos8700_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 
int32_t FXOS8700_SPI_Deinit (fxos8700_spi_sensorhandle_t *pSensorHandle)
 The interface function to De Initialize sensor.. More...
 
void FXOS8700_SPI_ReadPreprocess (void *pCmdOut, uint32_t offset, uint32_t size)
 The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. More...
 
void FXOS8700_SPI_WritePreprocess (void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
 The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. More...
 

Detailed Description

The fxos8700_drv.h file describes the fxos8700 driver interface and structures.

Definition in file fxos8700_drv.h.

Macro Definition Documentation

◆ FXOS8700_SPI_CMD_LEN

#define FXOS8700_SPI_CMD_LEN   (2)

The size of the Sensor specific SPI Header.

Definition at line 73 of file fxos8700_drv.h.

Referenced by FXOS8700_SPI_Initialize(), FXOS8700_SPI_ReadPreprocess(), and FXOS8700_SPI_WritePreprocess().

◆ FXOS8700_SPI_MAX_MSG_SIZE

#define FXOS8700_SPI_MAX_MSG_SIZE   (64)

The MAX size of SPI message.

Definition at line 69 of file fxos8700_drv.h.

◆ FXOS8700_SS_ACTIVE_VALUE

#define FXOS8700_SS_ACTIVE_VALUE   SPI_SS_ACTIVE_LOW

Is the Slave Select Pin Active Low or High.

Definition at line 77 of file fxos8700_drv.h.

Referenced by FXOS8700_SPI_Initialize().

Function Documentation

◆ FXOS8700_I2C_Configure()

int32_t FXOS8700_I2C_Configure ( fxos8700_i2c_sensorhandle_t *  pSensorHandle,
const registerwritelist_t *  pRegWriteList 
)

The interface function to configure he sensor.

This function configure the sensor with requested ODR, Range and registers in the regsiter pair array.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pRegWriteListpointer to the register list.
Constraints:
This can be called any number of times only after FXOS8700_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXOS8700_I2C_Configure() returns the status .

Validate for the correct handle and register write list.

Check whether sensor handle is initialized before applying configuration.

Definition at line 260 of file fxos8700_drv.c.

References fxos8700_i2c_sensorhandle_t::deviceInfo, FXOS8700_CTRL_REG1, FXOS8700_CTRL_REG1_ACTIVE_ACTIVE_MODE, FXOS8700_CTRL_REG1_ACTIVE_MASK, FXOS8700_CTRL_REG1_ACTIVE_STANDBY_MODE, int32_t(), fxos8700_i2c_sensorhandle_t::isInitialized, fxos8700_i2c_sensorhandle_t::pCommDrv, Register_I2C_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_I2C_Write(), fxos8700_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by apply_register_write(), and main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXOS8700_I2C_Deinit()

int32_t FXOS8700_I2C_Deinit ( fxos8700_i2c_sensorhandle_t *  pSensorHandle)

The interface function to De Initialize sensor..

This function made sensor in a power safe state and de initialize its handle.

Parameters
[in]pSensorHandlehandle to the sensor.
Constraints:
This can be called only after FXOS8700_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXOS8700_I2C_Deinit() returns the status .

Check whether sensor handle is initialized before triggering sensor reset.

Trigger sensor device reset.

Definition at line 334 of file fxos8700_drv.c.

References fxos8700_i2c_sensorhandle_t::deviceInfo, FXOS8700_CTRL_REG2, FXOS8700_CTRL_REG2_RST_EN, FXOS8700_CTRL_REG2_RST_MASK, fxos8700_i2c_sensorhandle_t::isInitialized, fxos8700_i2c_sensorhandle_t::pCommDrv, Register_I2C_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, and fxos8700_i2c_sensorhandle_t::slaveAddress.

Here is the call graph for this function:

◆ FXOS8700_I2C_Initialize()

int32_t FXOS8700_I2C_Initialize ( fxos8700_i2c_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_I2C *  pBus,
uint8_t  index,
uint16_t  sAddress,
uint8_t  whoAmi 
)

The interface function to initialize the sensor.

This function initialize the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible I2C bus object.
[in]indexthe I2C device number.
[in]sAddressslave address of the device on the bus.
[in]whoamiWHO_AM_I value of the device.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXOS8700_I2C_Initialize() returns the status .

Read and store the device's WHO_AM_I.

Initialize the sensor handle.

Definition at line 222 of file fxos8700_drv.c.

References fxos8700_i2c_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, registerDeviceInfo_t::functionParam, FXOS8700_WHO_AM_I, registerDeviceInfo_t::idleFunction, int32_t(), fxos8700_i2c_sensorhandle_t::isInitialized, fxos8700_i2c_sensorhandle_t::pCommDrv, Register_I2C_Read(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, fxos8700_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXOS8700_I2C_ReadData()

int32_t FXOS8700_I2C_ReadData ( fxos8700_i2c_sensorhandle_t *  pSensorHandle,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called any number of times only after FXOS8700_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXOS8700_I2C_ReadData() returns the status .

Validate for the correct handle and register read list.

Check whether sensor handle is initialized before reading sensor data.

Parse through the read list and read the data one by one

Definition at line 305 of file fxos8700_drv.c.

References fxos8700_i2c_sensorhandle_t::deviceInfo, int32_t(), fxos8700_i2c_sensorhandle_t::isInitialized, fxos8700_i2c_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, Sensor_I2C_Read(), fxos8700_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by apply_register_read(), apply_register_readall(), and main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXOS8700_I2C_SetIdleTask()

void FXOS8700_I2C_SetIdleTask ( fxos8700_i2c_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the I2C Idle Task.

Parameters
[in]fxos8700_i2c_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on I2C Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after FXOS8700_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 252 of file fxos8700_drv.c.

References fxos8700_i2c_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by main().

Here is the caller graph for this function:

◆ FXOS8700_SPI_Configure()

int32_t FXOS8700_SPI_Configure ( fxos8700_spi_sensorhandle_t *  pSensorHandle,
const registerwritelist_t *  pRegWriteList 
)

The interface function to configure he sensor.

This function configure the sensor with requested ODR, Range and registers in the regsiter pair array.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pRegWriteListpointer to the register list.
Constraints:
This can be called any number of times only after FXOS8700_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXOS8700_SPI_Configure() returns the status .

Validate for the correct handle and register write list.

Check whether sensor handle is initialized before applying configuration.

Put the device into standby mode so that configuration can be applied.

Apply the Sensor Configuration based on the Register Write List

Put the device into active mode and ready for reading data.

Definition at line 124 of file fxos8700_drv.c.

References fxos8700_spi_sensorhandle_t::deviceInfo, FXOS8700_CTRL_REG1, FXOS8700_CTRL_REG1_ACTIVE_ACTIVE_MODE, FXOS8700_CTRL_REG1_ACTIVE_MASK, FXOS8700_CTRL_REG1_ACTIVE_STANDBY_MODE, int32_t(), fxos8700_spi_sensorhandle_t::isInitialized, fxos8700_spi_sensorhandle_t::pCommDrv, Register_SPI_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_SPI_Write(), fxos8700_spi_sensorhandle_t::slaveParams, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXOS8700_SPI_Deinit()

int32_t FXOS8700_SPI_Deinit ( fxos8700_spi_sensorhandle_t *  pSensorHandle)

The interface function to De Initialize sensor..

This function made sensor in a power safe state and de initialize its handle.

Parameters
[in]pSensorHandlehandle to the sensor.
Constraints:
This can be called only after after FXOS8700_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXOS8700_SPI_Deinit() returns the status.

Check whether sensor handle is initialized before triggering sensor reset.

Trigger sensor device reset.

De-initialize sensor handle. We do not validate write success since 8700 reset before sensing ack for the transaction.

Definition at line 198 of file fxos8700_drv.c.

References fxos8700_spi_sensorhandle_t::deviceInfo, FXOS8700_CTRL_REG2, FXOS8700_CTRL_REG2_RST_EN, FXOS8700_CTRL_REG2_RST_MASK, fxos8700_spi_sensorhandle_t::isInitialized, fxos8700_spi_sensorhandle_t::pCommDrv, Register_SPI_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, and fxos8700_spi_sensorhandle_t::slaveParams.

Here is the call graph for this function:

◆ FXOS8700_SPI_Initialize()

int32_t FXOS8700_SPI_Initialize ( fxos8700_spi_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_SPI *  pBus,
uint8_t  index,
void *  pSlaveSelect,
uint8_t  whoAmi 
)

The interface function to initialize the sensor.

This function initializes the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible SPI bus object.
[in]indexthe I2C device number.
[in]pSlaveSelectslave select hndle of the device on the bus.
[in]whoamiWHO_AM_I value of the device.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXOS8700_SPI_Initialize() returns the status .

Check the input parameters.

Initialize the sensor handle.

Read and store the device's WHO_AM_I.

Definition at line 67 of file fxos8700_drv.c.

References GENERIC_DRIVER_GPIO::clr_pin, fxos8700_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, Driver_GPIO_KSDK, registerDeviceInfo_t::functionParam, FXOS8700_SPI_CMD_LEN, FXOS8700_SPI_ReadPreprocess(), FXOS8700_SPI_WritePreprocess(), FXOS8700_SS_ACTIVE_VALUE, FXOS8700_WHO_AM_I, GPIO_DIRECTION_OUT, registerDeviceInfo_t::idleFunction, int32_t(), fxos8700_spi_sensorhandle_t::isInitialized, fxos8700_spi_sensorhandle_t::pCommDrv, pGPIODriver, GENERIC_DRIVER_GPIO::pin_init, spiSlaveSpecificParams_t::pReadPreprocessFN, spiSlaveSpecificParams_t::pTargetSlavePinID, spiSlaveSpecificParams_t::pWritePreprocessFN, Register_SPI_Read(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, GENERIC_DRIVER_GPIO::set_pin, fxos8700_spi_sensorhandle_t::slaveParams, SPI_SS_ACTIVE_LOW, spiSlaveSpecificParams_t::spiCmdLen, spiSlaveSpecificParams_t::ssActiveValue, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXOS8700_SPI_ReadData()

int32_t FXOS8700_SPI_ReadData ( fxos8700_spi_sensorhandle_t *  pSensorHandle,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called any number of times only after FXOS8700_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXOS8700_SPI_ReadData() returns the status .

Validate for the correct handle and register read list.

Check whether sensor handle is initialized before reading sensor data.

Parse through the read list and read the data one by one.

Definition at line 169 of file fxos8700_drv.c.

References fxos8700_spi_sensorhandle_t::deviceInfo, int32_t(), fxos8700_spi_sensorhandle_t::isInitialized, fxos8700_spi_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, Sensor_SPI_Read(), fxos8700_spi_sensorhandle_t::slaveParams, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXOS8700_SPI_ReadPreprocess()

void FXOS8700_SPI_ReadPreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size 
)

The SPI Read Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Read Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start reading from.
[in]sizenumber of bytes to read.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 30 of file fxos8700_drv.c.

References FXOS8700_SPI_CMD_LEN, fxos8700_spiRead_CmdBuffer, fxos8700_spiRead_DataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by FXOS8700_SPI_Initialize().

Here is the caller graph for this function:

◆ FXOS8700_SPI_SetIdleTask()

void FXOS8700_SPI_SetIdleTask ( fxos8700_spi_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the SPI Idle Task.

Parameters
[in]fxos8700_spi_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on SPI Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after FXOS8700_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 116 of file fxos8700_drv.c.

References fxos8700_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by main().

Here is the caller graph for this function:

◆ FXOS8700_SPI_WritePreprocess()

void FXOS8700_SPI_WritePreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size,
void *  pWritebuffer 
)

The SPI Write Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Write Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start writing from.
[in]sizenumber of bytes to write.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 47 of file fxos8700_drv.c.

References FXOS8700_SPI_CMD_LEN, fxos8700_spiWrite_CmdDataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by FXOS8700_SPI_Initialize().

Here is the caller graph for this function: