ISSDK  1.8
IoT Sensing Software Development Kit
Macros | Functions | Variables
register_io_i2c.c File Reference

The register_io_i2c.c file contains definitions for low-level interface functions for reading and writing sensor registers. More...

#include <string.h>
#include "issdk_hal.h"
#include "register_io_i2c.h"
Include dependency graph for register_io_i2c.c:

Go to the source code of this file.

Macros

#define I2C_COUNT   (sizeof(i2cBases) / sizeof(void *))
 

Functions

int32_t Register_I2C_BlockWrite (ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, const uint8_t *pBuffer, uint8_t bytesToWrite)
 The interface function to write a sensor register. More...
 
int32_t Register_I2C_Write (ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t value, uint8_t mask, bool repeatedStart)
 The interface function to write a sensor register. More...
 
int32_t Register_I2C_Read (ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
 The interface function to read a sensor register. More...
 

Variables

I2C_Type *const i2cBases [] = I2C_BASE_PTRS
 
volatile bool b_I2C_CompletionFlag [I2C_COUNT] = {false}
 
volatile uint32_t g_I2C_ErrorEvent [I2C_COUNT] = {ARM_I2C_EVENT_TRANSFER_DONE}
 

Detailed Description

The register_io_i2c.c file contains definitions for low-level interface functions for reading and writing sensor registers.

Definition in file register_io_i2c.c.

Macro Definition Documentation

◆ I2C_COUNT

#define I2C_COUNT   (sizeof(i2cBases) / sizeof(void *))

Definition at line 25 of file register_io_i2c.c.

Function Documentation

◆ Register_I2C_BlockWrite()

int32_t Register_I2C_BlockWrite ( ARM_DRIVER_I2C *  pCommDrv,
registerDeviceInfo_t *  devInfo,
uint16_t  slaveAddress,
uint8_t  offset,
const uint8_t *  pBuffer,
uint8_t  bytesToWrite 
)

The interface function to write a sensor register.

The interface function to block write sensor registers.

Definition at line 149 of file register_io_i2c.c.

References b_I2C_CompletionFlag, registerDeviceInfo_t::deviceInstance, registerDeviceInfo_t::functionParam, g_I2C_ErrorEvent, registerDeviceInfo_t::idleFunction, int32_t(), SENSOR_MAX_REGISTER_COUNT, and status.

Referenced by ADS_FXLC95000Query(), ADS_MMA9553Query(), FXLC95000_I2C_CheckRomMode(), FXLC95000_I2C_Initialize(), Host_IO_Receive(), MMA9553_I2C_Initialize(), and Sensor_I2C_BlockWrite().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ Register_I2C_Read()

int32_t Register_I2C_Read ( ARM_DRIVER_I2C *  pCommDrv,
registerDeviceInfo_t *  devInfo,
uint16_t  slaveAddress,
uint8_t  offset,
uint8_t  length,
uint8_t *  pOutBuffer 
)

◆ Register_I2C_Write()

int32_t Register_I2C_Write ( ARM_DRIVER_I2C *  pCommDrv,
registerDeviceInfo_t *  devInfo,
uint16_t  slaveAddress,
uint8_t  offset,
uint8_t  value,
uint8_t  mask,
bool  repeatedStart 
)

The interface function to write a sensor register.

The interface function to write a sensor register.

Set the register based on the values in the register value pair configuration.

Send the register address to read from.

Read the value.

'OR' in the requested values to the current contents of the register

Overwrite the register with specified value.

Write the updated value.

Definition at line 193 of file register_io_i2c.c.

References b_I2C_CompletionFlag, registerDeviceInfo_t::deviceInstance, registerDeviceInfo_t::functionParam, g_I2C_ErrorEvent, registerDeviceInfo_t::idleFunction, int32_t(), and status.

Referenced by FXAS21002_I2C_Configure(), FXAS21002_I2C_Deinit(), FXLS8962_I2C_Configure(), FXLS8962_I2C_DeInit(), FXLS896x_I2C_Configure(), FXLS896x_I2C_DeInit(), FXLS8974_I2C_Configure(), FXLS8974_I2C_DeInit(), FXOS8700_I2C_Configure(), FXOS8700_I2C_Deinit(), FXPQ3115_I2C_Configure(), FXPQ3115_I2C_DeInit(), ISL29023_I2C_DeInit(), MAG3110_I2C_Configure(), MAG3110_I2C_DeInit(), main(), MMA845x_I2C_Configure(), MMA845x_I2C_Deinit(), MMA865x_I2C_Configure(), MMA865x_I2C_DeInit(), MPL3115_I2C_Configure(), MPL3115_I2C_DeInit(), perform_selftest(), and Sensor_I2C_Write().

Here is the call graph for this function:
Here is the caller graph for this function:

Variable Documentation

◆ b_I2C_CompletionFlag

volatile bool b_I2C_CompletionFlag[I2C_COUNT] = {false}

◆ g_I2C_ErrorEvent

volatile uint32_t g_I2C_ErrorEvent[I2C_COUNT] = {ARM_I2C_EVENT_TRANSFER_DONE}

◆ i2cBases

I2C_Type* const i2cBases[] = I2C_BASE_PTRS

Definition at line 30 of file register_io_i2c.c.