14 #ifndef MMA865x_DRV_H_ 15 #define MMA865x_DRV_H_ 111 #endif // MMA865x_DRV_H_ ARM_DRIVER_I2C * pCommDrv
This structure defines the device specific info required by register I/O.
This structure defines the Write command List.
int32_t MMA865x_I2C_Configure(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
This defines the sensor specific information.
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
int32_t MMA865x_I2C_DeInit(mma865x_i2c_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor..
The register_io_i2c.h file declares low-level interface functions for reading and writing sensor regi...
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
void MMA865x_I2C_SetIdleTask(mma865x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
int32_t MMA865x_I2C_Initialize(mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
registerDeviceInfo_t deviceInfo
This structure defines the Read command List.
This structure defines the mma865x raw data buffer.
int32_t MMA865x_I2C_ReadData(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
The sensor_io_i2c.h file declares low-level interface functions for reading and writing sensor regist...