ISSDK  1.8
IoT Sensing Software Development Kit
mma865x_drv.c
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016, Freescale Semiconductor, Inc.
3  * Copyright 2016-2017 NXP
4  * All rights reserved.
5  *
6  * SPDX-License-Identifier: BSD-3-Clause
7  */
8 
9 /**
10  * @file mma865x_drv.c
11  * @brief The mma865x_drv.c file implements the mma865x functional interface.
12  */
13 
14 //-----------------------------------------------------------------------
15 // ISSDK Includes
16 //-----------------------------------------------------------------------
17 #include "mma865x_drv.h"
18 
19 //-----------------------------------------------------------------------
20 // Functions
21 //-----------------------------------------------------------------------
23  mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
24 {
26  uint8_t reg;
27 
28  /*! Check the input parameters. */
29  if ((pSensorHandle == NULL) || (pBus == NULL))
30  {
32  }
33 
34  pSensorHandle->deviceInfo.deviceInstance = index;
35  pSensorHandle->deviceInfo.functionParam = NULL;
36  pSensorHandle->deviceInfo.idleFunction = NULL;
37 
38  /*! Read and store the device's WHO_AM_I.*/
39  status = Register_I2C_Read(pBus, &pSensorHandle->deviceInfo, sAddress, MMA865x_WHO_AM_I, 1, &reg);
40  if ((ARM_DRIVER_OK != status) || (whoAmi != reg))
41  {
42  pSensorHandle->isInitialized = false;
43  return SENSOR_ERROR_INIT;
44  }
45 
46  /*! Initialize the sensor handle. */
47  pSensorHandle->pCommDrv = pBus;
48  pSensorHandle->slaveAddress = sAddress;
49  pSensorHandle->isInitialized = true;
50  return SENSOR_ERROR_NONE;
51 }
52 
54  registeridlefunction_t idleTask,
55  void *userParam)
56 {
57  pSensorHandle->deviceInfo.functionParam = userParam;
58  pSensorHandle->deviceInfo.idleFunction = idleTask;
59 }
60 
62 {
64 
65  /*! Validate for the correct handle and register write list.*/
66  if ((pSensorHandle == NULL) || (pRegWriteList == NULL))
67  {
69  }
70 
71  /*! Check whether sensor handle is initialized before applying configuration.*/
72  if (pSensorHandle->isInitialized != true)
73  {
74  return SENSOR_ERROR_INIT;
75  }
76 
77  /* Put the device into standby mode so that configuration can be applied. */
78  status =
79  Register_I2C_Write(pSensorHandle->pCommDrv, &pSensorHandle->deviceInfo, pSensorHandle->slaveAddress,
81  if (ARM_DRIVER_OK != status)
82  {
83  return SENSOR_ERROR_WRITE;
84  }
85 
86  /*! Apply the Sensor Configuration based on the Register Write List */
87  status = Sensor_I2C_Write(pSensorHandle->pCommDrv, &pSensorHandle->deviceInfo, pSensorHandle->slaveAddress,
88  pRegWriteList);
89  if (ARM_DRIVER_OK != status)
90  {
91  return SENSOR_ERROR_WRITE;
92  }
93 
94  /*! Put the device into active mode and ready for reading data.*/
95  status =
96  Register_I2C_Write(pSensorHandle->pCommDrv, &pSensorHandle->deviceInfo, pSensorHandle->slaveAddress,
98  if (ARM_DRIVER_OK != status)
99  {
100  return SENSOR_ERROR_WRITE;
101  }
102 
103  return SENSOR_ERROR_NONE;
104 }
105 
107  const registerreadlist_t *pReadList,
108  uint8_t *pBuffer)
109 {
110  int32_t status;
111 
112  /*! Validate for the correct handle and register read list.*/
113  if ((pSensorHandle == NULL) || (pReadList == NULL) || (pBuffer == NULL))
114  {
116  }
117 
118  /*! Check whether sensor handle is initialized before reading sensor data.*/
119  if (pSensorHandle->isInitialized != true)
120  {
121  return SENSOR_ERROR_INIT;
122  }
123 
124  /*! Parse through the read list and read the data one by one. */
125  status = Sensor_I2C_Read(pSensorHandle->pCommDrv, &pSensorHandle->deviceInfo, pSensorHandle->slaveAddress,
126  pReadList, pBuffer);
127  if (ARM_DRIVER_OK != status)
128  {
129  return SENSOR_ERROR_READ;
130  }
131 
132  return SENSOR_ERROR_NONE;
133 }
134 
136 {
137  int32_t status;
138 
139  if (pSensorHandle == NULL)
140  {
142  }
143 
144  /*! Check whether sensor handle is initialized before triggering sensor reset.*/
145  if (pSensorHandle->isInitialized != true)
146  {
147  return SENSOR_ERROR_INIT;
148  }
149 
150  /*! Trigger sensor device reset.*/
151  status = Register_I2C_Write(pSensorHandle->pCommDrv, &pSensorHandle->deviceInfo, pSensorHandle->slaveAddress,
153  if (ARM_DRIVER_OK != status)
154  {
155  return SENSOR_ERROR_WRITE;
156  }
157  else
158  {
159  /*! De-initialize sensor handle. */
160  pSensorHandle->isInitialized = false;
161  }
162 
163  return SENSOR_ERROR_NONE;
164 }
ARM_DRIVER_I2C * pCommDrv
Definition: mma865x_drv.h:32
int32_t Sensor_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerreadlist_t *pReadList, uint8_t *pOutBuffer)
Read register data from a sensor.
This structure defines the Write command List.
Definition: sensor_drv.h:68
This defines the sensor specific information.
Definition: mma865x_drv.h:29
int32_t status
int32_t Register_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
The interface function to read a sensor register.
int32_t Register_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t value, uint8_t mask, bool repeatedStart)
The interface function to write a sensor register.
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
int32_t MMA865x_I2C_ReadData(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
Definition: mma865x_drv.c:106
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor.
Definition: sensor_io_i2c.c:71
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
Definition: sensor_drv.h:97
#define MMA865x_CTRL_REG2_RST_EN
Definition: mma865x.h:1614
int32_t MMA865x_I2C_Configure(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
Definition: mma865x_drv.c:61
#define MMA865x_CTRL_REG1_ACTIVE_STANDBY
Definition: mma865x.h:1558
The mma865x_drv.h file describes the MMA865x driver interface and structures.
#define MMA865x_CTRL_REG1_ACTIVE_MASK
Definition: mma865x.h:1528
#define MMA865x_CTRL_REG1_ACTIVE_ACTIVATED
Definition: mma865x.h:1559
#define MMA865x_CTRL_REG2_RST_MASK
Definition: mma865x.h:1601
registerDeviceInfo_t deviceInfo
Definition: mma865x_drv.h:31
int32_t MMA865x_I2C_DeInit(mma865x_i2c_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor..
Definition: mma865x_drv.c:135
This structure defines the Read command List.
Definition: sensor_drv.h:78
void MMA865x_I2C_SetIdleTask(mma865x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
Definition: mma865x_drv.c:53
int32_t MMA865x_I2C_Initialize(mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
Definition: mma865x_drv.c:22
registeridlefunction_t idleFunction
Definition: sensor_drv.h:104