![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The lpc55s16.h file defines GPIO pin mappings for LPCXpresso55S16 board. More...
#include "pin_mux.h"#include "fsl_power.h"#include "RTE_Device.h"#include "gpio_driver.h"#include "clock_config.h"

Go to the source code of this file.
Macros | |
| #define | PORT0 0 |
| #define | PORT1 1 |
| #define | I2C_S1_SCL_PIN D15 |
| #define | I2C_S1_SDA_PIN D14 |
| #define | I2C_S1_DRIVER Driver_I2C4 |
| #define | I2C_S1_DEVICE_INDEX I2C4_INDEX |
| #define | I2C_S1_SIGNAL_EVENT I2C4_SignalEvent_t |
| #define | SPI_S_DRIVER Driver_SPI7 |
| #define | SPI_S_BAUDRATE 500000U |
| Transfer baudrate - 500k. More... | |
| #define | SPI_S_DEVICE_INDEX SPI7_INDEX |
| #define | SPI_S_SIGNAL_EVENT SPI7_SignalEvent_t |
| #define | HOST_S_DRIVER Driver_USART0 |
| #define | HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | HOST_B_DRIVER Driver_USART1 |
| #define | HOST_B_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | ASK_USER_TO_RESUME(x) |
| #define | SMC NULL |
Functions | |
| status_t | SMC_SetPowerModeWait (void *) |
| Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility. More... | |
| status_t | SMC_SetPowerModeVlpr (void *) |
| Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility. More... | |
| void | BOARD_BootClockRUN (void) |
| This function executes configuration of clocks. More... | |
The lpc55s16.h file defines GPIO pin mappings for LPCXpresso55S16 board.
Definition in file lpc55s16.h.
| #define ASK_USER_TO_RESUME | ( | x | ) |
Definition at line 62 of file lpc55s16.h.
| #define HOST_B_DRIVER Driver_USART1 |
Definition at line 58 of file lpc55s16.h.
| #define HOST_B_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 59 of file lpc55s16.h.
| #define HOST_S_DRIVER Driver_USART0 |
Definition at line 56 of file lpc55s16.h.
| #define HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 57 of file lpc55s16.h.
| #define I2C_S1_DEVICE_INDEX I2C4_INDEX |
Definition at line 46 of file lpc55s16.h.
| #define I2C_S1_DRIVER Driver_I2C4 |
Definition at line 45 of file lpc55s16.h.
| #define I2C_S1_SCL_PIN D15 |
Definition at line 43 of file lpc55s16.h.
| #define I2C_S1_SDA_PIN D14 |
Definition at line 44 of file lpc55s16.h.
| #define I2C_S1_SIGNAL_EVENT I2C4_SignalEvent_t |
Definition at line 47 of file lpc55s16.h.
| #define PORT0 0 |
Definition at line 21 of file lpc55s16.h.
| #define PORT1 1 |
Definition at line 22 of file lpc55s16.h.
| #define SMC NULL |
Definition at line 73 of file lpc55s16.h.
| #define SPI_S_BAUDRATE 500000U |
Transfer baudrate - 500k.
Definition at line 51 of file lpc55s16.h.
| #define SPI_S_DEVICE_INDEX SPI7_INDEX |
Definition at line 52 of file lpc55s16.h.
| #define SPI_S_DRIVER Driver_SPI7 |
Definition at line 50 of file lpc55s16.h.
| #define SPI_S_SIGNAL_EVENT SPI7_SignalEvent_t |
Definition at line 53 of file lpc55s16.h.
| void BOARD_BootClockRUN | ( | void | ) |
This function executes configuration of clocks.
This function executes configuration of clocks.
| void |
Definition at line 168 of file clock_config.c.
| status_t SMC_SetPowerModeVlpr | ( | void * | arg | ) |
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 169 of file lpc54114.c.
| status_t SMC_SetPowerModeWait | ( | void * | arg | ) |
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 155 of file lpc54114.c.
| gpioHandleKSDK_t BLUE_LED |
Definition at line 195 of file frdm_k64f.c.
Definition at line 72 of file frdm_k64f.c.
Definition at line 79 of file frdm_k64f.c.
| gpioHandleKSDK_t D11 |
Definition at line 56 of file frdm_k64f.c.
| gpioHandleKSDK_t D12 |
Definition at line 63 of file frdm_k64f.c.
| gpioHandleKSDK_t D13 |
Definition at line 49 of file frdm_k64f.c.
| gpioHandleKSDK_t D14 |
Definition at line 24 of file frdm_k64f.c.
| gpioHandleKSDK_t D15 |
Definition at line 17 of file frdm_k64f.c.
| gpioHandleKSDK_t GREEN_LED |
Definition at line 188 of file frdm_k64f.c.
| gpioHandleKSDK_t RED_LED |
Definition at line 181 of file frdm_k64f.c.