![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The evkmimxrt685.h file defines GPIO pin mappings for evkmimxrt685 board. More...


Go to the source code of this file.
Macros | |
| #define | I2C_S1_SCL_PIN A5 |
| #define | I2C_S1_SDA_PIN A4 |
| #define | I2C_S1_DRIVER Driver_I2C2 |
| #define | I2C_S1_DEVICE_INDEX I2C2_INDEX |
| #define | I2C_S1_SIGNAL_EVENT I2C2_SignalEvent_t |
| #define | I2C_S2_SCL_PIN D15 |
| #define | I2C_S2_SDA_PIN D14 |
| #define | I2C_S2_DRIVER Driver_I2C0 |
| #define | I2C_S2_DEVICE_INDEX I2C0_INDEX |
| #define | I2C_S2_SIGNAL_EVENT I2C0_SignalEvent_t |
| #define | SPI_S_SCLK D13 |
| #define | SPI_S_MISO D12 |
| #define | SPI_S_MOSI D11 |
| #define | SPI_S_DRIVER Driver_SPI1 |
| #define | SPI_S_BAUDRATE 500000U |
| Transfer baudrate - 500k. More... | |
| #define | SPI_S_DEVICE_INDEX SPI1_INDEX |
| #define | SPI_S_SIGNAL_EVENT SPI1_SignalEvent_t |
| #define | HOST_S_DRIVER Driver_USART1 |
| #define | HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | FXOS8700_BB_I2C_ADDR 0x1E |
| #define | FXOS8700_BB_INT1 INT1 |
| #define | FXOS8700_BB_INT2 INT2 |
| #define | ASK_USER_TO_RESUME(x) |
| #define | SMC NULL |
Functions | |
| status_t | SMC_SetPowerModeWait (void *) |
| Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility. More... | |
| status_t | SMC_SetPowerModeVlpr (void *) |
| Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility. More... | |
The evkmimxrt685.h file defines GPIO pin mappings for evkmimxrt685 board.
Definition in file evkmimxrt685.h.
| #define ASK_USER_TO_RESUME | ( | x | ) |
Definition at line 72 of file evkmimxrt685.h.
| #define FXOS8700_BB_I2C_ADDR 0x1E |
Definition at line 67 of file evkmimxrt685.h.
| #define FXOS8700_BB_INT1 INT1 |
Definition at line 68 of file evkmimxrt685.h.
| #define FXOS8700_BB_INT2 INT2 |
Definition at line 69 of file evkmimxrt685.h.
| #define HOST_S_DRIVER Driver_USART1 |
Definition at line 63 of file evkmimxrt685.h.
| #define HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 64 of file evkmimxrt685.h.
| #define I2C_S1_DEVICE_INDEX I2C2_INDEX |
Definition at line 43 of file evkmimxrt685.h.
| #define I2C_S1_DRIVER Driver_I2C2 |
Definition at line 42 of file evkmimxrt685.h.
| #define I2C_S1_SCL_PIN A5 |
Definition at line 40 of file evkmimxrt685.h.
| #define I2C_S1_SDA_PIN A4 |
Definition at line 41 of file evkmimxrt685.h.
| #define I2C_S1_SIGNAL_EVENT I2C2_SignalEvent_t |
Definition at line 44 of file evkmimxrt685.h.
| #define I2C_S2_DEVICE_INDEX I2C0_INDEX |
Definition at line 50 of file evkmimxrt685.h.
| #define I2C_S2_DRIVER Driver_I2C0 |
Definition at line 49 of file evkmimxrt685.h.
| #define I2C_S2_SCL_PIN D15 |
Definition at line 47 of file evkmimxrt685.h.
| #define I2C_S2_SDA_PIN D14 |
Definition at line 48 of file evkmimxrt685.h.
| #define I2C_S2_SIGNAL_EVENT I2C0_SignalEvent_t |
Definition at line 51 of file evkmimxrt685.h.
| #define SMC NULL |
Definition at line 83 of file evkmimxrt685.h.
| #define SPI_S_BAUDRATE 500000U |
Transfer baudrate - 500k.
Definition at line 58 of file evkmimxrt685.h.
| #define SPI_S_DEVICE_INDEX SPI1_INDEX |
Definition at line 59 of file evkmimxrt685.h.
| #define SPI_S_DRIVER Driver_SPI1 |
Definition at line 57 of file evkmimxrt685.h.
| #define SPI_S_MISO D12 |
Definition at line 55 of file evkmimxrt685.h.
| #define SPI_S_MOSI D11 |
Definition at line 56 of file evkmimxrt685.h.
| #define SPI_S_SCLK D13 |
Definition at line 54 of file evkmimxrt685.h.
| #define SPI_S_SIGNAL_EVENT SPI1_SignalEvent_t |
Definition at line 60 of file evkmimxrt685.h.
| status_t SMC_SetPowerModeVlpr | ( | void * | arg | ) |
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 169 of file lpc54114.c.
| status_t SMC_SetPowerModeWait | ( | void * | arg | ) |
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 155 of file lpc54114.c.
Definition at line 40 of file frdm_k64f.c.
Definition at line 33 of file frdm_k64f.c.
Definition at line 72 of file frdm_k64f.c.
Definition at line 79 of file frdm_k64f.c.
Definition at line 56 of file frdm_k64f.c.
Definition at line 63 of file frdm_k64f.c.
Definition at line 49 of file frdm_k64f.c.
Definition at line 24 of file frdm_k64f.c.
Definition at line 17 of file frdm_k64f.c.