![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The evkmimxrt1015.h file defines GPIO pin mappings for evkmimxrt1015 board. More...


Go to the source code of this file.
Macros | |
| #define | I2C_S1_SCL_PIN A5 |
| #define | I2C_S1_SDA_PIN A4 |
| #define | I2C_S1_DRIVER Driver_I2C1 |
| #define | I2C_S1_DEVICE_INDEX I2C1_INDEX |
| #define | I2C_S1_SIGNAL_EVENT I2C1_SignalEvent_t |
| #define | I2C_S2_SCL_PIN D15 |
| #define | I2C_S2_SDA_PIN D14 |
| #define | I2C_S2_DRIVER Driver_I2C0 |
| #define | I2C_S2_DEVICE_INDEX I2C0_INDEX |
| #define | I2C_S2_SIGNAL_EVENT I2C0_SignalEvent_t |
| #define | I2C_BB_SCL_PIN A5 |
| #define | I2C_BB_SDA_PIN A4 |
| #define | I2C_BB_DRIVER Driver_I2C3 |
| #define | I2C_BB_DEVICE_INDEX I2C3_INDEX |
| #define | I2C_BB_SIGNAL_EVENT I2C3_SignalEvent_t |
| #define | SPI_S_SCLK D13 |
| #define | SPI_S_MISO D12 |
| #define | SPI_S_MOSI D11 |
| #define | SPI_S_DRIVER Driver_SPI1 |
| #define | SPI_S_BAUDRATE 500000U |
| Transfer baudrate - 500k. More... | |
| #define | SPI_S_DEVICE_INDEX SPI1_INDEX |
| #define | SPI_S_SIGNAL_EVENT SPI1_SignalEvent_t |
| #define | HOST_S_DRIVER Driver_USART1 |
| #define | HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | FXOS8700_BB_I2C_ADDR 0x1E |
| #define | FXOS8700_BB_INT1 INT1 |
| #define | FXOS8700_BB_INT2 INT2 |
| #define | ASK_USER_TO_RESUME(x) |
| #define | I2C1 LPI2C1 |
| #define | I2C_Type LPI2C_Type |
| #define | I2C_BASE_PTRS LPI2C_BASE_PTRS |
| #define | SPI1 LPSPI1 |
| #define | SPI_Type LPSPI_Type |
| #define | SPI_BASE_PTRS LPSPI_BASE_PTRS |
| #define | SMC NULL |
Functions | |
| status_t | SMC_SetPowerModeWait (void *) |
| Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility. More... | |
| status_t | SMC_SetPowerModeVlpr (void *) |
| Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility. More... | |
The evkmimxrt1015.h file defines GPIO pin mappings for evkmimxrt1015 board.
Definition in file evkmimxrt1015.h.
| #define ASK_USER_TO_RESUME | ( | x | ) |
Definition at line 101 of file evkmimxrt1015.h.
| #define FXOS8700_BB_I2C_ADDR 0x1E |
Definition at line 96 of file evkmimxrt1015.h.
| #define FXOS8700_BB_INT1 INT1 |
Definition at line 97 of file evkmimxrt1015.h.
| #define FXOS8700_BB_INT2 INT2 |
Definition at line 98 of file evkmimxrt1015.h.
| #define HOST_S_DRIVER Driver_USART1 |
Definition at line 92 of file evkmimxrt1015.h.
| #define HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 93 of file evkmimxrt1015.h.
| #define I2C1 LPI2C1 |
Definition at line 112 of file evkmimxrt1015.h.
| #define I2C_BASE_PTRS LPI2C_BASE_PTRS |
Definition at line 114 of file evkmimxrt1015.h.
| #define I2C_BB_DEVICE_INDEX I2C3_INDEX |
Definition at line 79 of file evkmimxrt1015.h.
| #define I2C_BB_DRIVER Driver_I2C3 |
Definition at line 78 of file evkmimxrt1015.h.
| #define I2C_BB_SCL_PIN A5 |
Definition at line 76 of file evkmimxrt1015.h.
| #define I2C_BB_SDA_PIN A4 |
Definition at line 77 of file evkmimxrt1015.h.
| #define I2C_BB_SIGNAL_EVENT I2C3_SignalEvent_t |
Definition at line 80 of file evkmimxrt1015.h.
| #define I2C_S1_DEVICE_INDEX I2C1_INDEX |
Definition at line 65 of file evkmimxrt1015.h.
| #define I2C_S1_DRIVER Driver_I2C1 |
Definition at line 64 of file evkmimxrt1015.h.
| #define I2C_S1_SCL_PIN A5 |
Definition at line 62 of file evkmimxrt1015.h.
| #define I2C_S1_SDA_PIN A4 |
Definition at line 63 of file evkmimxrt1015.h.
| #define I2C_S1_SIGNAL_EVENT I2C1_SignalEvent_t |
Definition at line 66 of file evkmimxrt1015.h.
| #define I2C_S2_DEVICE_INDEX I2C0_INDEX |
Definition at line 72 of file evkmimxrt1015.h.
| #define I2C_S2_DRIVER Driver_I2C0 |
Definition at line 71 of file evkmimxrt1015.h.
| #define I2C_S2_SCL_PIN D15 |
Definition at line 69 of file evkmimxrt1015.h.
| #define I2C_S2_SDA_PIN D14 |
Definition at line 70 of file evkmimxrt1015.h.
| #define I2C_S2_SIGNAL_EVENT I2C0_SignalEvent_t |
Definition at line 73 of file evkmimxrt1015.h.
| #define I2C_Type LPI2C_Type |
Definition at line 113 of file evkmimxrt1015.h.
| #define SMC NULL |
Definition at line 120 of file evkmimxrt1015.h.
| #define SPI1 LPSPI1 |
Definition at line 115 of file evkmimxrt1015.h.
| #define SPI_BASE_PTRS LPSPI_BASE_PTRS |
Definition at line 117 of file evkmimxrt1015.h.
| #define SPI_S_BAUDRATE 500000U |
Transfer baudrate - 500k.
Definition at line 87 of file evkmimxrt1015.h.
| #define SPI_S_DEVICE_INDEX SPI1_INDEX |
Definition at line 88 of file evkmimxrt1015.h.
| #define SPI_S_DRIVER Driver_SPI1 |
Definition at line 86 of file evkmimxrt1015.h.
| #define SPI_S_MISO D12 |
Definition at line 84 of file evkmimxrt1015.h.
| #define SPI_S_MOSI D11 |
Definition at line 85 of file evkmimxrt1015.h.
| #define SPI_S_SCLK D13 |
Definition at line 83 of file evkmimxrt1015.h.
| #define SPI_S_SIGNAL_EVENT SPI1_SignalEvent_t |
Definition at line 89 of file evkmimxrt1015.h.
| #define SPI_Type LPSPI_Type |
Definition at line 116 of file evkmimxrt1015.h.
| status_t SMC_SetPowerModeVlpr | ( | void * | arg | ) |
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 169 of file lpc54114.c.
| status_t SMC_SetPowerModeWait | ( | void * | arg | ) |
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 155 of file lpc54114.c.
Definition at line 88 of file frdm_k64f.c.
Definition at line 95 of file frdm_k64f.c.
Definition at line 102 of file frdm_k64f.c.
Definition at line 109 of file frdm_k64f.c.
Definition at line 40 of file frdm_k64f.c.
Definition at line 33 of file frdm_k64f.c.
| gpioHandleiMXSDK_t BLUE_LED |
Definition at line 195 of file frdm_k64f.c.
Definition at line 72 of file frdm_k64f.c.
Definition at line 79 of file frdm_k64f.c.
Definition at line 172 of file frdm_k64f.c.
Definition at line 56 of file frdm_k64f.c.
Definition at line 63 of file frdm_k64f.c.
Definition at line 49 of file frdm_k64f.c.
Definition at line 24 of file frdm_k64f.c.
Definition at line 17 of file frdm_k64f.c.
Definition at line 116 of file frdm_k64f.c.
Definition at line 123 of file frdm_k64f.c.
Definition at line 130 of file frdm_k64f.c.
Definition at line 137 of file frdm_k64f.c.
Definition at line 49 of file evkmimxrt1015.h.
Definition at line 158 of file frdm_k64f.c.
Definition at line 165 of file frdm_k64f.c.
| gpioHandleiMXSDK_t GREEN_LED |
Definition at line 188 of file frdm_k64f.c.
| gpioHandleiMXSDK_t INT1 |
Definition at line 204 of file frdm_k64f.c.
| gpioHandleiMXSDK_t INT2 |
Definition at line 211 of file frdm_k64f.c.
| gpioHandleiMXSDK_t RED_LED |
Definition at line 181 of file frdm_k64f.c.