![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
middleware driver for NVM on Kinetis devices More...

Go to the source code of this file.
Macros | |
| #define | ERROR 1 |
| #define | SUCCESS 0; |
Functions | |
| byte | NVM_SetBlockFlash (uint8_t *Source, uint32_t Dest, uint16_t Count) |
middleware driver for NVM on Kinetis devices
Definition in file driver_KSDK_NVM.c.
| #define ERROR 1 |
Definition at line 21 of file driver_KSDK_NVM.c.
Referenced by NVM_SetBlockFlash().
| #define SUCCESS 0; |
Definition at line 22 of file driver_KSDK_NVM.c.
Referenced by NVM_SetBlockFlash().
| byte NVM_SetBlockFlash | ( | uint8_t * | Source, |
| uint32_t | Dest, | ||
| uint16_t | Count | ||
| ) |
Definition at line 24 of file driver_KSDK_NVM.c.
References CALIBRATION_NVM_ADDR, ERROR, FLASH_ERASE_KEY, FLASH_SECTOR_SIZE_PROPERTY, NVM_PAGE_NUMBER, NVM_SECTOR_NUMBER, NVM_SetBlockFlash(), SUCCESS, and SystemCoreClock.
Referenced by EraseAccelCalibrationFromNVM(), EraseGyroCalibrationFromNVM(), EraseMagCalibrationFromNVM(), NVM_SetBlockFlash(), SaveAccelCalibrationToNVM(), SaveGyroCalibrationToNVM(), and SaveMagCalibrationToNVM().