![]()  | 
  
    ISSDK
    1.8
    
   IoT Sensing Software Development Kit 
   | 
 
#include "fsl_common.h"

Go to the source code of this file.
Macros | |
| #define | BOARD_XTAL0_CLK_HZ 12000000U | 
| #define | BOARD_XTAL32K_CLK_HZ 32768U | 
| #define | BOARD_BootClockRUN BOARD_BootClockFROHF48M | 
| #define | BOARD_BOOTCLOCKFRO12M_CORE_CLOCK 12000000U | 
| #define | BOARD_BOOTCLOCKFROHF48M_CORE_CLOCK 48000000U | 
| #define | BOARD_BOOTCLOCKFROHF96M_CORE_CLOCK 96000000U | 
Functions | |
| void | BOARD_BootClockFRO12M (void) | 
| This function executes configuration of clocks.  More... | |
| void | BOARD_BootClockFROHF48M (void) | 
| This function executes configuration of clocks.  More... | |
| void | BOARD_BootClockFROHF96M (void) | 
| This function executes configuration of clocks.  More... | |
| #define BOARD_BOOTCLOCKFRO12M_CORE_CLOCK 12000000U | 
Core clock frequency: 12000000Hz
Definition at line 28 of file clock_config.h.
Referenced by BOARD_BootClockFRO12M().
| #define BOARD_BOOTCLOCKFROHF48M_CORE_CLOCK 48000000U | 
Core clock frequency: 48000000Hz
Definition at line 53 of file clock_config.h.
Referenced by BOARD_BootClockFROHF48M().
| #define BOARD_BOOTCLOCKFROHF96M_CORE_CLOCK 96000000U | 
Core clock frequency: 96000000Hz
Definition at line 78 of file clock_config.h.
Referenced by BOARD_BootClockFROHF96M().
| #define BOARD_BootClockRUN BOARD_BootClockFROHF48M | 
Definition at line 19 of file clock_config.h.
Referenced by main().
| #define BOARD_XTAL0_CLK_HZ 12000000U | 
Board xtal0 frequency in Hz
Definition at line 17 of file clock_config.h.
| #define BOARD_XTAL32K_CLK_HZ 32768U | 
Board xtal32K frequency in Hz
Definition at line 18 of file clock_config.h.
Referenced by BOARD_BootClockRUN().
| void BOARD_BootClockFRO12M | ( | void | ) | 
This function executes configuration of clocks.
< Set up the clock sources
< Set up FRO
< Ensure FRO is on
< Switch to FRO 12MHz first to ensure we can change voltage without accidentally being below the voltage for current speed
< Set up FRO to the 12 MHz, just for sure
< Set voltage for the one of the fastest clock outputs: System clock output
< Set FLASH wait states for core
< Set up dividers
< Set AHBCLKDIV divider to value 1
< Set up clock selectors - Attach clocks to the peripheries
< Switch MAIN_CLK to FRO12M
< Set SystemCoreClock variable.
< Set up the clock sources
< Configure FRO192M
< Ensure FRO is on
< Set up FRO to the 12 MHz, just for sure
< Switch to FRO 12MHz first to ensure we can change the clock setting
< Set FLASH wait states for core
< Set up dividers
< Set AHBCLKDIV divider to value 1
< Set up clock selectors - Attach clocks to the peripheries
< Switch MAIN_CLK to FRO12M
Definition at line 63 of file clock_config.c.
| void BOARD_BootClockFROHF48M | ( | void | ) | 
This function executes configuration of clocks.
< Set up the clock sources
< Set up FRO
< Ensure FRO is on
< Switch to FRO 12MHz first to ensure we can change voltage without accidentally being below the voltage for current speed
< Set voltage for the one of the fastest clock outputs: System clock output
< Set FLASH wait states for core
< Set up high frequency FRO output to selected frequency
< Set up dividers
< Set AHBCLKDIV divider to value 1
< Set up clock selectors - Attach clocks to the peripheries
< Switch MAIN_CLK to FRO_HF
< Set SystemCoreClock variable.
Definition at line 101 of file clock_config.c.
References BOARD_BOOTCLOCKFROHF48M_CORE_CLOCK, and SystemCoreClock.
| void BOARD_BootClockFROHF96M | ( | void | ) | 
This function executes configuration of clocks.
< Set up the clock sources
< Set up FRO
< Ensure FRO is on
< Switch to FRO 12MHz first to ensure we can change voltage without accidentally being below the voltage for current speed
< Set voltage for the one of the fastest clock outputs: System clock output
< Set FLASH wait states for core
< Set up high frequency FRO output to selected frequency
< Set up dividers
< Set AHBCLKDIV divider to value 1
< Set up clock selectors - Attach clocks to the peripheries
< Switch MAIN_CLK to FRO_HF
< Set SystemCoreClock variable.
< Set up the clock sources
< Configure FRO192M
< Ensure FRO is on
< Set up FRO to the 12 MHz, just for sure
< Switch to FRO 12MHz first to ensure we can change the clock setting
< Set FLASH wait states for core
< Set up dividers
< Set AHBCLKDIV divider to value 1
< Set up clock selectors - Attach clocks to the peripheries
< Switch MAIN_CLK to FRO_HF
Definition at line 142 of file clock_config.c.