![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "fsl_irqsteer.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "fxas21002_drv.h"
Go to the source code of this file.
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | fxas21002_Config_Normal [] |
| const registerreadlist_t | fxas21002_DRDY [] = {{.readFrom = FXAS21002_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| const registerreadlist_t | fxas21002_Output_Values [] |
| int main | ( | void | ) |
Main function.
Initialize the MCU hardware.
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize the FXAS21002 sensor driver.
Configure the FXAS21002 sensor driver.
Wait for data ready from the FXAS21002.
Read the raw sensor data from the FXAS21002.
Convert the raw sensor data to signed 16-bit container for display to the debug port.
Definition at line 50 of file fxas21002_poll.c.
References ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, FXAS21002_DR_STATUS_ZYXDR_MASK, FXAS21002_GYRO_DATA_SIZE, FXAS21002_I2C_ADDR, FXAS21002_I2C_Configure(), FXAS21002_I2C_Initialize(), FXAS21002_I2C_ReadData(), FXAS21002_WHO_AM_I_WHOAMI_PROD_VALUE, fxas21002_gyrodata_t::gyro, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), rawData, SENSOR_ERROR_NONE, and status.

| const registerwritelist_t fxas21002_Config_Normal[] |
Prepare the register write list to configure FXAS21002 in non-FIFO mode.
Definition at line 32 of file fxas21002_poll.c.
| const registerreadlist_t fxas21002_DRDY[] = {{.readFrom = FXAS21002_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Prepare the register read list to read FXAS21002 DataReady status.
Definition at line 38 of file fxas21002_poll.c.
| const registerreadlist_t fxas21002_Output_Values[] |
Prepare the register read list to read the raw gyro data from the FXAS21002.
Definition at line 41 of file fxas21002_poll.c.