18 #include "clock_config.h"    20 #include "fsl_debug_console.h"    25 #include "issdk_hal.h"    26 #include "gpio_driver.h"    33 #include "Driver_I2C.h"    38 #define FXLS8964_DATA_SIZE      6    39 #define FXLS8964_STANDBY_MODE   0    40 #define FXLS8964_ACTIVE_MODE    1   111     uint8_t intStatus, eventStatus = 0;
   112     uint8_t sleeptowake = 0;
   113                 uint8_t waketosleep = 0;
   114     uint8_t firsttransition = 1;
   115     uint8_t onetime_modetransition = 1;
   123     PRINTF(
"\r\n ISSDK FXLS896xAF sensor driver example to detect motion event & AWS\r\n");
   133     if (ARM_DRIVER_OK != status)
   135         PRINTF(
"\r\n I2C Initialization Failed\r\n");
   140     status = 
I2Cdrv->PowerControl(ARM_POWER_FULL);
   141     if (ARM_DRIVER_OK != status)
   143         PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
   148     status = 
I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   149     if (ARM_DRIVER_OK != status)
   151         PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
   158     if (ARM_DRIVER_OK != status)
   160         PRINTF(
"\r\n Sensor Initialization Failed\r\n");
   165                 PRINTF(
"\r\n Successfully Initialized Gemini with WHO_AM_I = 0x%X\r\n", whoami);
   169                 PRINTF(
"\r\n Successfully Initialized Timandra with WHO_AM_I = 0x%X\r\n", whoami);
   173                 PRINTF(
"\r\n Successfully Initialized Newstein with WHO_AM_I = 0x%X\r\n", whoami);
   177                 PRINTF(
"\r\n Bad WHO_AM_I = 0x%X\r\n", whoami);
   188         PRINTF(
"\r\n FXLS8964 Sensor Configuration Failed, Err = %d\r\n", status);
   191     PRINTF(
"\r\n Successfully Applied FXLS8964 Sensor Configuration\r\n");
   198         if (ARM_DRIVER_OK != status)
   207               if (sleeptowake == 1)
   210                 PRINTF(
"\r\n Motion Detected....\r\n");
   211                 PRINTF(
"\r\n Motion Wake Mode Detected....SYSMODE = %d\r\n", eventStatus);
   212                 PRINTF(
"\r\n MCU woke-up on sensor motion event\r\n");
   213                 PRINTF(
"\r\n Will enter sleep mode after expiration of ASLP counter = ~5sec\r\n\r\n");
   223            if ((waketosleep == 1) || (firsttransition == 1))
   225              if (1 == onetime_modetransition)
   227                onetime_modetransition = 0;
   231              if (ARM_DRIVER_OK != status)
   235              PRINTF(
"\r\n ASLP counter expired....\r\n");
   236              PRINTF(
"\r\n Going to Sleep Mode....SYSMODE = %d\r\n", eventStatus);
   237              PRINTF(
"\r\n Putting MCU in low power sleep\r\n\r\n");
 void(* set_pin)(pinID_t aPinId)
 
The fxls896x_drv.h file describes the FXLS8964/67AF driver interface and structures. 
 
This structure defines the Write command List. 
 
#define FXLS896x_SENS_CONFIG1_FSR_4G
 
#define FXLS896x_SYS_MODE_SYS_MODE_WAKE
 
#define FXLS896x_I2C_ADDR
 
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
 
#define FXLS896x_SENS_CONFIG3_WAKE_ODR_400HZ
 
const registerreadlist_t cFxls896xReadIntStatus[]
Read register list to read INT_STATUS Register. 
 
#define FXLS896x_SDCD_CONFIG2_SDCD_EN_EN
 
int32_t FXLS896x_I2C_Initialize(fxls896x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t *whoami)
The interface function to initialize the sensor. 
 
Access structure of the GPIO Driver. 
 
#define FXLS896x_INT_PIN_SEL_WK_OUT_INT2_DIS
 
#define FXLS896x_SENS_CONFIG4_INT_POL_MASK
 
#define __END_WRITE_DATA__
 
void(* clr_pin)(pinID_t aPinId)
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
#define FXLS896x_INT_EN_WAKE_OUT_EN_MASK
 
#define FXLS8967_WHOAMI_VALUE
 
#define FXLS896x_SDCD_CONFIG2_SDCD_EN_MASK
 
const registerreadlist_t cFxls896xReadSysMode[]
Read register list to read SysMode Register. 
 
#define I2C_S_SIGNAL_EVENT
 
#define FXLS896x_SDCD_CONFIG1_X_OT_EN_MASK
 
#define FXLS896x_SDCD_CONFIG1_Y_OT_EN_EN
 
#define FXLS896x_SDCD_CONFIG1_OT_ELE_MASK
 
#define FXLS896x_SENS_CONFIG3_SLEEP_ODR_MASK
 
#define BOARD_BootClockRUN
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
#define FXLS896x_SENS_CONFIG1_FSR_MASK
 
int main(void)
This is the The main function implementation. 
 
#define FXLS896x_SDCD_CONFIG1_Y_OT_EN_MASK
 
#define FXLS896x_SENS_CONFIG4_WK_SDCD_OT_MASK
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
#define FXLS896x_SDCD_CONFIG2_REF_UPDM_SDCD_REF
 
This defines the sensor specific information for I2C. 
 
#define FXLS896x_SENS_CONFIG4_WK_SDCD_OT_EN
 
#define FXLS896x_SENS_CONFIG3_SLEEP_ODR_6_25HZ
 
void fxls896x_int_callback(void *pUserData)
This is the Sensor Data Ready ISR implementation. 
 
int32_t FXLS896x_I2C_Configure(fxls896x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
#define __END_READ_DATA__
 
int32_t FXLS896x_I2C_ReadData(fxls896x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
#define FXLS896x_SDCD_CONFIG1_X_OT_EN_EN
 
#define FXLS896x_INT_PIN_SEL_WK_OUT_INT2_MASK
 
GENERIC_DRIVER_GPIO * pGpioDriver
 
#define FXLS896x_SDCD_CONFIG2_REF_UPDM_MASK
 
fxls896x_i2c_sensorhandle_t fxls896xDriver
 
void FXLS896x_I2C_SetIdleTask(fxls896x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
volatile bool gFxls896xIntFlag
 
#define FXLS896x_SDCD_CONFIG1_Z_OT_EN_MASK
 
#define FXLS896x_SENS_CONFIG4_INT_POL_ACT_HIGH
 
void BOARD_SystickEnable(void)
Function to enable systicks framework. 
 
const registerwritelist_t cFxls896xAwsConfig[]
Register settings for configuring SDCD-OT for tap-detection and Auto-Wake/Sleep in interrupt mode...
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
#define FXLS896x_SDCD_CONFIG1_Z_OT_EN_EN
 
This structure defines the Read command List. 
 
gpioHandleKSDK_t GREEN_LED
 
#define FXLS8974_WHOAMI_VALUE
 
#define FXLS8968_WHOAMI_VALUE
 
#define I2C_S_DEVICE_INDEX
 
#define FXLS896x_SDCD_CONFIG1_OT_ELE_DIS
 
void BOARD_InitDebugConsole(void)
 
#define FXLS8962_WHOAMI_VALUE
 
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features. 
 
#define FXLS896x_SENS_CONFIG3_WAKE_ODR_MASK
 
#define FXLS8964_WHOAMI_VALUE
 
#define FXLS896x_INT_EN_WAKE_OUT_EN_EN