Run and Debug from Command-Line Environment / LINUX
RT500 SDK has been configured to be as flexible as possible to support multiple toolchains, including ARMGCC and XCC command-line environment. The principles and essentials are still the same as with the IDE. Command-line environment settings are nearly identical between WIN32 and LINUX, just with a few different path settings.
Build and Debug Arm Application
The Arm application requires the GNU Arm Embedded Toolchain and CMake version 3.x for command line compile and linking. See the ‘Getting Started with MCUXpresso SDK for RT500.pdf’ in the <SDK_ROOT>/docs/ directory for more information on installation and configuration of required build tools for command line development.
Launch a command prompt / terminal and change directory to the xaf_record application.
user@linux:~/SDK/boards/evkmimxrt595/dsp_examples/xaf_record/cm33/Armgcc$ **ls -1** build_all.bat build_all.sh build_debug.bat build_debug.sh build_flash_debug.bat build_flash_debug.sh build_flash_release.bat build_flash_release.sh build_release.bat build_release.sh clean.bat clean.sh CMakeLists.txt
Use .bat files to build the configuration on Windows, and .sh files on Linux/UNIX.
user@linux:~/SDK/boards/evkmimxrt595/dsp_examples/xaf_record/cm33/Armgcc$ **./build\_debug.sh** ... [100%] Linking C executable debug/dsp_xaf_record_cm33.elf [100%] Built target dsp_xaf_record_cm33.elf
Launch the GDB server (NOTE: J-Link requires version >= 6.46).
user@linux:/opt/JLink$ ./JLinkGDBServerCLExe -device MIMXRT595_M33 -if SWD SEGGER J-Link GDB Server V6.46j Command Line Version ... Listening on TCP/IP port 2331 Connecting to target...Connected to target Waiting for GDB connection...
Connect with GDB to the device and load Arm application.
user@jlinux:~/SDK/boards/evkmimxrt595/dsp_examples/xaf_record/cm33/Armgcc$ Arm-none-eabi-gdb debug/dsp_xaf_demo_cm33.elf ... Reading symbols from debug/dsp_xaf_record_cm33.elf... (gdb) **target remote localhost:2331** Remote debugging using localhost:2331 0x1301ec7a in ?? () (gdb) **mon reset** Resetting target (gdb) **load** Loading section .flash_config, size 0x200 lma 0x7f400 Loading section .interrupts, size 0x130 lma 0x80000 Loading section .text, size 0xe330 lma 0x80130 Loading section CodeQuickAccess, size 0x52c lma 0x8e460 Loading section .Arm, size 0x8 lma 0x8e98c Loading section .init_array, size 0x4 lma 0x8e994 Loading section .fini_array, size 0x4 lma 0x8e998 Loading section .data, size 0x104 lma 0x8e99c Start address 0x801e4, load size 60576 Transfer rate: 272 KB/sec, 5506 bytes/write. (gdb) **b main** Breakpoint 1 at 0x808f2: file /SDK/boards/src/dsp_examples/xaf_record/cm33/main_cm33.c, line 161. (gdb) **c** Continuing. Breakpoint 1, main () at /SDK/boards/src/dsp_examples/xaf_record/cm33/main_cm33.c:161 161 BOARD_InitHardware();
Parent topic:Run and Debug from Command-Line Environment / LINUX
Build and Debug DSP Application
The Xtensa command line toolchain is installed as part of the Xplorer IDE. The tools can optionally be installed on a new Windows or Linux system without the IDE using the redistributable compressed file found under <XTENSA_ROOT>/XtDevTools/downloads/RI-2023.11/tools/. For details, see Install Xtensa On Chip Debugger Daemon.
In order to use the command line tools, some environment variables need to be setup that are used by the cmake build scripts:
# Add tools binaries to PATH. Assume ~/xtensa/ is install root - please adjust accordingly.
export PATH=$PATH:~/xtensa/XtDevTools/install/tools/RI-2023.11-linux/XtensaTools/bin
# (Optional) Use environment variable to control license file
# NOTE: ~/.flexlmrc will override this selection. Please delete that file before proceeding.
export LM_LICENSE_FILE=~/RT500.lic
# Setup env vars needed for compile and linking
export XCC_DIR=~/xtensa/XtDevTools/install/tools/RI-2023.11-linux/XtensaTools
export XTENSA_SYSTEM=~/xtensa/XtDevTools/install/builds/RI-2023.11-linux/nxp_RT500_RI23_11_newlib/
export XTENSA_CORE=nxp_RT500_RI23_11_newlib
Note: On Windows, you can use the ‘setx’ command instead of ‘export’ to set environment variables.
Use the batch/shell script to build out the DSP application from the command-line, in the ‘xcc’ directory.
user@linux:~/SDK/boards/evkmimxrt595/dsp_examples/xaf_record/dsp/xcc$ **./build\_debug.sh** ... [100%] Built target dsp_xaf_record_fusion1.elf
Note: Some warnings during the linking process (floating point ABI) may appear – these are normal and can be ignored.
Launch xt-ocd debugging server (replace topology.xml with your custom version – see section 1.5 of this document):
user@linux:/opt/Tensilica/xocd-14.11$ ./xt-ocd.exe -c topology.xml
Note: If the xt-ocd daemon fails to start, it may be because the DSP has not been initialized by the ARM core which must be done first.
Connect with Xtensa GDB to the device and execute the DSP application:
user@linux:/SDK/boards/evkmimxrt595/dsp_examples/xaf_record/dsp/xcc$ **xt-gdb debug/dsp\_xaf\_demo\_fusion1.elf** GNU gdb (GDB) 7.11.1 Xtensa Tools <VERSION_INFO> ... Reading symbols from debug/dsp_xaf_record_fusion1.elf...done. (xt-gdb) (xt-gdb) **target remote localhost:20000** Remote debugging using localhost:20000 _DoubleExceptionVector () at /home/xpgcust/tree/RI-2023.11/ib/tools/swtools-x86_64-linux/xtensa-elf/src/xos/src/xos_vectors.S:216 216 /home/xpgcust/tree/RI-2023.11/ib/tools/swtools-x86_64-linux/xtensa-elf/src/xos/src/xos_vectors.S: No such file or directory. (xt-gdb) **reset** _ResetVector () at /home/xpgcust/tree/RI-2023.11/ib/tools/swtools-x86_64-linux/xtensa-elf/src/xtos/xea2/reset-vector-xea2.S:71 71 /home/xpgcust/tree/RI-2023.11/ib/tools/swtools-x86_64-linux/xtensa-elf/src/xtos/xea2/reset-vector-xea2.S: No such file or directory. (xt-gdb) **load** Loading section .rtos.rodata, size 0x80 lma 0x200000 Loading section .rodata, size 0x17d50 lma 0x200080 Loading section .text, size 0x633f0 lma 0x217dd0 Loading section .rtos.percpu.data, size 0x4 lma 0x27b1c0 Loading section .data, size 0x110c lma 0x27b1d0 Loading section NonCacheable, size 0x2960 lma 0x20040000 Loading section .Level3InterruptVector.literal, size 0x4 lma 0x24000000 Loading section .DebugExceptionVector.literal, size 0x4 lma 0x24000004 Loading section .NMIExceptionVector.literal, size 0x4 lma 0x24000008 Loading section .ResetVector.text, size 0x13c lma 0x24020000 Loading section .WindowVectors.text, size 0x16c lma 0x24020400 Loading section .Level2InterruptVector.text, size 0x1c lma 0x2402057c Loading section .Level3InterruptVector.text, size 0xc lma 0x2402059c Loading section .DebugExceptionVector.text, size 0xc lma 0x240205bc Loading section .NMIExceptionVector.text, size 0xc lma 0x240205dc Loading section .KernelExceptionVector.text, size 0xc lma 0x240205fc Loading section .UserExceptionVector.text, size 0x18 lma 0x2402061c Loading section .DoubleExceptionVector.text, size 0x8 lma 0x2402063c Start address 0x24020000, load size 520016 Transfer rate: 8 KB/sec, 10612 bytes/write. (xt-gdb) **b main** Breakpoint 1 at 0x21ab5b: file /home/jlydick/mcu-sdk-2.0/boards/src/dsp_examples/xaf_record/dsp/xaf_main_dsp.c, line 366. (xt-gdb) **c** Continuing. Breakpoint 1, main () at /SDK/boards/src/dsp_examples/xaf_record/dsp/xaf_main_dsp.c:366 366 xos_start_main("main", 7, 0); (xt-gdb) **c** Continuing. Initializing... InitializedNote: You can use the gdb command ‘set substitute-path’ to map the missing symbols from the toolchain libraries. For example:
set substitute-path /home/xpgcust/tree/RI-2023.11/ib/tools/swtools-x86_64-linux ~/xtensa/tools/RI-2023.11/XtensaTools.For more details about xt-gdb, see the Cadence GNU Debugger User’s Guide and Cadence Xtensa Debug Guide. These are located at:
~/xtensa/XtDevTools/downloads/RI-2023.11/docs/gnu_gdb_ug.pdf~/xtensa/XtDevTools/downloads/RI-2023.11/docs/xtensa_debug_guide.pdf
Parent topic:Run and Debug from Command-Line Environment / LINUX