lvgl_demo_benchmark

Overview

A demo application runs different functions for benchmark test.

Known issue

The CPU load remains at 100% even during low-intensity tests, confirming that FreeRTOS is not reporting the load correctly.

For all tests that use FreeRTOS, the following macros must be defined, typically at the end of FreeRTOSConfig_Gen.h

workaround code:

#if defined(ICCARM)||defined(__CC_ARM)||defined(GNUC) extern void traceTaskSwitchedOut(void); extern void traceTaskSwitchedIn(void); #endif

#define traceTASK_SWITCHED_IN() traceTaskSwitchedIn() #define traceTASK_SWITCHED_OUT() traceTaskSwitchedOut()

Supported Boards