Hardware requirements#
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
Board settings#
To use EXT PMIC, Please do following Config Changes:
Change J41/J53/J67/J68/J69 Jumper Setting from 1-2 to 2-3
Change J71/J73/J19 Jumper Setting from 1-2 to OPEN
Change J72/J74/J77 Jumper Setting from OPEN to 1-2
DNP R1851,R1853 Populate R1852,R1854
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the pf5020 driver example in the terminal window:
------------------------ PF5020 Functional Block Menu ---------------------------------
Please select the function block you want to run:
[1]. Regulators Setting.
[2]. Clock Setting.
[3]. Enter Standby State.
[4]. Dump Register Value.