MCUXpresso SDK Documentation

Encrypted XIP using BEE (Bus Encryption Engine)

Contents

Encrypted XIP using BEE (Bus Encryption Engine)#

This document extends the documentation of MCUBoot and encrypted XIP in OTA examples and provides an additional information related to the BEE module.

1. Introduction#

BEE is specific for RT10xx (except RT1010) and supports up to two separate regions using two separate AES keys. In the ota examples, BEE region 1 is used for encrypting the execution slot and BEE region 0 is reserved for a bootloader.

BEE configuration blocks are organized as EPRDB (Encrypted Protection Region Descriptor Block), where the EPRDB is encrypted using AES-CBC mode with AES key and IV located in KIB (Key Info Block). The KIB is encrypted as EKIB (Encrypted KIB) using a key provisioned by the user. Each BEE region has its PRDB/KIB pair.

The EKIB is decrypted by a key based on selection in BEE_KEYn_SEL fuse:

  • Software key

    • default value in BEE_KEYn_SEL

    • evaluating BEE without fusing the device

  • SW-GP2

    • fused by user and typically used for offline encryption

    • limited funcionality due hardware bugs, see errata

    • not supported in the examples

  • OTPMK

    • provisioned by NXP in factory

    • unique per device instance - prevents image cloning

    • recommended

Following image shows complete metadata structure used for devices with BEE.

Image

Firmware in execution slot is de/encrypted using AES-CTR combining nonce extracted from PRDB and this device key. The extension automatically detects device key by evaluating BEE_KEYn_SEL fuse.

The whole BEE initialization and encryption metadata handling is resolved in module encrypted_xip_platform_bee.c.

Additional information can be found in Security Reference Manual of target device and in application notes AN12800, AN12852 and AN12901.