Changelog#
All notable changes to NXP Bluetooth LE Host will be documented in this file.
NXP Bluetooth LE Host Stack is certified Bluetooth 6.0
[1.10.20] - mcux v2026-06-00#
Added#
Tire Pressure Monitoring System (TPMS) sample demo applications (KW4x)
Tire Pressure Monitoring System (TPMS) documentation added to DAUG
Localization accelerator LCE support for KW43/MCXW70
Added LE Power Control support in BLE Shell application
LE Read All Remote Features (LLEFS) support in HOST-GAP
LE Channel Assessment (CHAS) Config HCI command support in HOST-GAP
Sensor support enabled on KW43/MCXW70
Improved#
CS procedure auto-loop shell command; improved RAS data drop mechanism
Allow ‘setnumprocs’ 0 for infinite CS procedure repeats
Synchronize code between loc_reader and ncp_loc_reader application files
Subevent interval added to RADE algoritm API
Updated connection handover setup info for FRDM-KW43 in CS application documentations
Documentation updates
Fixed#
L2CAP data fragmentation fix causing inccorect fragmentation over the air
Fix for no valid subevents in localization
Allow sub_mode_type 255 in CS config params
Incorrect connection handle (0 instead of 0xFFFF) for non-connection enhanced notification events
Channel Sounding subevent abort (No CS_SYNC mode0) after rebond
Set ‘preferredPeerAntenna’ based on peer capabilities
Miscellaneous minor application bug fixes
Changed#
Reduced cyclomatic complexity (CCM) in multiple localization functions
Decoupled buttons from LEDs in Bluetooth applications
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23, KW43, MCXW70
[1.10.19] - mcux v2026-06-00-pvw2#
Added#
Support for LE Read All Remote Features after connection is established
Experimental Inline PCT Transfer support for localization sample applications
Support for configurable limits for concurrent Channel Sounding connections/procedures
Improved#
Optimized memory allocation in isp_mciq_ranging_compute for localization applications
Updated RAS loc_reader application for multiple CS connections
Updated handover documentation with broadcast time synchronization details
Documentation updates
Fixed#
Fixed double free issue in L2ca_SendAclDataWithSegmentation
Fixed consecutive CS procedures sustainability issue
Miscellaneous minor application bug fixes
Changed#
CS procedure state management: do not allow new procedure to start before previous one completes
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23, KW43
[1.10.18] - mcux v2026-06-00-pvw1#
Added#
Support for RTT 0 m calibration in applications.
Support for CS Enhancements at Host level:
Inline PCT Transfer
RTT 2M PHY
New connection event ‘gConnEvtRemoteFeaturesRead_c’, providing the peer feature bitmask read via the Read Remote Features procedure
Support for 5 advertising sets in the Bluetooth LE Host
Method to specify GATT handles on the client, avoiding repeated service discovery
Slope calibration algorithm for CS (experimental, disabled by default). Computes distance and quality indicators per antenna path
Handover broadcast time synchronization, allowing one connected anchor to synchronize multiple target anchors simultaneously
Added common configuration header ‘app_localization_config.h’, overridable by the user
Improved#
Updated handling of ‘Procedure_Results_Start’ to correctly process multiple subevents in a single message
Improved CS temperature polling mechanism
BTCS Server now explicitly notifies the PSM channel via ‘AppLocalization_SetPsmChannelId’ upon handover connection
RAS/BTCS clients can disable algorithm execution via ‘gRunAlgo_d’
Updated and cleaned ‘app_preinclude.h’ for sample applications
Documentation and configuration updates for LCE enable/disable
Documentation updates
Miscellaneous minor application bug fixes
Fixed#
If the LE Set Periodic Adv Subevent Data command finishes with an error, use ‘gInternalError_c’ with ‘gLeSetPeriodicAdvSubeventData_c’ as the source and the command complete status as the error code
Correct handling of AddrType values in MonAdvReport generated from XML
Changed#
Removed the Bluetooth LE Host library from the wireless_uart_host project
Disabled use of Random Static Address for all applications except: digital_key_car_anchor and digital_key_car_anchor_cs
Set maximum CS procedure duration to: (procedure interval x connection interval x 2 - 1) slots
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.17] - mcux v2026-03-00#
Added#
Test mode functionality for the Intrusion Detection System
GAP API for HCI LE_Set_Local_Slave_Latency_Enable vendor command
gRasUseNotifOrInd_cto allow configuration of Indication or Notification on RAScs_sync_phyargument tosetcsconfigshell commandsnr_control_initandsnr_control_reflarguments tosetcsprocshell commandDetailed description for
setcsconfigandsetcsproccommand arguments to the CCC w/ CS and Localization applications notesMode0 step information parsing for both RAS and BTCS, made available for the export module
Improved#
ATT Write Commands can now be sent at any time, as per specification
Enhanced CCC and RAS Channel Sounding by incorporating real-time local and remote data decompression
Localization applications now record the PHY used for establishing the connection and incorporate it into the CS procedure parameters configuration
Localization applications keep the
subevtStopIdxfor the remote data and provide it to the algorithmLocalization applications now pass remote mode map to algorithm
Eliminated the dependency on
hci_interface.hin localization filesDocumentation updates
Miscellaneous minor application bug fixes
Fixed#
Wrong data field type in
GAP2GenericEventVendorSpecificDebugFatalErrorLocalization application now processes CS results only when local data is available
Digital key car anchor application issue related to setting the GAP role prior to any use
Error in the definition of a CCC PSM VDBT Version GATT characteristic
Issue with PACKET_NADM byte not being packed correctly into the TOF buffer for mode-3 steps
MISRA fixes
Changed#
Modified linker section names, comments, and RAM layout in the
connectivity.icfandconnectivity_ble_loc.ldfiles for every KW47 and MCXW72 boardSet the default CS submode and default
rtt_typeto 3Set the default radio core speed for the Channel Sounding application to 48 MHz
Localization applications configured to use the extended heap as the final segment of DATA1
Deleted the
gcGapMaximumActiveConnections_cdefinition from applicationsEliminated unused fields related to CS Test Mode
Deleted initializations of range settings that were subsequently overwritten
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.16] - mcux v2026-03-00-pvw2#
Added#
Implemented Bluetooth LE Host Transient Application Key feature (experimental). in ble_shell, loc_reader and loc_user_device
Added Bluetooth LE Host Transient Application Key in ble_shell, loc_reader and loc_user_device
Added Channel Sounding phase calibration, with 0.5m compensation for all boards
Added Vendor Specific Command to enable Link Layer experimental features
Added
gAppCsTimeInfo_ddefine in app_preinclude.h for digital_key_car_anchor_cs on KW47EVKAdded Channel Sounding phase calibration logic and updates in RAS CS Procedure Timing Measurement
Improved#
Updated RADE algorithm source files license description with NXP proprietary license
Improved data logging for digital key application
Updated CCC enumeration values to align with CCC v4.0.0 specification
Updated Intrusion Detection System documentation with event details
Documentation miscellaneous updates
Fixed#
Fixed ranging data body parser on the client side — aborted steps are now counted correctly to prevent subevent misalignment
Fixed handling of CS Procedure Disable at Host and application level
Fixed app_localization timer blocking when sensors were disabled
Fixed setting of
gCsTimeInfo.transferStartfor BTCS Client L2CAP transferRemoved unused
gAppRealTimeDataTransfer_cdefine from digital_key_car_anchor_csRemoved pin_mux files from core1 application projects
Fixed issues in data transfer and event updates related to timing measurement
Changed#
Updated
(SHELL_MAX_ARGS = 20)inapp_preinclude.hfor localization applications.
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.15] – mcux v2026-03-00-pvw1#
Added#
Added an API to update local synchronization parameters after PAwR is already established on the scanner side
Added Connection Subrating feature (experimental) in the Bluetooth LE Host
Added Connection Subrating feature in ble_shell
CCC v4.1.0: renamed DK_VERSION to VDBT_VERSION as per updated specification
Improved#
Improved localization applications timer mechanism to reduce the number of wakeups
Updated localization timeout values to be overridable by the application
Retain the subevent_done_status local and remote values for all subevents and pass them to the algorithm
Documentation miscellaneous updates
Fixed#
Fixed L2CAP credit-based channel disconnection where the channel’s timer ID would be set to 0 instead of gTmrInvalidTimerID_c
Fixed Channel Sounding applications issue: clear the Indication Pending flag for a peer device on disconnect
ble_shell: Set maximum arguments in command (SHELL_MAX_ARGS = 20) in app_preinclude.h
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.14] - mcux v2025-12-00#
Added#
KW47/MCXW72 CCC and IOT Channel Sounding Localization applications on GitHub repository
Monitoring Advertisers support in fsci_black_box and BleShell applications
Local average and remote average RSSI values to the CS measurement report
The “-Os” optimization flag to the ARMGCC release configuration for NCP applications
Improved#
Enabled low power support in loc_reader_host application
Fixed#
loc_reader_host application event set issue
Missing handler for Version2 of the Set RPA Timeout command
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.13] - mcux v2025-12-00-pvw2#
Added#
Threshold for the invalid number of Anchor Monitor events received by the target anchor
Experimental Monitoring Advertisers feature in Bluetooth LE Host
Experimental Randomized RPA feature in Bluetooth LE Host
Application defines for default connection and default advertising tx power
Improved#
Miscellaneous applications updates
Central applications now wait for status of Encrypt procedure in case of bonded device
Logging data on localization applications
NBU Low Power Mode enabled by default for Localization Applications
PCT rotation calibration added to localization apps
Configured CS Reflector to start the CS procedure with the tdm command and updated the documentation
Populated the optionalSubfeaturesSupported field correctly
Prevented CORE 0 from entering deep sleep while LCE is computing by setting the low power mode constraint to PWR_WFI during LCE computation and releasing it afterwards
Implemented in CCC_CS, Channel Sounding data transfer from the anchor to the device
Documentation miscellaneous updates
Updated all kw47 and kw45 armgcc ld linker files to take gUseInternalStorageLink_d flag value into consideration
Fixed#
Memory issue when setting scan response data would return an error status from the LL
Set advertises with the public address, overwritten by a previously used random address on receiving the Advertising Set Terminated event
Changed#
Updated memory configuration: replaced the extended heap area in the available SMU2 memory with a 24KB array in the data1
Removed redundant cached remote capabilities write on reflectors, as the initiator will always trigger a capabilities exchange and trying to write cached capabilities afterwards results in an HCI error
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.12] - mcux v2025-12-00-pvw1#
Added#
Gap_LoadCustomBondedDeviceInformation API to retrieve custom peer information using NVM index
Improved#
Miscellaneous application updates
Fixed#
Updated privacy timeout mechanism affected by LE Set Extended Advertising Enable Command
Changed#
Merged Gap_SetPeriodicAdvParameters and Gap_SetPeriodicAdvParametersV2 into Gap_SetPeriodicAdvParameters
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.11] - mcux v2025-09-00#
Added#
CCC sample applications updated to CCC Digital Key v4.0.0 Specification
RAS/RAP PTS 8.7.4 test support added in Localization Sample applications
Support for CS start procedure while the previous procedure is not completed; old procedure replaced with the new one
Support for arm gcc for ncp_loc_reader__cm33_core1
Improved#
Localization Sample Applications Ram partition
RAS/RAP profile and service
Various sample applications have been updated
Fixed#
Privacy setting issue on ncp_loc_reader
Extended NBU FSCI message handling issue
Ble_shell updated to set the Random Static Address properly
Always set the Advertising Legacy Set handle if the legacy API was used
fsci_bridge and w_uart_host memory leak
PAWR parameters in PeriodicSyncTransferReceived are now parsed correctly
Ensure an RPA/NRPA is properly set from the application to enable a central using Controller Privacy to connect to unbonded peripherals
CS algorithm buffer overwrite issue during Connection Handover application
Various sample applications bug fixes applied
Pass correct Codded PHY (S2) to Channel Sounding Set Procedure Parameters
Changed#
Merged Gap_SetExtAdvertisingParameters and Gap_SetExtAdvertisingParametersV2 into Gap_SetExtAdvertisingParameters
ce_status_buffer type changed to int32_t
BLE_Shell prints Random Static address as identity address instead of the Public Device Address
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.10] - mcux v2025-09-00-pvw2#
Improved#
CS Event Handling: CS (Channel Sounding) events are now sent to the application task for processing, rather than being handled directly in the Host task
Various sample applications have been updated
Fixed#
Bluetooth Advertising Sets: Now supports 4 advertising sets in the Bluetooth host libraries
Various sample applications bug fixes applied
Changed#
Bluetooth Address Type: The default address type has been changed from Public to Random Static
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.9] - mcux v2025-09-00-pvw1#
Added#
IDS event trigger when incoming ATT packets exceed agreed MTU
IDS event trigger when Unexpected SMP Messages received in idle states (before pairing starts)
Average RSSI reporting in Anchor Monitor event
Support for gAppDeferAlgoRun_d in btcs_client.c
Multi-connection monitoring in Handover/Monitor Mode
Improved#
Updated NBU channel sounding applications to support 64MHz clock speed
Cleanup of commComplete structures that only contain status from hci_interface.h
Fixed#
CCC Application handover monitoring RSSI issue
Intrusion Detection System not reporting event type
Extended NBU armgcc projects stability
Advertising Extended Applications when Gap_PeriodicAdvCreateSync fails
Changed#
Updated digital_key_car_anchor applications to configure coding scheme via Host API
Enhanced RAS handling of ACK Ranging Data in invalid conditions
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.8] - mcux v2025-06-00#
Added#
Gap_SetBondedDeviceName() to set device name using NVM index
RAS queue for GATT indications sent
gHciStatusBase_c to csError status
Option to use statically allocated memory for dynamic GATT database (prevents heap fragmentation)
Checks for controller supported features and setting PAST bits accordingly
Anchor support to export device data via RAS using gAppHciDataLogExport_d = 2
Anchor support to export device local HCI data using gAppHciDataLogExport_d = 1
Shell commands to list peer devices and trigger connection handover
Define for enabling optional CCC LE Coded PHY advertising
cs_sync_phy parameter to mDefaultRangeSettings (renamed from outdated RTTPhy)
Improved#
Stack Host now saves the most recently set random address after successful controller response
Miscellaneous minor application updates
Fixed#
Compilation issue in loc_reader app with real-time RAS transfer
CCC application handover state machine race condition
CCC resets gCurrentAdvHandle upon connection
RAS uses correct bit for data overwrite preference
Changed#
Updated Bluetooth LE Host Documentation.
BLE_Shell Tx timer interval adjusted for max throughput on 1M PHY
CS_ConfigVendorCommand updated with Inline Phase Return field
Renamed tx_pwr_phy to phy and removed obsolete rtt_phy field
Updated documentation to clarify Controller Privacy restrictions
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.7] - mcux v2025-06-00-pvw2#
Added#
Support for Bluetooth LE Debug Keys
Support for pairing failure reason 0x10 (Busy)
Extended NBU Wireless_uart_host battery service
Channel Sounding RSSI Information at application level
Application support for 4-antenna configuration
Improved#
Clean include directives
Allow central-only devices to use Gap_EncryptAdvertisingData
CSTACK size optimization for RADE using baremetal apps
Fixed#
Extended NBU memory leak issues
Issues when gAppOtaASyncFlashTransactions_c is set to 0
Issue with CS procedure affected by the CS data export
Extended NBU Wireless_uart_host privacy
Changed#
Updated Bluetooth LE Host Documentation.
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, K32W1
[1.10.6] - mcux v2025-06-00-pvw1#
Added#
Encypted Advertising Data support in Extendded Advertising Applications.
Support for disable UART for CS applications for low power measurements.
Support for LCE (DSPV) non-blocking API integration to RADE.
Intrusion Detection System as Experimental.
Improved#
L2CAP command length validation to cover all signaling commands.
Extended NBU Wireless_uart_host multiple connections support.
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, K32W1
[1.10.5] - mcux v2025-03-00#
Added#
MCXW72 Extended NBU support and w_uart_host, fsci_bridge and ncp_fscibb sample applications.
L2CAP support for Channel Sounding IQ Sample Transfer in CCC CS sample applications.
Bluetooth LE Sample applications for MCX-W71-EVK board.
Changed#
Updated FSCI XML file.
Updated Bluetooth LE Host Documentation.
Fixed#
Cleared the mpRemoteCachedCaps entry when the peer disconnects (CS sample applications).
Transfer RAS subscription data during connection handover (CCC CS sample applications).
EAD - Updated advertising data length check to ensure encrypted data fits inside one AD.
Updated digital_key_car_anchor and digital_key_car_anchor_cs applications to manage Random Static address from the application layer.
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, K32W1
[1.10.4] - mcux v2025-03-00-pvw2#
Added#
PAWR support in BLE Shell sample application.
PAWR support in adv_ext_peripheral and adv_ext_central sample applications.
New sample applications for FRDM-MCXW72.
Gap_SetScanningCallback API.
Support for handover connection interval update command.
Changed#
Updated HID Device for Windows 11 compatibility.
Updated CCC demos to Digital Key R4 spec version 1.0.0.
Improved RPA resolution at the Host level, now performed synchronously.
Enhanced parsing of the CS procedure in Ranging Service.
Fixed#
Corrected parsing of the PAST command in FSCI GAP.
Fixed scan event reporting in PAST scenario.
Added an error case for
Gap_SetChannelMapin the generic event handler.
Supported Platforms#
KW45, KW47, MCXW71, MCXW72, K32W1