MCUXpresso SDK Changelog#
Board Support Files#
board#
[25.06.00]#
Initial version
clock_config#
[25.06.00]#
Initial version
pin_mux#
[25.06.00]#
Initial version
ACMP#
[2.5.0]#
New Feature
Supported the plateforms which don’t have continuous mode.
[2.4.0]#
New Feature
Supported the plateforms which don’t have continuous mode.
[2.3.0]#
Improvements
Expose C0 register FILTER_CNT bitfield and FPR bitfield to the user.
[2.2.0]#
Improvements
Updated feature macros for roundrobin mode, window mode, filter mode, and 3V domain removes.
[2.1.0]#
New Feature
Supported the plateforms which don’t have hysteresis mode.
[2.0.6]#
Bug Fixes
Fixed the wrong comments, the DAC value should range from 0 to 255.
[2.0.5]#
Bug Fixes
Fixed the out-of-bounds error of Coverity caused by missing an assert sentence to avoid the return value of ACMP_GetInstance() exceeding the array bounds.
Fixed the violations of MISRA C-2012 rules:
Rule 10.1, 14.4, 16.4, 17.7.
[2.0.4]#
Bug Fixes
Avoided changing w1c bit in ACMP_SetRoundRobinPreState().
[2.0.3]#
New Features
Added feature functions for usage of different power domains(1.8 V and 3 V). These functions are first enabled in ULP1. They are about:
ACMP_EnableLinkToDAC()
ACMP_SetDiscreteModeConfig()
ACMP_GetDefaultDiscreteModeConfig()
[2.0.2]#
Other Changes
Changed coding style of peripheral base address from “s_acmpBases” to “s_acmpBase”.
[2.0.1]#
Bug Fixes
Fixed bug regarding the function “ACMP_SetRoundRobinConfig”. It will not continue execution but returns directly after disabling round robin mode.
ADC12#
[2.0.8]#
Bug Fixes
Fix build warning when
FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROLis defined as 1.
[2.0.7]#
Improvements
Change the method for judging the end of calibration. Previously, it was judged based on the COCO bit of the SC1 register. After the update, it is judged based on the CAL bit of the SC3 register. In some cases, SC1[COCO] was already set to 1 before calibration was performed, which caused calibration to fail.
[2.0.6]#
Improvements
Removed useless comments of ADC12_DoAutoCalibration() function.
[2.0.5]#
Bug Fixes
Fixed the violations of MISRA C-2012 rule 10.4.
[2.0.4]#
Bug Fixes
Fixed the violations of MISRA C-2012 rules:
Rule 4.7 10.1 10.3 10.4 10.8 12.2 16.4 17.7
[2.0.3]#
Improvements
Used conversion control feature macro instead of that in IO map.
[2.0.2]#
Bug Fixes
Set ADC clock frequency as half of the maximum value for calibration.
[2.0.1]#
New Features
Added a feature to control enablement of DMA.
[2.0.0]#
Initial version.
CLOCK#
[2.0.0]#
Initial version.
COMMON#
[2.6.7]#
Improvements
EnableIRQ/DisableIRQ: Use IRQSTEER_GetInstIdxByIRQ() to determine IRQSTEER instance index instead of simple division. Supports multiple IRQSTEER instances with different interrupt counts.
[2.6.6]#
Improvements
Support Cortex M55.
[2.6.5]#
Bug Fixes
Fixed the issue that the function SDK_DelayAtLeastUs may underflow and cause a long delay when the input parameter is small and the system clock is low.
[2.6.4]#
New Features
Add macros to tag deprecated features and experimental features.
[2.6.3]#
New Features
Added bit mask inversion macros to avoid type promotion.
Added register operation macros.
Improvements
Make function
MSDK_EnableCpuCycleCountercompatible with CMSIS-5 and CMSIS-6.
Bug Fixes
Fixed build issue of CMSIS PACK BSP example caused by CMSIS 6.1 issue.
[2.6.2]#
Bug Fixes
Fixed violations of MISRA C-2012 rule for implicit conversions in boolean contexts
[2.6.1]#
Improvements
Support Cortex M23.
[2.6.0]#
Bug Fixes
Fix CERT-C violations.
[2.5.0]#
New Features
Added new APIs InitCriticalSectionMeasurementContext, DisableGlobalIRQEx and EnableGlobalIRQEx so that user can measure the execution time of the protected sections.
[2.4.3]#
Improvements
Enable irqs that mount under irqsteer interrupt extender.
[2.4.2]#
Improvements
Add the macros to convert peripheral address to secure address or non-secure address.
[2.4.1]#
Improvements
Improve for the macro redefinition error when integrated with zephyr.
[2.4.0]#
New Features
Added EnableIRQWithPriority, IRQ_SetPriority, and IRQ_ClearPendingIRQ for ARM.
Added MSDK_EnableCpuCycleCounter, MSDK_GetCpuCycleCount for ARM.
[2.3.3]#
New Features
Added NETC into status group.
[2.3.2]#
Improvements
Make driver aarch64 compatible
[2.3.1]#
Bug Fixes
Fixed MAKE_VERSION overflow on 16-bit platforms.
[2.3.0]#
Improvements
Split the driver to common part and CPU architecture related part.
[2.2.10]#
Bug Fixes
Fixed the ATOMIC macros build error in cpp files.
[2.2.9]#
Bug Fixes
Fixed MISRA C-2012 issue, 5.6, 5.8, 8.4, 8.5, 8.6, 10.1, 10.4, 17.7, 21.3.
Fixed SDK_Malloc issue that not allocate memory with required size.
[2.2.8]#
Improvements
Included stddef.h header file for MDK tool chain.
New Features:
Added atomic modification macros.
[2.2.7]#
Other Change
Added MECC status group definition.
[2.2.6]#
Other Change
Added more status group definition.
Bug Fixes
Undef __VECTOR_TABLE to avoid duplicate definition in cmsis_clang.h
[2.2.5]#
Bug Fixes
Fixed MISRA C-2012 rule-15.5.
[2.2.4]#
Bug Fixes
Fixed MISRA C-2012 rule-10.4.
[2.2.3]#
New Features
Provided better accuracy of SDK_DelayAtLeastUs with DWT, use macro SDK_DELAY_USE_DWT to enable this feature.
Modified the Cortex-M7 delay count divisor based on latest tests on RT series boards, this setting lets result be closer to actual delay time.
[2.2.2]#
New Features
Added include RTE_Components.h for CMSIS pack RTE.
[2.2.1]#
Bug Fixes
Fixed violation of MISRA C-2012 Rule 3.1, 10.1, 10.3, 10.4, 11.6, 11.9.
[2.2.0]#
New Features
Moved SDK_DelayAtLeastUs function from clock driver to common driver.
[2.1.4]#
New Features
Added OTFAD into status group.
[2.1.3]#
Bug Fixes
MISRA C-2012 issue fixed.
Fixed the rule: rule-10.3.
[2.1.2]#
Improvements
Add SUPPRESS_FALL_THROUGH_WARNING() macro for the usage of suppressing fallthrough warning.
[2.1.1]#
Bug Fixes
Deleted and optimized repeated macro.
[2.1.0]#
New Features
Added IRQ operation for XCC toolchain.
Added group IDs for newly supported drivers.
[2.0.2]#
Bug Fixes
MISRA C-2012 issue fixed.
Fixed the rule: rule-10.4.
[2.0.1]#
Improvements
Removed the implementation of LPC8XX Enable/DisableDeepSleepIRQ() function.
Added new feature macro switch “FSL_FEATURE_HAS_NO_NONCACHEABLE_SECTION” for specific SoCs which have no noncacheable sections, that helps avoid an unnecessary complex in link file and the startup file.
Updated the align(x) to attribute(aligned(x)) to support MDK v6 armclang compiler.
[2.0.0]#
Initial version.
CRC#
[2.1.0]#
Bug fix:
Choosing CRC clocks from CRC clock array according to instance instead of hardcoded value.
[2.0.5]#
Bug fix:
Fix CERT-C issue with boolean-to-unsigned integer conversion.
[2.0.4]#
Improvements
Release peripheral from reset if necessary in init function.
[2.0.3]#
Bug fix:
Fix MISRA issues.
[2.0.2]#
Bug fix:
Fix MISRA issues.
[2.0.1]#
Bug fix:
DATA and DATALL macro definition moved from header file to source file.
[2.0.0]#
Initial version.
DMAMUX#
[2.1.4]#
Bug Fixes
Fixed CERT INT31-C violation in DMAMUX_SetSource by adding non-negative assertion and explicit cast.
[2.1.3]#
Improvements
Wrap DMAMUX_GetInstance into FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL to avoid build issues.
[2.1.2]#
Bug Fixes
Add macro FSL_DMAMUX_CHANNEL_NUM to calculat correct DMAMUX channel number when input EDAM channel number.
[2.1.1]#
Improvements
Add macro FSL_FEATURE_DMAMUX_CHANNEL_NEEDS_ENDIAN_CONVERT and DMAMUX_CHANNEL_ENDIAN_CONVERTn do channel endian convert.
[2.1.0]#
Improvements
Modify the type of parameter source from uint32_t to int32_t in the DMAMUX_SetSource.
[2.0.5]#
Improvements
Added feature FSL_FEATURE_DMAMUX_CHCFG_REGISTER_WIDTH for the difference of CHCFG register width.
[2.0.4]#
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.4.
[2.0.3]#
Bug Fixes
Fixed the issue for MISRA-2012 check.
Fixed rule 10.4 and rule 10.3.
[2.0.2]#
New Features
Added an always-on enable feature to a DMA channel for ULP1 DMAMUX support.
[2.0.1]#
Bug Fixes
Fixed the build warning issue by changing the type of parameter source from uint8_t to uint32_t when setting DMA request source in DMAMUX_SetSourceChange.
[2.0.0]#
Initial version.
EDMA#
[2.4.9]#
Bug Fixes
Fixed CERT INT31-C and INT30-C violations in edma driver.
[2.4.8]#
New Features
Added common IRQ handler entry EDMA_DriverIRQHandler.
[2.4.7]#
Bug Fixes
Fixed coverity MSG issues with CERT INT31-C compliance.
[2.4.6]#
Bug Fixes
Fixed the EDMA header index retrieval error caused by done bit calculation mistake issue.
[2.4.5]#
Bug Fixes
Fixed memory convert would convert NULL as zero address issue.
[2.4.4]#
Bug Fixes
Fixed comments by replacing STCD with TCD
Fixed the TCD overwrite issue when submit transfer request in the callback if there is a active TCD in hardware.
Fixed violations of MISRA C-2012 rule 10.8,5.6.
[2.4.3]#
Improvements
Added FSL_FEATURE_MEMORY_HAS_ADDRESS_OFFSET to convert the address between system mapped address and dma quick access address.
Bug Fixes
Fixed the wrong tcd done count calculated in first TCD interrupt for the non scatter gather case.
[2.4.2]#
Bug Fixes
Fixed the wrong tcd done count calculated in first TCD interrupt by correct the initial value of the header.
Fixed violations of MISRA C-2012 rule 10.3, 10.4.
[2.4.1]#
Bug Fixes
Added clear CITER and BITER registers in EDMA_AbortTransfer to make sure the TCD registers in a correct state for next calling of EDMA_SubmitTransfer.
Removed the clear DONE status for ESG not enabled case to aovid DONE bit cleared unexpectedly.
[2.4.0]#
Improvements
Added api EDMA_EnableContinuousChannelLinkMode to support continuous link mode.
Added apis EDMA_SetMajorOffsetConfig/EDMA_TcdSetMajorOffsetConfig to support major loop address offset feature.
Added api EDMA_EnableChannelMinorLoopMapping for minor loop offset feature.
Removed the reduntant IRQ Handler in edma driver.
[2.3.2]#
Improvements
Fixed HIS ccm issue in function EDMA_PrepareTransferConfig.
Fixed violations of MISRA C-2012 rule 11.6, 10.7, 10.3, 18.1.
Bug Fixes
Added ACTIVE & BITER & CITER bitfields to determine the channel status to fixed the issue of the transfer request cannot submit by function EDMA_SubmitTransfer when channel is idle.
[2.3.1]#
Improvements
Added source/destination address alignment check.
Added driver IRQ handler support for multi DMA instance in one SOC.
[2.3.0]#
Improvements
Added new api EDMA_PrepareTransferConfig to allow different configurations of width and offset.
Bug Fixes
Fixed violations of MISRA C-2012 rule 10.4, 10.1.
Fixed the Coverity issue regarding out-of-bounds write.
[2.2.0]#
Improvements
Added peripheral-to-peripheral support in EDMA driver.
[2.1.9]#
Bug Fixes
Fixed MISRA issue: Rule 10.7 and 10.8 in function EDMA_DisableChannelInterrupts and EDMA_SubmitTransfer.
Fixed MISRA issue: Rule 10.7 in function EDMA_EnableAsyncRequest.
[2.1.8]#
Bug Fixes
Fixed incorrect channel preemption base address used in EDMA_SetChannelPreemptionConfig API which causes incorrect configuration of the channel preemption register.
[2.1.7]#
Bug Fixes
Fixed incorrect transfer size setting.
Added 8 bytes transfer configuration and feature for RT series;
Added feature to support 16 bytes transfer for Kinetis.
Fixed the issue that EDMA_HandleIRQ would go to incorrect branch when TCD was not used and callback function not registered.
[2.1.6]#
Bug Fixes
Fixed KW3X MISRA Issue.
Rule 14.4, 10.8, 10.4, 10.7, 10.1, 10.3, 13.5, and 13.2.
Improvements
Cleared the IRQ handler unavailable for specific platform with macro FSL_FEATURE_EDMA_MODULE_CHANNEL_IRQ_ENTRY_SHARED_OFFSET.
[2.1.5]#
Improvements
Improved EDMA IRQ handler to support half interrupt feature.
[2.1.4]#
Bug Fixes
Cleared enabled request, status during EDMA_Init for the case that EDMA is halted before reinitialization.
[2.1.3]#
Bug Fixes
Added clear DONE bit in IRQ handler to avoid overwrite TCD issue.
Optimized above solution for the case that transfer request occurs in callback.
[2.1.2]#
Improvements
Added interface to get next TCD address.
Added interface to get the unused TCD number.
[2.1.1]#
Improvements
Added documentation for eDMA data flow when scatter/gather is implemented for the EDMA_HandleIRQ API.
Updated and corrected some related comments in the EDMA_HandleIRQ API and edma_handle_t struct.
[2.1.0]#
Improvements
Changed the EDMA_GetRemainingBytes API into EDMA_GetRemainingMajorLoopCount due to eDMA IP limitation (see API comments/note for further details).
[2.0.5]#
Improvements
Added pubweak DriverIRQHandler for K32H844P (16 channels shared).
[2.0.4]#
Improvements
Added support for SoCs with multiple eDMA instances.
Added pubweak DriverIRQHandler for KL28T DMA1 and MCIMX7U5_M4.
[2.0.3]#
Bug Fixes
Fixed the incorrect pubweak IRQHandler name issue, which caused re-definition build errors when client set his/her own IRQHandler, by changing the 32-channel IRQHandler name to DriverIRQHandler.
[2.0.2]#
Bug Fixes
Fixed incorrect minorLoopBytes type definition in _edma_transfer_config struct, and defined minorLoopBytes as uint32_t instead of uint16_t.
[2.0.1]#
Bug Fixes
Fixed the eDMA callback issue (which did not check valid status) in EDMA_HandleIRQ API.
[2.0.0]#
Initial version.
EWM#
[2.0.4]#
Bug Fixes
Fixed CERT INT31-C violations.
[2.0.3]#
Bug Fixes
Fixed violation of MISRA C-2012 rules: 10.1, 10.3.
[2.0.2]#
Bug Fixes
Fixed violation of MISRA C-2012 rules: 10.3, 10.4.
[2.0.1]#
Bug Fixes
Fixed the hard fault in EWM_Deinit.
[2.0.0]#
Initial version.
FLASH#
[3.3.0]#
New Feature
Support for EEPROM Quick Write on devices with FTFC
[3.2.0]#
New Feature
Basic support for FTFC
[3.1.3]#
New Feature
Support 512KB flash for Kinetis E serials.
[3.1.2]#
Bug Fixes — Remove redundant comments.
[3.1.1]#
Bug Fixes — MISRA C-2012 issue fixed: rule 10.3
[3.1.0]#
New Feature
Support erase flash asynchronously.
[3.0.2]#
Bug Fixes — MISRA C-2012 issue fixed: rule 8.4, 17.7, 10.4, 16.1, 21.15, 11.3, 10.7 — building warning -Wnull-dereference on arm compiler v6
[3.0.1]#
New Features
Added support FlexNVM alias for (kw37/38/39).
[3.0.0]#
Improvements
Reorganized FTFx flash driver source file.
Extracted flash cache driver from FTFx driver.
Extracted flexnvm flash driver from FTFx driver.
[2.3.1]#
Bug Fixes
Unified Flash IFR design from K3.
New encoding rule for K3 flash size.
[2.3.0]#
New Features
Added support for device with LP flash (K3S/G).
Added flash prefetch speculation APIs.
Improvements
Refined flash_cache_clear function.
Reorganized the member of flash_config_t struct.
[2.2.0]#
New Features
Supported FTFL device in FLASH_Swap API.
Supported various pflash start addresses.
Added support for KV58 in cache clear function.
Added support for device with secondary flash (KW40).
Bug Fixes
Compiled execute-in-ram functions as PIC binary code for driver use.
Added missed flexram properties.
Fixed unaligned variable issue for execute-in-ram function code array.
[2.1.0]#
Improvements
Updated coding style to align with KSDK 2.0.
Different-alignment-size support for pflash and flexnvm.
Improved the implementation of execute-in-ram functions.
[2.0.0]#
Initial version
FLEXIO#
[2.3.2]#
Bug Fixes
Fixed MISRA 10.4 issues.
[2.3.1]#
New Features
Added common IRQ handler entry FLEXIO_CommonDriverIRQHandler.
[2.3.0]#
Improvements
Supported platforms which don’t have DOZE mode control.
Added more pin control functions.
[2.2.3]#
Improvements
Adapter the FLEXIO driver to platforms which don’t have system level interrupt controller, such as NVIC.
[2.2.2]#
Improvements
Release peripheral from reset if necessary in init function.
[2.2.1]#
Improvements
Added doxygen index parameter comment in FLEXIO_SetClockMode.
[2.2.0]#
New Features
Added new APIs to support FlexIO pin register.
[2.1.0]#
Improvements
Added API FLEXIO_SetClockMode to set flexio channel counter and source clock.
[2.0.4]#
Bug Fixes
Fixed MISRA 8.4 issues.
[2.0.3]#
Bug Fixes
Fixed MISRA 10.4 issues.
[2.0.2]#
Improvements
Split FLEXIO component which combines all flexio/flexio_uart/flexio_i2c/flexio_i2s drivers into several components: FlexIO component, flexio_uart component, flexio_i2c_master component, and flexio_i2s component.
Bug Fixes
Fixed MISRA issues
Fixed rules 10.1, 10.3, 10.4, 10.7, 11.6, 11.9, 14.4, 17.7.
[2.0.1]#
Bug Fixes
Fixed the dozen mode configuration error in FLEXIO_Init API. For enableInDoze = true, the configuration should be 0; for enableInDoze = false, the configuration should be 1.
FLEXIO_I2C#
[2.6.3]#
Bug Fixes
Fixed MISRA 10.4, 10.7 and 14.4 issues.
[2.6.2]#
Improvements
Added timeout for while loop in FLEXIO_I2C_MasterTransferBlocking().
Bug Fixes
Fixed build issues related to I2C_RETRY_TIMES.
[2.6.1]#
Bug Fixes
Fixed coverity issues
[2.6.0]#
Improvements
Supported platforms which don’t have DOZE mode control.
[2.5.1]#
Improvements
Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.
[2.5.0]#
Improvements
Split some functions, fixed CCM problem in file fsl_flexio_i2c_master.c.
[2.4.0]#
Improvements
Added delay of 1 clock cycle in FLEXIO_I2C_MasterTransferRunStateMachine to ensure that bus would be idle before next transfer if master is nacked.
Fixed issue that the restart setup time is less than the time in I2C spec by adding delay of 1 clock cycle before restart signal.
[2.3.0]#
Improvements
Used 3 timers instead of 2 to support transfer which is more than 14 bytes in single transfer.
Improved FLEXIO_I2C_MasterTransferGetCount so that the API can check whether the transfer is still in progress.
Bug Fixes
Fixed MISRA 10.4 issues.
[2.2.0]#
New Features
Added timeout mechanism when waiting certain state in transfer API.
Added an API for checking bus pin status.
Bug Fixes
Fixed COVERITY issue of useless call in FLEXIO_I2C_MasterTransferRunStateMachine.
Fixed MISRA issues
Fixed rules 10.1, 10.3, 10.4, 10.7, 11.6, 11.9, 14.4, 17.7.
Added codes in FLEXIO_I2C_MasterTransferCreateHandle to clear pending NVIC IRQ, disable internal IRQs before enabling NVIC IRQ.
Modified code so that during master’s nonblocking transfer the start and slave address are sent after interrupts being enabled, in order to avoid potential issue of sending the start and slave address twice.
[2.1.7]#
Bug Fixes
Fixed the issue that FLEXIO_I2C_MasterTransferBlocking did not wait for STOP bit sent.
Fixed COVERITY issue of useless call in FLEXIO_I2C_MasterTransferRunStateMachine.
Fixed the issue that I2C master did not check whether bus was busy before transfer.
[2.1.6]#
Bug Fixes
Fixed the issue that I2C Master transfer APIs(blocking/non-blocking) did not support the situation of master transfer with subaddress and transfer data size being zero, which means no data followed the subaddress.
[2.1.5]#
Improvements
Unified component full name to FLEXIO I2C Driver.
[2.1.4]#
Bug Fixes
The following modifications support FlexIO using multiple instances:
Removed FLEXIO_Reset API in module Init APIs.
Updated module Deinit APIs to reset the shifter/timer config instead of disabling module/clock.
Updated module Enable APIs to only support enable operation.
[2.1.3]#
Improvements
Changed the prototype of FLEXIO_I2C_MasterInit to return kStatus_Success if initialized successfully or to return kStatus_InvalidArgument if “(srcClock_Hz / masterConfig->baudRate_Bps) / 2 - 1” exceeds 0xFFU.
[2.1.2]#
Bug Fixes
Fixed the FLEXIO I2C issue where the master could not receive data from I2C slave in high baudrate.
Fixed the FLEXIO I2C issue where the master could not receive NAK when master sent non-existent addr.
Fixed the FLEXIO I2C issue where the master could not get transfer count successfully.
Fixed the FLEXIO I2C issue where the master could not receive data successfully when sending data first.
Fixed the Dozen mode configuration error in FLEXIO_I2C_MasterInit API. For enableInDoze = true, the configuration should be 0; for enableInDoze = false, the configuration should be 1.
Fixed the issue that FLEXIO_I2C_MasterTransferBlocking API called FLEXIO_I2C_MasterTransferCreateHandle, which lead to the s_flexioHandle/s_flexioIsr/s_flexioType variable being written. Then, if calling FLEXIO_I2C_MasterTransferBlocking API multiple times, the s_flexioHandle/s_flexioIsr/s_flexioType variable would not be written any more due to it being out of range. This lead to the following situation: NonBlocking transfer APIs could not work due to the fail of register IRQ.
[2.1.1]#
Bug Fixes
Implemented the FLEXIO_I2C_MasterTransferBlocking API which is defined in header file but has no implementation in the C file.
[2.1.0]#
New Features
Added Transfer prefix in transactional APIs.
Added transferSize in handle structure to record the transfer size.
FLEXIO_I2S#
[2.2.2]#
Bug Fixes
Fixed violations of MISRA C-2012 rule 12.4.
[2.2.1]#
Improvements
Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.
[2.2.0]#
New Features
Added timeout mechanism when waiting certain state in transfer API.
Bug Fixes
Fixed IAR Pa082 warnings.
Fixed violations of the MISRA C-2012 rules 10.4, 14.4, 11.8, 11.9, 10.1, 17.7, 11.6, 10.3, 10.7.
[2.1.6]#
Bug Fixes
Added reset flexio before flexio i2s init to make sure flexio status is normal.
[2.1.5]#
Bug Fixes
Fixed the issue that I2S driver used hard code for bitwidth setting.
[2.1.4]#
Improvements
Unified component’s full name to FLEXIO I2S (DMA/EDMA) driver.
[2.1.3]#
Bug Fixes
The following modifications support FLEXIO using multiple instances:
Removed FLEXIO_Reset API in module Init APIs.
Updated module Deinit APIs to reset the shifter/timer config instead of disabling module/clock.
Updated module Enable APIs to only support enable operation.
[2.1.2]#
New Features
Added configure items for all pin polarity and data valid polarity.
Added default configure for pin polarity and data valid polarity.
[2.1.1]#
Bug Fixes
Fixed FlexIO I2S RX data read error and eDMA address error.
Fixed FlexIO I2S slave timer compare setting error.
[2.1.0]#
New Features
Added Transfer prefix in transactional APIs.
Added transferSize in handle structure to record the transfer size.
FLEXIO_I2S_EDMA#
[2.1.9]#
Bug Fixes
Fixed violations of MISRA C-2012 rule 12.4.
[2.1.8]#
Improvements
Applied EDMA ERRATA 51327.
FLEXIO_SPI#
[2.4.4]#
Bug Fixes
Fixed MISRA 10.4 issues.
[2.4.3]#
Improvements
Make SPI_RETRY_TIMES configurable by CONFIG_SPI_RETRY_TIMES.
[2.4.2]#
Bug Fixes
Fixed
FLEXIO_SPI_MasterTransferBlockingandFLEXIO_SPI_MasterTransferNonBlockingissue in CS continuous mode, the CS might not be continuous.
[2.4.1]#
Bug Fixes
Fixed coverity issues
[2.4.0]#
Improvements
Supported platforms which don’t have DOZE mode control.
[2.3.5]#
Improvements
Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.
[2.3.4]#
Bug Fixes
Fixed the txData from void * to const void * in transmit API
[2.3.3]#
Bugfixes
Fixed cs-continuous mode.
[2.3.2]#
Improvements
Changed FLEXIO_SPI_DUMMYDATA to 0x00.
[2.3.1]#
Bugfixes
Fixed IRQ SHIFTBUF overrun issue when one FLEXIO instance used as multiple SPIs.
[2.3.0]#
New Features
Supported FLEXIO_SPI slave transfer with continuous master CS signal and CPHA=0.
Supported FLEXIO_SPI master transfer with continuous CS signal.
Support 32 bit transfer width.
Bug Fixes
Fixed wrong timer compare configuration for dma/edma transfer.
Fixed wrong byte order of rx data if transfer width is 16 bit, since the we use shifter buffer bit swapped/byte swapped register to read in received data, so the high byte should be read from the high bits of the register when MSB.
[2.2.1]#
Bug Fixes
Fixed bug in FLEXIO_SPI_MasterTransferAbortEDMA that when aborting EDMA transfer EDMA_AbortTransfer should be used rather than EDMA_StopTransfer.
[2.2.0]#
Improvements
Added timeout mechanism when waiting certain states in transfer driver.
Bug Fixes
Fixed MISRA 10.4 issues.
Added codes in FLEXIO_SPI_MasterTransferCreateHandle and FLEXIO_SPI_SlaveTransferCreateHandle to clear pending NVIC IRQ before enabling NVIC IRQ, to fix issue of pending IRQ interfering the on-going process.
[2.1.3]#
Improvements
Unified component full name to FLEXIO SPI(DMA/EDMA) Driver.
Bug Fixes
Fixed MISRA issues
Fixed rules 10.1, 10.3, 10.4, 10.7, 11.6, 11.9, 14.4, 17.7.
[2.1.2]#
Bug Fixes
The following modification support FlexIO using multiple instances:
Removed FLEXIO_Reset API in module Init APIs.
Updated module Deinit APIs to reset the shifter/timer config instead of disabling module/clock.
Updated module Enable APIs to only support enable operation.
[2.1.1]#
Bug Fixes
Fixed bug where FLEXIO SPI transfer data is in 16 bit per frame mode with eDMA.
Fixed bug when FLEXIO SPI works in eDMA and interrupt mode with 16-bit per frame and Lsbfirst.
Fixed the Dozen mode configuration error in FLEXIO_SPI_MasterInit/FLEXIO_SPI_SlaveInit API. For enableInDoze = true, the configuration should be 0; for enableInDoze = false, the configuration should be 1.
Improvements
Added #ifndef/#endif to allow users to change the default TX value at compile time.
[2.1.0]#
New Features
Added Transfer prefix in transactional APIs.
Added transferSize in handle structure to record the transfer size.
Bug Fixes
Fixed the error register address return for 16-bit data write in FLEXIO_SPI_GetTxDataRegisterAddress.
Provided independent IRQHandler/transfer APIs for Master and slave to fix the baudrate limit issue.
FLEXIO_UART#
[2.6.5]#
Bug Fixes
Fixed MISRA 10.4 issues.
[2.6.4]#
Improvements
Make UART_RETRY_TIMES configurable by CONFIG_UART_RETRY_TIMES.
[2.6.3]#
Bug Fixes
Fixed coverity issues
[2.6.2]#
Bug Fixes
Fixed coverity issues
[2.6.1]#
Improvements
Improve baudrate calculation method, to support higher frequency FlexIO clock source.
[2.6.0]#
Improvements
Supported platforms which don’t have DOZE mode control.
[2.5.1]#
Improvements
Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.
[2.5.0]#
Improvements
Added API FLEXIO_UART_FlushShifters to flush UART fifo.
[2.4.0]#
Improvements
Use separate data for TX and RX in flexio_uart_transfer_t.
Bug Fixes
Fixed bug that when ring buffer is used, if some data is received in ring buffer first before calling FLEXIO_UART_TransferReceiveNonBlocking, the received data count returned by FLEXIO_UART_TransferGetReceiveCount is wrong.
[2.3.0]#
Improvements
Added check for baud rate’s accuracy that returns kStatus_FLEXIO_UART_BaudrateNotSupport when the best achieved baud rate is not within 3% error of configured baud rate.
Bug Fixes
Added codes in FLEXIO_UART_TransferCreateHandle to clear pending NVIC IRQ before enabling NVIC IRQ, to fix issue of pending IRQ interfering the on-going process.
[2.2.0]#
Improvements
Added timeout mechanism when waiting for certain states in transfer driver.
Bug Fixes
Fixed MISRA 10.4 issues.
[2.1.6]#
Bug Fixes
Fixed IAR Pa082 warnings.
Fixed MISRA issues
Fixed rules 10.1, 10.3, 10.4, 10.7, 11.6, 11.9, 14.4, 17.7.
[2.1.5]#
Improvements
Triggered user callback after all the data in ringbuffer were received in FLEXIO_UART_TransferReceiveNonBlocking.
[2.1.4]#
Improvements
Unified component full name to FLEXIO UART(DMA/EDMA) Driver.
[2.1.3]#
Bug Fixes
The following modifications support FLEXIO using multiple instances:
Removed FLEXIO_Reset API in module Init APIs.
Updated module Deinit APIs to reset the shifter/timer configuration instead of disabling module and clock.
Updated module Enable APIs to only support enable operation.
[2.1.2]#
Bug Fixes
Fixed the transfer count calculation issue in FLEXIO_UART_TransferGetReceiveCount, FLEXIO_UART_TransferGetSendCount, FLEXIO_UART_TransferGetReceiveCountDMA, FLEXIO_UART_TransferGetSendCountDMA, FLEXIO_UART_TransferGetReceiveCountEDMA and FLEXIO_UART_TransferGetSendCountEDMA.
Fixed the Dozen mode configuration error in FLEXIO_UART_Init API. For enableInDoze = true, the configuration should be 0; for enableInDoze = false, the configuration should be 1.
Added code to report errors if the user sets a too-low-baudrate which FLEXIO cannot reach.
Disabled FLEXIO_UART receive interrupt instead of all NVICs when reading data from ring buffer. If ring buffer is used, receive nonblocking will disable all NVIC interrupts to protect the ring buffer. This had negative effects on other IPs using interrupt.
[2.1.1]#
Bug Fixes
Changed the API name FLEXIO_UART_StopRingBuffer to FLEXIO_UART_TransferStopRingBuffer to align with the definition in C file.
[2.1.0]#
New Features
Added Transfer prefix in transactional APIs.
Added txSize/rxSize in handle structure to record the transfer size.
Bug Fixes
Added an error handle to handle the situation that data count is zero or data buffer is NULL.
FLEXIO_UART_EDMA#
[2.3.1]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules.
[2.3.0]#
Refer FLEXIO_UART driver change log to 2.3.0
FTM#
[2.7.6]#
Bug Fixes
Fixed QUADEN bit not cleared in FTM_SetupPwm() and FTM_SetupPwmMode() when switching from quadrature decoder mode to PWM mode. QUADEN has higher priority and overrides PWM operation if left set.
Improvements
Added support for devices with reduced FTM register set by introducing new feature macros:
FSL_FEATURE_FTM_HAS_NO_COMBINE_COMBINE1: COMBINE register has no per-pair grouping.FSL_FEATURE_FTM_HAS_NO_COMBINE_FAULTEN: COMBINE register has no FAULTEN field.FSL_FEATURE_FTM_HAS_NO_MODE_FAULTM: MODE register has no FAULTM field.FSL_FEATURE_FTM_HAS_NO_MODE_FAULTIE: MODE register has no FAULTIE field.FSL_FEATURE_FTM_HAS_NO_FLTCTRL: FLTCTRL register is not present.FSL_FEATURE_FTM_HAS_NO_FMS_FAULTF: FMS register has no FAULTF field.
Added assert checks to detect unsupported channel pair numbers on devices where COMBINE has no per-pair grouping (only pair 0 is valid).
[2.7.5]#
Bug Fixes
Corrected the bit shift calculation for fault input filter enable in FTM_SetupFaultInput().
[2.7.4]#
Bug Fixes
Fixed violations of the CERT INT31-C.
Fixed MISRA C-2012 issue: rule 10.1.
[2.7.3]#
Bug Fixes
Fixed violations of the CERT INT30-C INT31-C.
[2.7.2]#
Improvements
Add API
FTM_ERRATA_010856for ERR010856 workaround.
[2.7.1]#
Bug Fixes
Added function macro when accsee FLTCTRL register FSTATE bit to prevent access nonexistent register.
Added function macro to prevent access nonexistent FTM channel for API FTM_ConfigSinglePWM() and FTM_ConfigCombinePWM().
[2.7.0]#
Improvements
Support period dithering and edge dithering feature with new APIs:
FTM_SetPeriodDithering()
FTM_SetEdgeDithering()
Support get channel n output and input state feature with new APIs:
FTM_GetChannelOutputState()
FTM_GetChannelInputState()
Support configure deadtime for specific combined channel pair with new API:
FTM_SetPairDeadTime()
Support filter clock prescale, fault output state.
Support new APIs to configure PWM and Modified Combine PWM:
FTM_ConfigSinglePWM()
FTM_ConfigCombinePWM()
Support new API to configure channel software output control:
FTM_SetSoftwareOutputCtrl()
FTM_GetSoftwareOutputValue()
FTM_GetSoftwareOutputEnable()
Support new API to update FTM counter initial value, modulo value and chanle value:
FTM_SetInitialModuloValue()
FTM_SetChannelValue()
[2.6.1]#
Improvements
Release peripheral from reset if necessary in init function.
[2.6.0]#
Improvements
Added support to half and full cycle reload feature with new APIs:
FTM_SetLdok()
FTM_SetHalfCycPeriod()
FTM_LoadFreq()
Bug Fixes
Set the HWRSTCNT and SWRSTCNT bits to optional at initialization.
[2.5.0]#
Improvements
Added FTM_CalculateCounterClkDiv to help calculates the counter clock prescaler.
Modify FTM_UpdatePwmDutycycle API to make it return pwm duty cycles status.
Bug Fixes
Fixed TPM_SetupPwm can’t configure 100% center align combined PWM issues.
[2.4.1]#
Bug Fixes
Added function macro to determine if FTM instance has only basic features, to prevent access to protected register bits.
[2.4.0]#
Improvements
Added CNTIN register initialization in FTM_SetTimerPeriod API.
Added a new API to read the captured value of a FTM channel configured in capture mode:
FTM_GetInputCaptureValue()
[2.3.0]#
Improvements
Added support of EdgeAligned/CenterAligned/Asymmetrical combine PWM mode in FTM_SetupPWM() and FTM_SetupPwmMode() APIs.
Remove kFTM_ComplementaryPwm from support PWM mode, and add new parameter “enableComplementary” in structure ftm_chnl_pwm_signal_param_t.
Rename FTM_SetupFault() API to FTM_SetupFaultInput() to avoid ambiguity.
[2.2.3]#
Bug Fixes
MISRA C-2012 issue fixed: rule 14.4 and 17.7.
[2.2.2]#
Bug Fixes
Fixed the issue that when FTM instance has only TPM features cannot be initialized by FTM_Init() function. By added function macro to assert FTM is TPM only instance.
[2.2.1]#
Bug Fixes
MISRA C-2012 issue fixed: rule 10.1, 10.3, 10.4, 10.6, 10.7 and 11.9.
[2.2.0]#
Bug Fixes
Fixed the issue of comparison between signed and unsigned integer expressions.
Improvements
Added support of complementary mode in FTM_SetupPWM() and FTM_SetupPwmMode() APIs.
Added new parameter “enableDeadtime” in structure ftm_chnl_pwm_signal_param_t.
[2.1.1]#
Bug Fixes
Fixed COVERITY integer handing issue where the right operand of a left bit shift statement should not be a negative value. This appears in FTM_SetReloadPoints().
[2.1.0]#
Improvements
Added a new API FTM_SetupPwmMode() to allow the user to set the channel match value in units of timer ticks. New configure structure called ftm_chnl_pwm_config_param_t was added to configure the channel’s PWM parameters. This API is similar with FTM_SetupPwm() API, but the new API will not set the timer period(MOD value), it will be useful for users to set the PWM parameters without changing the timer period.
Bug Fixes
Added feature macro to enable/disable the external trigger source configuration.
[2.0.4]#
Improvements
Added a new API to enable DMA transfer:
FTM_EnableDmaTransfer()
[2.0.3]#
Bug Fixes
Updated the FTM driver to enable fault input after configuring polarity.
[2.0.2]#
Improvements
Added support to Quad Decoder feature with new APIs:
FTM_GetQuadDecoderFlags()
FTM_SetQuadDecoderModuloValue()
FTM_GetQuadDecoderCounterValue()
FTM_ClearQuadDecoderCounterValue()
[2.0.1]#
Bug Fixes
Updated the FTM driver to fix write to ELSA and ELSB bits.
FTM combine mode: set the COMBINE bit before writing to CnV register.
[2.0.0]#
Initial version.
GPIO#
[2.8.6]#
Bug Fixes
Fixed CERT INT31-C violations in
GPIO_FIT_REGmacro for platforms with 8-bit register width.
[2.8.5]#
Improvements
Add AND logic in GPIO_GpioClearInterruptFlags to support clearing multiple interrupt flags simultaneously.
[2.8.4]#
Improvements
Make function
GPIO_PortGetInterruptFlagsandGPIO_PortClearInterruptFlagsavailable for all variants, they are used for all pins flags in one GPIO port.
[2.8.3]#
Bug Fixes
Fixed violations of the MISRA C-2012 Rule 10.1, 5.7.
[2.8.2]#
Bug Fixes
Fixed COVERITY issue that GPIO_GetInstance could return clock array overflow values due to GPIO base and clock being out of sync.
[2.8.1]#
Bug Fixes
Fixed CERT INT31-C issues.
[2.8.0]#
Improvements
Add API GPIO_PortInit/GPIO_PortDeinit to set GPIO clock enable and releasing GPIO reset.
[2.8.0]#
Improvements
Add API GPIO_PortInit/GPIO_PortDeinit to set GPIO clock enable and releasing GPIO reset.
Remove support for API GPIO_GetPinsDMARequestFlags with GPIO_ISFR_COUNT <= 1.
[2.7.3]#
Improvements
Release peripheral from reset if necessary in init function.
[2.7.2]#
New Features
Support devices without PORT module.
[2.7.1]#
Bug Fixes
Fixed MISRA C-2012 rule 10.4 issues in GPIO_GpioGetInterruptChannelFlags() function and GPIO_GpioClearInterruptChannelFlags() function.
[2.7.0]#
New Features
Added API to support Interrupt select (IRQS) bitfield.
[2.6.0]#
New Features
Added API to get GPIO version information.
Added API to control a pin for general purpose input.
Added some APIs to control pin in secure and previliege status.
[2.5.3]#
Bug Fixes
Correct the feature macro typo: FSL_FEATURE_GPIO_HAS_NO_INDEP_OUTPUT_CONTORL.
[2.5.2]#
Improvements
Improved GPIO_PortSet/GPIO_PortClear/GPIO_PortToggle functions to support devices without Set/Clear/Toggle registers.
[2.5.1]#
Bug Fixes
Fixed wrong macro definition.
Fixed MISRA C-2012 rule issues in the FGPIO_CheckAttributeBytes() function.
Defined the new macro to separate the scene when the width of registers is different.
Removed some redundant macros.
New Features
Added some APIs to get/clear the interrupt status flag when the port doesn’t control pins’ interrupt.
[2.4.1]#
Improvements
Improved GPIO_CheckAttributeBytes() function to support 8 bits width GACR register.
[2.4.0]#
Improvements
API interface added:
New APIs were added to configure the GPIO interrupt clear settings.
[2.3.2]#
Bug Fixes
Fixed the issue for MISRA-2012 check.
Fixed rule 3.1, 10.1, 8.6, 10.6, and 10.3.
[2.3.1]#
Improvements
Removed deprecated APIs.
[2.3.0]#
New Features
Updated the driver code to adapt the case of interrupt configurations in GPIO module. New APIs were added to configure the GPIO interrupt settings if the module has this feature on it.
[2.2.1]#
Improvements
API interface changes:
Refined naming of APIs while keeping all original APIs by marking them as deprecated. The original APIs will be removed in next release. The main change is updating APIs with prefix of _PinXXX() and _PortXXX.
[2.1.1]#
Improvements
API interface changes:
Added an API for the check attribute bytes.
[2.1.0]#
Improvements
API interface changes:
Added “pins” or “pin” to some APIs’ names.
Renamed “_PinConfigure” to “GPIO_PinInit”.
LPI2C#
[2.6.8]#
Bug Fixes
LPI2C_MasterTransferBlocking - added waiting while TX FIFO is not empty.
Added a check for an error from the previous transfer in the transfer API (when kLPI2C_TransferNoStopFlag was used).
Updated LPI2C_MasterReceive() to return kStatus_InvalidArgument when rxSize is 0.
Updated transfer API functions to return kStatus_InvalidArgument when transfer->dataSize is 0 and transfer->direction is kLPI2C_Read.
Fixed assert issue in LPI2C_MasterSetBaudRate().
Fixed CERT-C issues.
Fixed MISRA issues.
Improved HIS CCM for LPI2C_MasterTransferBlocking() and LPI2C_SlaveTransferHandleIRQ().
[2.6.7]#
Bug Fixes
Fixed MISRA 10.3 and 10.8 issues.
Fixed LPI2C_MasterStop() to send I2C STOP in case of error.
[2.6.6]#
Bug Fixes
Set handle->chunkSize to 0 in LPI2C_MasterTransferNonBlocking().
[2.6.5]#
Bug Fixes
Removed write to STAR register in LPI2C_SlaveTransferHandleIRQ handler in case of kLPI2C_SlaveRepeatedStartDetectFlag or kLPI2C_SlaveStopDetectFlag.
Removed configuration of FILTSDA from LPI2C_MasterSetBaudRate().
Set minimal possible value for FILTSDA and FILTSCL to 0.
Updated configuration of glitch filters in LPI2C_SlaveInit().
Set minimal possible value for SCFGR2[CLKHOLD] to 1.
Added error check to while loop in LPI2C_TransferStateMachineSendCommand().
Improvements
Removed receive data size limitation in LPI2C_MasterTransferBlocking() and LPI2C_MasterTransferNonBlocking().
[2.6.4]#
Bug Fixes
Limited value of filtSda in LPI2C_MasterSetBaudRate().
Updated LPI2C_MasterStop() and LPI2C_MasterTransferBlocking() to send I2C STOP also in case of error.
Removed unused flag kLPI2C_TransferRepeatedStartFlag.
[2.6.3]#
Bug Fixes
Fixed static analysis identified issues.
[2.6.2]#
Improvements
Added timeout for while loop in LPI2C_TransferStateMachineSendCommand().
[2.6.1]#
Bug Fixes
Fixed coverity issues.
[2.6.0]#
New Feature
Added common IRQ handler entry LPI2C_DriverIRQHandler.
[2.5.7]#
Improvements
Added support for separated IRQ handlers.
[2.5.6]#
Improvements
Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.
[2.5.5]#
Bug Fixes
Fixed LPI2C_SlaveInit() - allow to disable SDA/SCL glitch filter.
[2.5.4]#
Bug Fixes
Fixed LPI2C_MasterTransferBlocking() - the return value was sometime affected by call of LPI2C_MasterStop().
[2.5.3]#
Improvements
Added handler for LPI2C7 and LPI2C8.
[2.5.2]#
Bug Fixes
Fixed ERR051119 to ignore the nak flag when IGNACK=1 in LPI2C_MasterCheckAndClearError.
[2.5.1]#
Bug Fixes
Added bus stop incase of bus stall in LPI2C_MasterTransferBlocking.
Improvements
Release peripheral from reset if necessary in init function.
[2.5.0]#
New Features
Added new function LPI2C_SlaveEnableAckStall to enable or disable ACKSTALL.
[2.4.1]#
Improvements
Before master transfer with transactional APIs, enable master function while disable slave function and vise versa for slave transfer to avoid the one affecting the other.
[2.4.0]#
Improvements
Split some functions, fixed CCM problem in file fsl_lpi2c.c.
Bug Fixes
Fixed bug in LPI2C_MasterInit that the MCFGR2’s value set in LPI2C_MasterSetBaudRate may be overwritten by mistake.
[2.3.2]#
Improvements
Initialized the EDMA configuration structure in the LPI2C EDMA driver.
[2.3.1]#
Improvements
Updated LPI2C_GetCyclesForWidth to add the parameter of minimum cycle, because for master SDA/SCL filter, master bus idle/pin low timeout and slave SDA/SCL filter configuration, 0 means disabling the feature and cannot be used.
Bug Fixes
Fixed bug in LPI2C_SlaveTransferHandleIRQ that when restart detect event happens the transfer structure should not be cleared.
Fixed bug in LPI2C_RunTransferStateMachine, that when only slave address is transferred or there is still data remaining in tx FIFO the last byte’s nack cannot be ignored.
Fixed bug in slave filter doze enable, that when FILTDZ is set it means disable rather than enable.
Fixed bug in the usage of LPI2C_GetCyclesForWidth. First its return value cannot be used directly to configure the slave FILTSDA, FILTSCL, DATAVD or CLKHOLD, because the real cycle width for them should be FILTSDA+3, FILTSCL+3, FILTSCL+DATAVD+3 and CLKHOLD+3. Second when cycle period is not affected by the prescaler value, prescaler value should be passed as 0 rather than 1.
Fixed wrong default setting for LPI2C slave. If enabling the slave tx SCL stall, then the default clock hold time should be set to 250ns according to I2C spec for 100kHz standard mode baudrate.
Fixed bug that before pushing command to the tx FIFO the FIFO occupation should be checked first in case FIFO overflow.
[2.3.0]#
New Features
Supported reading more than 256 bytes of data in one transfer as master.
Added API LPI2C_GetInstance.
Bug Fixes
Fixed bug in LPI2C_MasterTransferAbortEDMA, LPI2C_MasterTransferAbort and LPI2C_MasterTransferHandleIRQ that before sending stop signal whether master is active and whether stop signal has been sent should be checked, to make sure no FIFO error or bus error will be caused.
Fixed bug in LPI2C master EDMA transactional layer that the bus error cannot be caught and returned by user callback, by monitoring bus error events in interrupt handler.
Fixed bug in LPI2C_GetCyclesForWidth that the parameter used to calculate clock cycle should be 2^prescaler rather than prescaler.
Fixed bug in LPI2C_MasterInit that timeout value should be configured after baudrate, since the timeout calculation needs prescaler as parameter which is changed during baudrate configuration.
Fixed bug in LPI2C_MasterTransferHandleIRQ and LPI2C_RunTransferStateMachine that when master writes with no stop signal, need to first make sure no data remains in the tx FIFO before finishes the transfer.
[2.2.0]#
Bug Fixes
Fixed issue that the SCL high time, start hold time and stop setup time do not meet I2C specification, by changing the configuration of data valid delay, setup hold delay, clock high and low parameters.
MISRA C-2012 issue fixed.
Fixed rule 8.4, 13.5, 17.7, 20.8.
[2.1.12]#
Bug Fixes
Fixed MISRA advisory 15.5 issues.
[2.1.11]#
Bug Fixes
Fixed the bug that, during master non-blocking transfer, after the last byte is sent/received, the kLPI2C_MasterNackDetectFlag is expected, so master should not check and clear kLPI2C_MasterNackDetectFlag when remainingBytes is zero, in case FIFO is emptied when stop command has not been sent yet.
Fixed the bug that, during non-blocking transfer slave may nack master while master is busy filling tx FIFO, and NDF may not be handled properly.
[2.1.10]#
Bug Fixes
MISRA C-2012 issue fixed.
Fixed rule 10.3, 14.4, 15.5.
Fixed unaligned access issue in LPI2C_RunTransferStateMachine.
Fixed uninitialized variable issue in LPI2C_MasterTransferHandleIRQ.
Used linked TCD to disable tx and enable rx in read operation to fix the issue that for platform sharing the same DMA request with tx and rx, during LPI2C read operation if interrupt with higher priority happened exactly after command was sent and before tx disabled, potentially both tx and rx could trigger dma and cause trouble.
Fixed MISRA issues.
Fixed rules 10.1, 10.3, 10.4, 11.6, 11.9, 14.4, 17.7.
Fixed the waitTimes variable not re-assignment issue for each byte read.
New Features
Added the IRQHandler for LPI2C5 and LPI2C6 instances.
Improvements
Updated the LPI2C_WAIT_TIMEOUT macro to unified name I2C_RETRY_TIMES.
[2.1.9]#
Bug Fixes
Fixed Coverity issue of unchecked return value in I2C_RTOS_Transfer.
Fixed Coverity issue of operands did not affect the result in LPI2C_SlaveReceive and LPI2C_SlaveSend.
Removed STOP signal wait when NAK detected.
Cleared slave repeat start flag before transmission started in LPI2C_SlaveSend/LPI2C_SlaveReceive. The issue was that LPI2C_SlaveSend/LPI2C_SlaveReceive did not handle with the reserved repeat start flag. This caused the next slave to send a break, and the master was always in the receive data status, but could not receive data.
[2.1.8]#
Bug Fixes
Fixed the transfer issue with LPI2C_MasterTransferNonBlocking, kLPI2C_TransferNoStopFlag, with the wait transfer done through callback in a way of not doing a blocking transfer.
Fixed the issue that STOP signal did not appear in the bus when NAK event occurred.
[2.1.7]#
Bug Fixes
Cleared the stopflag before transmission started in LPI2C_SlaveSend/LPI2C_SlaveReceive. The issue was that LPI2C_SlaveSend/LPI2C_SlaveReceive did not handle with the reserved stop flag and caused the next slave to send a break, and the master always stayed in the receive data status but could not receive data.
[2.1.6]#
Bug Fixes
Fixed driver MISRA build error and C++ build error in LPI2C_MasterSend and LPI2C_SlaveSend.
Reset FIFO in LPI2C Master Transfer functions to avoid any byte still remaining in FIFO during last transfer.
Fixed the issue that LPI2C_MasterStop did not return the correct NAK status in the bus for second transfer to the non-existing slave address.
[2.1.5]#
Bug Fixes
Extended the Driver IRQ handler to support LPI2C4.
Changed to use ARRAY_SIZE(kLpi2cBases) instead of FEATURE COUNT to decide the array size for handle pointer array.
[2.1.4]#
Bug Fixes
Fixed the LPI2C_MasterTransferEDMA receive issue when LPI2C shared same request source with TX/RX DMA request. Previously, the API used scatter-gather method, which handled the command transfer first, then the linked TCD which was pre-set with the receive data transfer. The issue was that the TX DMA request and the RX DMA request were both enabled, so when the DMA finished the first command TCD transfer and handled the receive data TCD, the TX DMA request still happened due to empty TX FIFO. The result was that the RX DMA transfer would start without waiting on the expected RX DMA request.
Fixed the issue by enabling IntMajor interrupt for the command TCD and checking if there was a linked TCD to disable the TX DMA request in LPI2C_MasterEDMACallback API.
[2.1.3]#
Improvements
Added LPI2C_WATI_TIMEOUT macro to allow the user to specify the timeout times for waiting flags in functional API and blocking transfer API.
Added LPI2C_MasterTransferBlocking API.
[2.1.2]#
Bug Fixes
In LPI2C_SlaveTransferHandleIRQ, reset the slave status to idle when stop flag was detected.
[2.1.1]#
Bug Fixes
Disabled the auto-stop feature in eDMA driver. Previously, the auto-stop feature was enabled at transfer when transferring with stop flag. Since transfer was without stop flag and the auto-stop feature was enabled, when starting a new transfer with stop flag, the stop flag would be sent before the new transfer started, causing unsuccesful sending of the start flag, so the transfer could not start.
Changed default slave configuration with address stall false.
[2.1.0]#
Improvements
API name changed:
LPI2C_MasterTransferCreateHandle -> LPI2C_MasterCreateHandle.
LPI2C_MasterTransferGetCount -> LPI2C_MasterGetTransferCount.
LPI2C_MasterTransferAbort -> LPI2C_MasterAbortTransfer.
LPI2C_MasterTransferHandleIRQ -> LPI2C_MasterHandleInterrupt.
LPI2C_SlaveTransferCreateHandle -> LPI2C_SlaveCreateHandle.
LPI2C_SlaveTransferGetCount -> LPI2C_SlaveGetTransferCount.
LPI2C_SlaveTransferAbort -> LPI2C_SlaveAbortTransfer.
LPI2C_SlaveTransferHandleIRQ -> LPI2C_SlaveHandleInterrupt.
[2.0.0]#
Initial version.
LPI2C_EDMA#
[2.4.9]#
Bug Fixes
Fixed CERT-C issues.
Fixed MISRA issues.
[2.4.8]#
Bug Fixes
Fixed MISRA 10.6 and 14.3 issues.
[2.4.7]#
Bug Fixes
Fixed incorrect TX FIFO size (maxTxFifo) in LPI2C_MasterTransferEDMA() and LPI2C_MasterTransferEdmaHandleIRQ().
[2.4.6]#
Bug Fixes
Fixed static analysis identified issues.
[2.4.5]#
Improvements
Added condition to IRQ handler to check whether the interrupt is enabled - kLPI2C_MasterTxReadyFlag.
[2.4.4]#
Improvements
Added support for 2KB data transfer
[2.4.3]#
Improvements
Added support for separated IRQ handlers.
[2.4.2]#
Improvements
Add EDMA ext API to accommodate more types of EDMA.
[2.4.1]#
Refer LPI2C driver change log 2.0.0 to 2.4.1
LPIT#
[2.1.3]#
Bug Fixes
Fixed doxygen generation warnings.
[2.1.2]#
Bug Fixes
Fix CERT INT31-C issues.
[2.1.1]#
Improvements
Release peripheral from reset if necessary in init function.
[2.1.0]#
Improvements
Add new function LPIT_SetTimerValue to set timeout period.
[2.0.2]#
Improvements
Improved LPIT_SetTimerPeriod implementation, configure timeout value with LPIT ticks minus 1 generate more correct interval.
Added timeout value configuration check for LPIT_SetTimerPeriod, at least input 3 ticks for calling LPIT_SetTimerPeriod.
Bug Fixes
Fixed MISRA C-2012 rule 17.7 violations.
[2.0.1]#
Bug Fixes
MISRA C-2012 issue fixed.
Fixed rules, containing: rule-10.3, rule-14.4, rule-15.5.
[2.0.0]#
Initial version.
LPSPI#
[2.7.8]#
Bug Fixes
Fixed CERT-C issues.
Fixed MISRA issues.
Improvements
Improved HIS CCM.
[2.7.7]#
Bug Fixes
Fixed timing parameter setting sequence issue in
LPSPI_MasterInit, the timing parameter should only be configured when LPSPI master is disabled.
Improvements
Improved performance of LPSPI_MasterTransferBlocking().
[2.7.6]#
Bug Fixes
Fixed calculation of SCK-to-SCK delay.
[2.7.5]#
Bug Fixes
Fixed MISRA 10.3, 12,2 and 10.7 issues.
[2.7.4]#
Bug Fixes
Clear WIDTH bits from the TCR register before writing a new value in LPSPI_MasterTransferBlocking().
[2.7.3]#
Improvements
Added timeout for while loop in LPSPI_MasterTransferWriteAllTxData().
Make SPI_RETRY_TIMES configurable by CONFIG_SPI_RETRY_TIMES.
[2.7.2]#
Bug Fixes
Fixed coverity issues.
[2.7.1]#
Bug Fixes
Workaround for errata ERR050607
Workaround for errata ERR010655
[2.7.0]#
New Feature
Added common IRQ handler entry LPSPI_DriverIRQHandler.
[2.6.10]#
Improvements
Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.
[2.6.9]#
Bug Fixes
Fixed reading of TCR register
Workaround for errata ERR050606
[2.6.8]#
Bug Fixes
Fixed build error when SPI_RETRY_TIMES is defined to non-zero value.
[2.6.7]#
Bug Fixes
Fixed the txData from void * to const void * in transmit API _lpspi_master_handle and _lpspi_slave_handle.
[2.6.6]#
Bug Fixes
Added LPSPI register init in LPSPI_MasterInit incase of LPSPI register exist.
[2.6.5]#
Improvements
Introduced FSL_FEATURE_LPSPI_HAS_NO_PCSCFG and FSL_FEATURE_LPSPI_HAS_NO_MULTI_WIDTH for conditional compile.
Release peripheral from reset if necessary in init function.
[2.6.4]#
Bug Fixes
Added LPSPI6_DriverIRQHandler for LPSPI6 instance.
[2.6.3]#
Hot Fixes
Added macro switch in function LPSPI_Enable about ERRATA051472.
[2.6.2]#
Bug Fixes
Disabled lpspi before LPSPI_MasterSetBaudRate incase of LPSPI opened.
[2.6.1]#
Bug Fixes
Fixed return value while calling LPSPI_WaitTxFifoEmpty in function LPSPI_MasterTransferNonBlocking.
[2.6.0]#
Feature
Added the new feature of multi-IO SPI .
[2.5.3]#
Bug Fixes
Fixed 3-wire txmask of handle vaule reentrant issue.
[2.5.2]#
Bug Fixes
Workaround for errata ERR051588 by clearing FIFO after transmit underrun occurs.
[2.5.1]#
Bug Fixes
Workaround for errata ERR050456 by resetting the entire module using LPSPIn_CR[RST] bit.
[2.5.0]#
Bug Fixes
Workaround for errata ERR011097 to wait the TX FIFO to go empty when writing TCR register and TCR[TXMSK] value is 1.
Added API LPSPI_WaitTxFifoEmpty for wait the txfifo to go empty.
[2.4.7]#
Bug Fixes
Fixed bug that the SR[REF] would assert if software disabled or enabled the LPSPI module in LPSPI_Enable.
[2.4.6]#
Improvements
Moved the configuration of registers for the 3-wire lpspi mode to the LPSPI_MasterInit and LPSPI_SlaveInit function.
[2.4.5]#
Improvements
Improved LPSPI_MasterTransferBlocking send performance when frame size is 1-byte.
[2.4.4]#
Bug Fixes
Fixed LPSPI_MasterGetDefaultConfig incorrect default inter-transfer delay calculation.
[2.4.3]#
Bug Fixes
Fixed bug that the ISR response speed is too slow on some platforms, resulting in the first transmission of overflow, Set proper RX watermarks to reduce the ISR response times.
[2.4.2]#
Bug Fixes
Fixed bug that LPSPI_MasterTransferBlocking will modify the parameter txbuff and rxbuff pointer.
[2.4.1]#
Bug Fixes
Fixed bug that LPSPI_SlaveTransferNonBlocking can’t detect RX error.
[2.4.0]#
Improvements
Split some functions, fixed CCM problem in file fsl_lpspi.c.
[2.3.1]#
Improvements
Initialized the EDMA configuration structure in the LPSPI EDMA driver.
Bug Fixes
Fixed bug that function LPSPI_MasterTransferBlocking should return after the transfer complete flag is set to make sure the PCS is re-asserted.
[2.3.0]#
New Features
Supported the master configuration of sampling the input data using a delayed clock to improve slave setup time.
[2.2.1]#
Bug Fixes
Fixed bug in LPSPI_SetPCSContinous when disabling PCS continous mode.
[2.2.0]#
Bug Fixes
Fixed bug in 3-wire polling and interrupt transfer that the received data is not correct and the PCS continous mode is not working.
[2.1.0]#
Improvements
Improved LPSPI_SlaveTransferHandleIRQ to fill up TX FIFO instead of write one data to TX register which improves the slave transmit performance.
Added new functional APIs LPSPI_SelectTransferPCS and LPSPI_SetPCSContinous to support changing PCS selection and PCS continous mode.
Bug Fixes
Fixed bug in non-blocking and EDMA transfer APIs that kStatus_InvalidArgument is returned if user configures 3-wire mode and full-duplex transfer at the same time, but transfer state is already set to kLPSPI_Busy by mistake causing following transfer can not start.
Fixed bug when LPSPI slave using EDMA way to transfer, tx should be masked when tx data is null, otherwise in 3-wire mode which tx/rx use the same pin, the received data will be interfered.
[2.0.5]#
Improvements
Added timeout mechanism when waiting certain states in transfer driver.
Bug Fixes
Fixed the bug that LPSPI can not transfer large data using EDMA.
Fixed MISRA 17.7 issues.
Fixed variable overflow issue introduced by MISRA fix.
Fixed issue that rxFifoMaxBytes should be calculated according to transfer width rather than FIFO width.
Fixed issue that completion flag was not cleared after transfer completed.
[2.0.4]#
Bug Fixes
Fixed in LPSPI_MasterTransferBlocking that master rxfifo may overflow in stall condition.
Eliminated IAR Pa082 warnings.
Fixed MISRA issues.
Fixed rules 10.1, 10.3, 10.4, 10.6, 11.9, 14.2, 14.4, 15.7, 17.7.
[2.0.3]#
Bug Fixes
Removed LPSPI_Reset from LPSPI_MasterInit and LPSPI_SlaveInit, because this API may glitch the slave select line. If needed, call this function manually.
[2.0.2]#
New Features
Added dummy data set up API to allow users to configure the dummy data to be transferred.
Enabled the 3-wire mode, SIN and SOUT pins can be configured as input/output pin.
[2.0.1]#
Bug Fixes
Fixed the bug that the clock source should be divided by the PRESCALE setting in LPSPI_MasterSetDelayTimes function.
Fixed the bug that LPSPI_MasterTransferBlocking function would hang in some corner cases.
Optimization
Added #ifndef/#endif to allow user to change the default TX value at compile time.
[2.0.0]#
Initial version.
LPSPI_EDMA#
[2.4.11]#
Bug Fixes
Fixed CERT-C issues.
Fixed MISRA issues.
Improvements
Improved HIS CCM in LPSPI_MasterTransferEDMALite() and LPSPI_SlaveTransferEDMA().
[2.4.10]#
Bug Fixes
Fixed MISRA 10.6 issues.
[2.4.9]#
Improvements
Removed unused code from LPSPI_SeparateEdmaReadData().
[2.4.8]#
Improvements
Added timeout for while loop in EDMA_LpspiMasterCallback() and EDMA_LpspiSlaveCallback().
[2.4.7]#
Bug Fixes
Add macro LPSPI_ALIGN_TCD_SIZE_MASK to align an address to edma_tcd_t size.
[2.4.6]#
Improvements
Increased transmit FIFO watermark to ensure whole transmit FIFO will be used during data transfer.
[2.4.5]#
Bug Fixes
Fixed reading of TCR register
Workaround for errata ERR050606
[2.4.4]#
Improvements
Add EDMA ext API to accommodate more types of EDMA.
[2.4.3]#
Improvements
Supported 32K bytes transmit in DMA, improve the max datasize in LPSPI_MasterTransferEDMALite.
[2.4.2]#
Improvements
Added callback status in EDMA_LpspiMasterCallback and EDMA_LpspiSlaveCallback to check transferDone.
[2.4.1]#
Improvements
Add the TXMSK wait after TCR setting.
[2.4.0]#
Improvements
Separated LPSPI_MasterTransferEDMA functions to LPSPI_MasterTransferPrepareEDMA and LPSPI_MasterTransferEDMALite to optimize the process of transfer.
LPTMR#
[2.2.1]#
Bug Fixes
Fix CERT INT31-C issues.
[2.2.0]#
Improvements
Updated lptmr_prescaler_clock_select_t, only define the valid options.
[2.1.1]#
Improvements
Updated the characters from “PTMR” to “LPTMR” in “FSL_FEATURE_PTMR_HAS_NO_PRESCALER_CLOCK_SOURCE_1_SUPPORT” feature definition.
[2.1.0]#
Improvements
Implement for some special devices’ not supporting for all clock sources.
Bug Fixes
Fixed issue when accessing CMR register.
[2.0.2]#
Bug Fixes
Fixed MISRA-2012 issues.
Rule 10.1.
[2.0.1]#
Improvements
Updated the LPTMR driver to support 32-bit CNR and CMR registers in some devices.
[2.0.0]#
Initial version.
LPUART#
[2.11.0]#
New Feature
Added support to enable transmitter RTS and configure transmitter RTS polarity.
Added support to enable Transmit Data Inversion.
Improvements
Updated to work on DSC platform.
[2.10.0]#
New Feature
Added support to configure RTS watermark.
[2.9.4]#
Improvements
Merged duplicate code.
[2.9.3]#
Improvements
Added timeout for while loops in LPUART_Deinit().
[2.9.2]#
Bug Fixes
Fixed coverity issues.
[2.9.1]#
Bug Fixes
Fixed coverity issues.
[2.9.0]#
New Feature
Added support for swap TXD and RXD pins.
Added common IRQ handler entry LPUART_DriverIRQHandler.
[2.8.3]#
Improvements
Conditionally compile interrupt handling code to solve the problem of using this driver on CPU cores that do not support interrupts.
[2.8.2]#
Bug Fix
Fixed the bug that LPUART_TransferEnable16Bit controled by wrong feature macro.
[2.8.1]#
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule-5.3, rule-5.8, rule-10.4, rule-11.3, rule-11.8.
[2.8.0]#
Improvements
Added support of DATA register for 9bit or 10bit data transmit in write and read API. Such as: LPUART_WriteBlocking16bit, LPUART_ReadBlocking16bit, LPUART_TransferEnable16Bit LPUART_WriteNonBlocking16bit, LPUART_ReadNonBlocking16bit.
[2.7.7]#
Bug Fixes
Fixed the bug that baud rate calculation overflow when srcClock_Hz is 528MHz.
[2.7.6]#
Bug Fixes
Fixed LPUART_EnableInterrupts and LPUART_DisableInterrupts bug that blocks if the LPUART address doesn’t support exclusive access.
[2.7.5]#
Improvements
Release peripheral from reset if necessary in init function.
[2.7.4]#
Improvements
Added support for atomic register accessing in LPUART_EnableInterrupts and LPUART_DisableInterrupts.
[2.7.3]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules 15.7.
[2.7.2]#
Bug Fix
Fixed the bug that the OSR calculation error when lupart init and lpuart set baud rate.
[2.7.1]#
Improvements
Added support for LPUART_BASE_PTRS_NS in security mode in file fsl_lpuart.c.
[2.7.0]#
Improvements
Split some functions, fixed CCM problem in file fsl_lpuart.c.
[2.6.0]#
Bug Fixes
Fixed bug that when there are multiple lpuart instance, unable to support different ISR.
[2.5.3]#
Bug Fixes
Fixed comments by replacing unused status flags kLPUART_NoiseErrorInRxDataRegFlag and kLPUART_ParityErrorInRxDataRegFlag with kLPUART_NoiseErrorFlag and kLPUART_ParityErrorFlag.
[2.5.2]#
Bug Fixes
Fixed bug that when setting watermark for TX or RX FIFO, the value may exceed the maximum limit.
Improvements
Added check in LPUART_TransferDMAHandleIRQ and LPUART_TransferEdmaHandleIRQ to ensure if user enables any interrupts other than transfer complete interrupt, the dma transfer is not terminated by mistake.
[2.5.1]#
Improvements
Use separate data for TX and RX in lpuart_transfer_t.
Bug Fixes
Fixed bug that when ring buffer is used, if some data is received in ring buffer first before calling LPUART_TransferReceiveNonBlocking, the received data count returned by LPUART_TransferGetReceiveCount is wrong.
[2.5.0]#
Bug Fixes
Added missing interrupt enable masks kLPUART_Match1InterruptEnable and kLPUART_Match2InterruptEnable.
Fixed bug in LPUART_EnableInterrupts, LPUART_DisableInterrupts and LPUART_GetEnabledInterrupts that the BAUD[LBKDIE] bit field should be soc specific.
Fixed bug in LPUART_TransferHandleIRQ that idle line interrupt should be disabled when rx data size is zero.
Deleted unused status flags kLPUART_NoiseErrorInRxDataRegFlag and kLPUART_ParityErrorInRxDataRegFlag, since firstly their function are the same as kLPUART_NoiseErrorFlag and kLPUART_ParityErrorFlag, secondly to obtain them one data word must be read out thus interfering with the receiving process.
Fixed bug in LPUART_GetStatusFlags that the STAT[LBKDIF], STAT[MA1F] and STAT[MA2F] should be soc specific.
Fixed bug in LPUART_ClearStatusFlags that tx/rx FIFO is reset by mistake when clearing flags.
Fixed bug in LPUART_TransferHandleIRQ that while clearing idle line flag the other bits should be masked in case other status bits be cleared by accident.
Fixed bug of race condition during LPUART transfer using transactional APIs, by disabling and re-enabling the global interrupt before and after critical operations on interrupt enable register.
Fixed DMA/eDMA transfer blocking issue by enabling tx idle interrupt after DMA/eDMA transmission finishes.
New Features
Added APIs LPUART_GetRxFifoCount/LPUART_GetTxFifoCount to get rx/tx FIFO data count.
Added APIs LPUART_SetRxFifoWatermark/LPUART_SetTxFifoWatermark to set rx/tx FIFO water mark.
[2.4.1]#
Bug Fixes
Fixed MISRA advisory 17.7 issues.
[2.4.0]#
New Features
Added APIs to configure 9-bit data mode, set slave address and send address.
[2.3.1]#
Bug Fixes
Fixed MISRA advisory 15.5 issues.
[2.3.0]#
Improvements
Modified LPUART_TransferHandleIRQ so that txState will be set to idle only when all data has been sent out to bus.
Modified LPUART_TransferGetSendCount so that this API returns the real byte count that LPUART has sent out rather than the software buffer status.
Added timeout mechanism when waiting for certain states in transfer driver.
[2.2.8]#
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule-10.3, rule-14.4, rule-15.5.
Eliminated Pa082 warnings by assigning volatile variables to local variables and using local variables instead.
Fixed MISRA issues.
Fixed rules 10.1, 10.3, 10.4, 10.8, 14.4, 11.6, 17.7.
Improvements
Added check for kLPUART_TransmissionCompleteFlag in LPUART_WriteBlocking, LPUART_TransferHandleIRQ, LPUART_TransferSendDMACallback and LPUART_SendEDMACallback to ensure all the data would be sent out to bus.
Rounded up the calculated sbr value in LPUART_SetBaudRate and LPUART_Init to achieve more acurate baudrate setting. Changed osr from uint32_t to uint8_t since osr’s bigest value is 31.
Modified LPUART_ReadBlocking so that if more than one receiver errors occur, all status flags will be cleared and the most severe error status will be returned.
[2.2.7]#
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule-12.1, rule-17.7, rule-14.4, rule-13.3, rule-14.4, rule-10.4, rule-10.8, rule-10.3, rule-10.7, rule-10.1, rule-11.6, rule-13.5, rule-11.3, rule-13.2, rule-8.3.
[2.2.6]#
Bug Fixes
Fixed the issue of register’s being in repeated reading status while dealing with the IRQ routine.
[2.2.5]#
Bug Fixes
Do not set or clear the TIE/RIE bits when using LPUART_EnableTxDMA and LPUART_EnableRxDMA.
[2.2.4]#
Improvements
Added hardware flow control function support.
Added idle-line-detecting feature in LPUART_TransferNonBlocking function. If an idle line is detected, a callback is triggered with status kStatus_LPUART_IdleLineDetected returned. This feature may be useful when the received Bytes is less than the expected received data size. Before triggering the callback, data in the FIFO (if has FIFO) is read out, and no interrupt will be disabled, except for that the receive data size reaches 0.
Enabled the RX FIFO watermark function. With the idle-line-detecting feature enabled, users can set the watermark value to whatever you want (should be less than the RX FIFO size). Data is received and a callback will be triggered when data receive ends.
[2.2.3]#
Improvements
Changed parameter type in LPUART_RTOS_Init struct from rtos_lpuart_config to lpuart_rtos_config_t.
Bug Fixes
Disabled LPUART receive interrupt instead of all NVICs when reading data from ring buffer. Otherwise when the ring buffer is used, receive nonblocking method will disable all NVICs to protect the ring buffer. This may has a negative effect on other IPs that are using the interrupt.
[2.2.2]#
Improvements
Added software reset feature support.
Added software reset API in LPUART_Init.
[2.2.1]#
Improvements
Added separate RX/TX IRQ number support.
[2.2.0]#
Improvements
Added support of 7 data bits and MSB.
[2.1.1]#
Improvements
Removed unnecessary check of event flags and assert in LPUART_RTOS_Receive.
Added code to always wait for RX event flag in LPUART_RTOS_Receive.
[2.1.0]#
Improvements
Update transactional APIs.
LPUART_EDMA#
[2.4.0]#
Refer LPUART driver change log 2.1.0 to 2.4.0
MCM#
[2.2.1]#
Improvements
Add feature to support platforms that do not have the MCM CPCR (Core Platform Control Register).
[2.2.0]#
Improvements
Support platforms with less features.
[2.1.0]#
Others
Remove byteID from mcm_lmem_fault_attribute_t for document update.
[2.0.0]#
Initial version.
PMC#
[2.0.4]#
Bug Fixes
Add validation before narrowing uint32_t to uint8_t conversions using assert
Replace direct boolean to integer casts with explicit ternary operators
Add INT31-C compliance comments for safe narrowing conversions
Apply fixes to PMC_ConfigureLowVoltDetect, PMC_ConfigureLowVoltWarning, and PMC_ConfigureBandgapBuffer functions
[2.0.3]#
Bug Fixes
Fixed the violation of MISRA C-2012 rule 11.3.
[2.0.2]#
Bug Fixes
Fixed the violations of MISRA 2012 rules:
Rule 10.3.
[2.0.1]#
Bug Fixes
Fixed MISRA issues.
Rule 10.8, Rule 10.3.
[2.0.0]#
Initial version.
PORT#
[2.5.1]#
Bug Fixes
Fix CERT INT31-C issues.
Fixed the violations of MISRA C-2012 rules: 10.1.
[2.5.0]#
Bug Fixes
Correct the kPORT_MuxAsGpio for some platforms.
[2.4.1]#
Bug Fixes
Fixed the violations of MISRA C-2012 rules: 10.1, 10.8 and 14.4.
[2.4.0]#
New Features
Updated port_pin_config_t to support input buffer and input invert.
[2.3.0]#
New Features
Added new APIs for Electrical Fast Transient(EFT) detect.
Added new API to configure port voltage range.
[2.2.0]#
New Features
Added new api PORT_EnablePinDoubleDriveStrength.
[2.1.1]#
Bug Fixes
Fixed the violations of MISRA C-2012 rules: 10.1, 10.4,11.3,11.8, 14.4.
[2.1.0]#
New Features
Updated the driver code to adapt the case of the interrupt configurations in GPIO module. Will move the pin configuration APIs to GPIO module.
[2.0.2]#
Other Changes
Added feature guard macros in the driver.
[2.0.1]#
Other Changes
Added “const” in function parameter.
Updated some enumeration variables’ names.
PWT#
[2.0.3]#
Improvements
Added support for 32-bit PWT register width (e.g. MCXC353) via FSL_FEATURE_PWT_REG_WIDTH feature macro.
New Features
Added TGL (input toggle) status flag support.
Added PWT_GetInputLevel() API to read the PWTIN level when overflow occurs.
[2.0.2]#
Bug Fixes
Fixed CERT INT31-C violations.
[2.0.1]#
Bug Fixes
Fixed violations of MISRA C-2012 rules: 10.8, 10.3, 10.6.
[2.0.0]#
Initial version.
RCM#
[2.0.6]#
Bug Fixes
Fixed RCM_GetVersionId() always returning 0 for the major version field due to a wrong mask/shift combination (CID 8644199).
[2.0.5]#
Bug Fixes
Replace direct boolean to integer casts with explicit ternary operators for INT31-C compliance.
Add validation before narrowing uint32_t to uint8_t conversion using assert.
Add INT31-C compliance comments for safe type handling.
Apply fixes to RCM_ConfigureResetPinFilter and RCM_SetForceBootRomSource functions.
[2.0.4]#
Bug Fixes
Fixed violation of MISRA C-2012 rule 10.3
[2.0.3]#
Bug Fixes
Fixed violation of MISRA C-2012 rules.
[2.0.2]#
Bug Fixes
Fixed MISRA issue.
Rule 10.8, rule 10.1, rule 13.2, rule 3.1.
[2.0.1]#
Bug Fixes
Fixed kRCM_SourceSw bit shift issue.
[2.0.0]#
Initial version.
RTC#
[2.4.0]#
New features
Add support for RTC clock output.
Add support for RTC time seconds interrupt configuration.
[2.3.3]#
Bug Fixes
Fix RTC_GetDatetime function validating datetime issue.
[2.3.2]#
Improvements
Handle errata 010716: Disable the counter before setting alarm register and then reenable the counter.
[2.3.1]#
Bug Fixes
Fixed CERT INT31-C violations.
[2.3.0]#
Improvements
Added API RTC_EnableLPOClock to set 1kHz LPO clock.
Added API RTC_EnableCrystalClock to replace API RTC_SetClockSource.
[2.2.2]#
Improvements
Refine _rtc_interrupt_enable order.
[2.2.1]#
Bug Fixes
Fixed the issue of Pa082 warning.
Fixed the issue of bit field mask checking.
Fixed the issue of hard code in RTC_Init.
[2.2.0]#
Bug Fixes
Fixed MISRA C-2012 issue.
Fixed rule contain: rule-17.7, rule-14.4, rule-10.4, rule-10.7, rule-10.1, rule-10.3.
Fixed central repository code formatting issue.
Improvements
Added an API for enabling wakeup pin.
[2.1.0]#
Improvements
Added feature macro check for many features.
[2.0.0]#
Initial version.
SIM#
[2.2.0]#
Improvements
Added API to trigger TRGMUX.
[2.1.3]#
Improvements
Updated function SIM_GetUniqueId to support different register names.
[2.1.2]#
Bug Fixes
Fixed SIM_GetUniqueId bug that could not get UIDH.
[2.1.1]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules 10.1, 10.4
[2.1.0]#
Improvements
Added new APIs: SIM_GetRfAddr() and SIM_EnableSystickClock().
[2.0.0]#
Initial version.
SMC#
[2.0.9]#
Bug Fixes
Replace width-unsafe register mask inversion with a
smc_reg_t-aware helper for INT31-C compliance
[2.0.8]#
Bug Fixes
Replace direct boolean to integer casts with explicit ternary operators for INT31-C compliance
Add validation before narrowing uint32_t to uint8_t conversion using assert
Add INT31-C compliance comments for safe type handling
Apply fixes to RCM_ConfigureResetPinFilter and RCM_SetForceBootRomSource functions
[2.0.7]#
Bug Fixes
Fixed MISRA-2012 issue 10.3.
[2.0.6]#
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule 10.3, rule 11.3.
[2.0.5]#
Bug Fixes
Fixed issue for MISRA-2012 check.
Fixed rule 15.7, rule 14.4, rule 10.3, rule 10.1, rule 10.4.
[2.0.4]#
Bug Fixes
When entering stop modes, used RAM function for the flash synchronization issue. Application should make sure that, the RW data of fsl_smc.c is located in memory region which is not powered off in stop modes.
[2.0.3]#
Improvements
Added APIs SMC_PreEnterStopModes, SMC_PreEnterWaitModes, SMC_PostExitWaitModes, and SMC_PostExitStopModes.
[2.0.2]#
Bug Fixes
Added DSB before WFI while ISB after WFI.
Other Changes
Updated SMC_SetPowerModeVlpw implementation.
[2.0.1]#
Other Changes
Updated for KL8x.
[2.0.0]#
Initial version.
TRGMUX#
[2.0.1]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules 10.1, 10.3, 10.8.
[2.0.0]#
Initial version.
TSI_V5#
[2.6.2]#
Bug Fixes
Fixed the violations of CERT INT31-C rule.
[2.6.1]#
Improvements
The SHIELD register write was fixed to be rewritten.
[2.6.0]#
Improvements
Add API TSI_ShieldChannelConfig to config all TSI shield channels.
[2.5.0]#
Improvements
Add API TSI_EnableShieldChannels to enable/disable TSI shield channels.
[2.4.0]#
Bug Fixes
Fixed some elements in the array tsi_sensitivity_xdn_option_t does not match the S_XDN bits.
[2.3.0]#
Other Changes
Changed the TSI SINC cutoff divider number.
[2.2.0]#
Improvements
Extended enableShield items from tsi_selfCap_config_t structure to cover three shields in the ke17z series.
Added interface for getting instance from TSI base address and apply it for clock and IRQ enable/disable.
[2.1.2]#
Bug Fixes
Fixed the violations of MISRA C-2012 rules: 10.1, 10.8.
[2.1.1]#
Improvements
Improved the module’s noise immunity in mutual cap mode by setting M_TRIM2[0] to 1 in TSI_MUL1 register.
Bug Fixes
Fixed the violations of MISRA C-2012 rules:
Rule 10.1, 10.3, 10.4, 10.8, 12.2, 14.4, 17.7.
[2.1.0]#
Bug Fixes
Fixed incorrect TSI SSC clock calculation.
[2.0.1]#
Improvements
Added functions for M_TX_USED bitfield for ke16z only (Unused TX mutual pins can work as GPIO).
[2.0.0]#
Initial version.
UART#
[2.5.2]#
New Features
Added common IRQ handler entry UART_DriverIRQHandler.
[2.5.1]#
Improvements
Use separate data for TX and RX in uart_transfer_t.
Bug Fixes
Fixed bug that when ring buffer is used, if some data is received in ring buffer first before calling UART_TransferReceiveNonBlocking, the received data count returned by UART_TransferGetReceiveCount is wrong.
[2.5.0]#
New Features
Added APIs UART_GetRxFifoCount/UART_GetTxFifoCount to get rx/tx FIFO data count.
Added APIs UART_SetRxFifoWatermark/UART_SetTxFifoWatermark to set rx/tx FIFO water mark.
Bug Fixes
Fixed bug of race condition during UART transfer using transactional APIs, by disabling and re-enabling the global interrupt before and after critical operations on interrupt enable registers.
Fixed DMA/eDMA transfer blocking issue by enabling tx idle interrupt after DMA/eDMA transmission finishes.
[2.4.0]#
New Features
Added APIs to configure 9-bit data mode, set slave address and send address.
[2.3.0]#
Bug Fixes
Fixed the bug that, when framing/parity/noise/overflow flag or idle line detect flag is set, receive FIFO should be flushed to avoid FIFO pointer being in unknown state, since FIFO has no valid data.
Improvements
Modified UART_TransferHandleIRQ so that txState will be set to idle only when all data has been sent out to bus.
Modified UART_TransferGetSendCount so that this API returns the real byte count that UART has sent out rather than the software buffer status.
Added timeout mechanism when waiting for certain states in transfer driver.
[2.2.0]#
New Features
Added UART hardware FIFO enable/disable API.
Improvements
Added check for kUART_TransmissionCompleteFlag in UART_TransferHandleIRQ, UART_SendEDMACallback and UART_TransferSendDMACallback to ensure all the data would be sent out to bus.
Bug Fixes
Eliminated IAR Pa082 warnings from UART_TransferGetRxRingBufferLength, UART_GetEnabledInterrupts, UART_GetStatusFlags and UART_TransferHandleIRQ.
Added code in UART_ReadBlocking so that if more than one receiver errors occur, all status flags will be cleared and the most severe error status will be returned.
Fixed MISRA issues.
Fixed rules 10.1, 10.3, 10.4, 14.4, 11.6, 17.7.
[2.1.6]#
Bug Fixes
Fixed the issue of register’s being in repeatedly reading status while performing the IRQ routine.
[2.1.5]#
Improvements
Added hardware flow control function support.
Added idle-line-detecting feature in UART_TransferNonBlocking function. If an idle line is detected, a callback will be triggered with status kStatus_UART_IdleLineDetected returned. This feature may be useful when the number of received bytes is less than the expected receive data size. Before triggering the callback, data in the FIFO is read out (if it has FIFO), and no interrupt will be disabled except for the case that the receive data size reaches 0.
Enabled the RX FIFO watermark function. With the idle-line-detecting feature enabled, you can set the watermark value to whatever you want (should not be bigger than the RX FIFO size). Data is then received and a callback will be triggered when data receive ends.
[2.1.4]#
Improvements
Changed parameter type in UART_RTOS_Init() struct rtos_uart_config –> uart_rtos_config_t.
Bug Fixes
Disabled UART receive interrupt instead of global interrupt when reading data from ring buffer. With ring buffer used, receive nonblocking will disable global interrupt to protect the ring buffer. This has a negative effect on other IPs using interrupt.
[2.1.3]#
New Features
Added RX framing error and parity error status check when using interrupt transfer.
[2.1.2]#
Bug Fixes
Fixed baud rate fine adjust bug to make the computed baud rate more accurate.
[2.1.1]#
Bug Fixes
Removed needless check of event flags and assert in UART_RTOS_Receive.
Always waited for RX event flag in UART_RTOS_Receive.
[2.1.0]#
Improvements
Added transactional API.
[2.0.0]#
Initial version.
UART_EDMA#
[2.5.2]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules.
[2.5.1]#
Bug Fixes
Fixed violations of the MISRA C-2012 rules.
[2.5.0]#
Refer UART driver change log 2.1.0 to 2.5.0
WDOG32#
[2.2.1]#
Bug Fixes
Fix CERT INT31-C that the bool value shall be converted to unsigned int 0 or 1 then passed to registers.
Fix MISRA 2012 20.3 vilation.
[2.2.0]#
Improvements
Added while loop timeout config value for WDOG32 reconfiguration and unlock sequence.
Change the return type of WDOG32_Init, WDOG32_Deinit and WDOG32_Unlock from void to status_t.
[2.1.0]#
Improvements
Release peripheral from reset if necessary in init function.
[2.0.4]#
Improvements
To ensure that the reconfiguration is inside 128 bus clocks unlock window, put all re-configuration APIs in quick access code section.
[2.0.3]#
Bug Fixes
Fixed the noncompliance issue of the reference document.
Waited until for new configuration to take effect by checking the RCS bit field.
Waited until for registers to be unlocked by checking the ULK bit field.
Improvements
Added 128 bus clocks delay ensures a smooth transition before restarting the counter with the new configuration when there is no RCS status bit.
[2.0.2]#
Bug Fixes
MISRA C-2012 issue fixed.
Fixed rules, containing: rule-10.3, rule-14.4, rule-15.5.
Fixed the issue of the inseparable process interrupted by other interrupt source.
WDOG32_Refresh
[2.0.1]#
Bug Fixes
WDOG must be configured within its configuration time period.
Added WDOG32_Init API to quick access section.
Defined register variable in WDOG32_Init API.
[2.0.0]#
Initial version.