MCUXpresso SDK Release Notes#
Development tools#
The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.
SDK 25.12.00 is the final release that includes MCUXpresso IDE support for KW4x devices. Beginning with SDK 26.x.x, MCUXpresso IDE will no longer be supported for KW4x development, and MCUXpresso for Visual Studio Code will become the recommended integrated development environment.
IAR Embedded Workbench for Arm, version is 9.70.4
MCUXpresso for VS Code v26.06
GCC Arm Embedded Toolchain 14.2.x
Supported development systems#
This release supports board and devices listed in following table. The board and devices in bold were tested in this release.
Development boards |
MCU devices |
|---|---|
KW45B41Z-EVK |
KW45B41Z82AFPA, KW45B41Z82AFTA, KW45B41Z83AFPA, |
MCUXpresso SDK release package#
The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.
Device support#
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.
Board support#
The boards folder provides the board-specific demo applications, driver examples, and middleware examples.
Demo application and other examples#
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
RTOS#
FreeRTOS#
Real-time operating system for microcontrollers from Amazon
Middleware#
GenFSK link layer#
The Generic FSK protocol enables radio operation using a custom GFSK/GMSK or MSK modulation format.
Main Features supported:
Highly configurable packet structure
Optimized Sequence Command Set
High-precision timebase to maintain network timing
Two timer-compare mechanisms for Interrupt Generation and Sequence Launching
Hardware automation for packet transmit and receive, CRC and Whitening
Up to four network addresses to synchronize to, can be 8-bit, 16-bit or 32-bit
Packet Lengths up to 2047 Bytes
Support complex auto-sequence, like CCA before TX, Auto-ACK, TR.
Many operating modes can support the sending and receiving of multiple protocol packets, such as Bluetooth LE.
Wireless XCVR#
The XCVR component provides a base Transceiver Driver for the 2.4 GHz narrowband radio.
Bluetooth LE Controller#
Main features supported:
Peripheral Role
Central Role
Multiple PHYs (1 Mbps, 2 Mbps, Coded PHY)
Asymmetric Connections
Public/Random/Static Addresses
Network/Device Privacy Modes
Extended Advertising
Extended Scanning
Passive/Active Scanning
LE Encryption
LE Ping Procedure
HCI Test Interface
UART Test Interface
Randomized Advertising Channel Indexing
ADI Field in Scan Response Data
HCI Support for Debug Keys in LE - Secure Connections
Main capabilities supported:
Simultaneous scanning 1 Mbps and Long Range
Scanning and advertising in parallel
24 connections as a central role
24 connections as a peripheral role
Any combination of central and peripheral roles (24 connections maximum)
8 connections with a 7.5 ms connection interval
Five advertising sets in parallel.
26 Accept List entries
36 Resolvable Private Address (RPA) entries
Up to two Chain Packets per Extended Advertising set
Enhanced Notification on end of - Scanning/Advertising/Connection events
Connection event counters associated to Bluetooth LE packet reception
Timestamp associated to Bluetooth LE packet reception
RF channel info associated to Bluetooth LE packet reception
NXP proprietary Bluetooth LE Handover feature
Decision Based Advertising Filtering (DBAF)
Advertising Coding Selection (ACS)
Periodic Advertising with Responses (PAwR) Additional features supported for KW47 and MCX W72 devices:
Channel Sounding
RTT_PHY capability
Channel Sounding Enhancement 1
Channel Sounding TX/SNR (18 dB, 21 dB, 24 dB and 27 dB)
Channel Sounding PHY 2 Mbit/s BT 2.0
Channel Sounding additional supported timings:
T_PM=10us
T_IP1/T_IP2=60, 50, 30
T_FCS=120, 100, 60
LL Extended Feature Set
Monitoring Advertisers
Randomized Resolvable Private Address (\RPA)
LE Enhanced Connection Update Additional features supported as EAR (\Early Access Release) in the KW47 experimental build:
Inline PCT Transfer (\IPT) Additional features supported as EAR (\Early Access Release) in the KW45/KW47 experimental builds:
LE Test Mode Enhancement (\UTP/OTA).
LE Power Control (\LEPC).
Note: Project configuration enabling Experimental features on KW45 and MCX W71 requires the Radio Subsystem (NBU) Firmware to be reprogrammed with the firmware provided in the SDK under \middleware\wireless\ble_controller\bin\experimental\. For NBU programming steps, see the EVK Quick Start Guide and Secure Provisioning SDK (SPSDK) documentation.
Project configurations that require usage of the Bluetooth LE controller including all Bluetooth LE examples require the Radio Subsystem (NBU) Firmware to be re-programmed with the firmware provided in the SDK under middleware\wireless\ble_controller\bin.
Bluetooth LE Host Stack and Applications#
The Bluetooth LE Host Stack component provides an implementation for a Bluetooth 6.0 mandatory and some optional, proprietary, and experimental features. The Bluetooth LE Host Stack component provides application examples, services, and profiles.
Main features supported:
Automotive Compliance
MISRA Compliance
HIS CCM <= 20
Advanced Secure Mode
Enhanced ATT
GATT Caching
GCC Libraries
IAR Libraries
Bluetooth LE Peripheral Libraries
Bluetooth LE Central Libraries
Bluetooth LE Full Host Features Libraries
Bluetooth LE Host Optional Features Libraries
Bluetooth LE Host Mandatory Features Libraries
BareMetal and FreeRTOS Support
Full Privacy Support
NCP Mode - FSCI Application
Enhanced Notifications
Dynamic Database
OTA Support - Sample Applications
Decision based Advertising Filtering (DBAF)
Advertising Coding Selection (ACS)
Periodic Advertising with Responses (PAwR)
Encrypted Advertising Data (EAD)
Monitoring Advertisers
Randomized RPA - Experimental feature
Intrusion Detection System (IDS) - Experimental feature
Note: The CDE(Complex-domain Distance Estimation) algorithm is an experimental feature intended only for testing purposes. It is not maintained and must not be included in production environments.
Note: “RADE (Ranging Distance Estimation) is NXP’s embedded Channel Sounding (CS) ranging algorithm. RADE is intended for non-U.S. markets and should not be used in U.S. market deployments. RADEX is the U.S.-market variant of the RADE algorithm.”
Connectivity framework#
The Connectivity Framework is a software component that provides hardware abstraction modules to the upper layer connectivity stacks and components. It also provides a list of services and APIs (see Supported services). The Connectivity Framework modules are located in the middleware\wireless\framework SDK folder.
Supported services#
FSCI - Framework Serial Communication Interface
FunctionLib - Common function library utilities
HWParameter - Hardware parameter management
LowPower - Low power mode management
ModuleInfo - Module information and versioning
NVS - Non-Volatile Storage
NVM - Non-Volatile Memory management
OtaSupport - Over-The-Air update support
SecLib_RNG - Security library and Random Number Generator
Sensors - Sensor abstraction layer
SFC - Smart Frequency Calibration
WorkQ - Work queue management
Supported platform#
KW45_MCXW71
KW47_MCXW72
MCXW23
RW61X
RT1060 and RT1170
i.MX RT595s
Advanced features supported on platforms#
KW45_MCXW71#
FRO32K with smart frequency calibration (see SFC)
Power down mode support (for evaluation only)
KW47_MCXW72#
FRO32K with smart frequency calibration (see SFC)
Power down mode support (for evaluation only)
Crystal 32M trimming with temperature
Debug module for NBU
Extended NBU support with SecLib and pseudo RNG support
CMSIS DSP Library#
The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.
TF-M#
Trusted Firmware - M Library
PSA Test Suite#
Arm Platform Security Architecture Test Suite
secure_storage#
secure_storage
EdgeLock SE050 Plug and Trust Middleware#
Secure subsystem library - SSS APIs
Multicore#
Multicore Software Development Kit
NXP IoT Agent#
NXP IoT Agent
mbedTLS#
mbedtls SSL/TLS library v3.x
mbedTLS#
mbedtls SSL/TLS library v2.x
LittleFS#
LittleFS filesystem stack
LIN Stack#
LIN Stack middleware
FreeMASTER#
FreeMASTER communication driver for 32-bit platforms.
NXP PSA CRYPTO DRIVER#
PSA crypto driver for crypto library integration via driver wrappers
Release contents#
Provides an overview of the MCUXpresso SDK release package contents and locations.
Deliverable |
Location |
|---|---|
Boards |
INSTALL_DIR/boards |
Demo Applications |
INSTALL_DIR/boards/<board_name>/demo_apps |
Driver Examples |
INSTALL_DIR/boards/<board_name>/driver_examples |
eIQ examples |
INSTALL_DIR/boards/<board_name>/eiq_examples |
Board Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/boards/<board_name>/project_template |
Driver, SoC header files, extension header files and feature header files, utilities |
INSTALL_DIR/devices/<device_name> |
CMSIS drivers |
INSTALL_DIR/devices/<device_name>/cmsis_drivers |
Peripheral drivers |
INSTALL_DIR/devices/<device_name>/drivers |
Toolchain linker files and startup code |
INSTALL_DIR/devices/<device_name>/<toolchain_name> |
Utilities such as debug console |
INSTALL_DIR/devices/<device_name>/utilities |
Device Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/devices/<device_name>/project_template |
CMSIS Arm Cortex-M header files, DSP library source |
INSTALL_DIR/CMSIS |
Components and board device drivers |
INSTALL_DIR/components |
RTOS |
INSTALL_DIR/rtos |
Release Notes, Getting Started Document and other documents |
INSTALL_DIR/docs |
Tools such as shared cmake files |
INSTALL_DIR/tools |
Middleware |
INSTALL_DIR/middleware |
What is new#
The following updates were implemented with respect to the previous SDK release version (26.09.00).
Bluetooth LE Host Stack and Applications
Note: Version 1.10.23 is the first NXP Bluetooth LE Host release officially certified according to the Bluetooth® Core Specification Version 6.3.
Added
Low Energy (LE) Power Control can now be enabled/disabled at application level via
gHostInclusionLePowerControl_d.
Improved
Handover time synchronization optimization.
Fixed
Handover: correctly handle
gHandoverAnchorSearchStartLl_con supervision timeout.Fixed Host Privacy scan response data length mismatch (31 versus 17 bytes).
Miscellaneous Coverity fixes.
Miscellaneous CERT-C fixes.
Miscellaneous MISRA fixes.
Miscellaneous MSG fixes.
Changed
Added application-level mitigation for Bluetooth Low Energy Re-Pairing (BLERP) forced re-pairing attacks.
Details can be found in github repository nxp-mcuxpresso/mcuxsdk-middleware-bluetooth-host/CHANGELOG.md.
Bluetooth LE Controller
Fixed EBQ failure — packet time restrictions not applied after LL_PHY_RSP (LL/CON/PER/BV-53-C). PAwR:
Fixed memory leak in PAWR. Handover:
Fixed issue where connection anchor start time computation for small connection intervals (at connection parameter update procedure during Received Signal Strength Indicator (RSSI) monitoring) was not correct.
Enhancement: removed one extra RX window in some cases during RSSI monitoring to save power.
Enhancement: updated handover anchor search command to reduce the HCI traffic and apply RX latency during RSSI monitoring for low power.
Fixed an issue where after connection handover the connection update procedure causes a disconnection. Genfsk:
Fixed issue where timestamp was invalid after running over 72 minutes. LEPC:
Fixed EBQ LEPC coded phy tests (LL/PCL/CEN/BV-36-C, LL/PCL/CEN/BV-40-C, LL/PCL/PER/BV-29-C, LL/PCL/PER/BV-40-C).
Transceiver Drivers (XCVR)
Added API to control Power Amplifier (PA) ramp type and duration.
Connectivity framework
Major Changes
[NVM] Refactored NVM handling to centralize address computation using offset-based flash access helpers (
*_AtOffset) instead of stored flash addresses, reducing unsafe pointer arithmetic.NvUpdateSize()now returnsuint16_t, addedNV_PartitionBlankCheckAtOffset(), and deprecatedNvIsMemoryAreaBlank(). Also fixed a data integrity issue inNvSaveAllDataSetEntry()and various Coverity/CERT-C findings.[platform] IFR BLE BD address is now reversed to match the BLE Host stack expectation. The
PLATFORM_IFR_BD_ADDR_IS_MSB_FIRSToption was removed with the reverse loop reworked accordingly.[OTA] Introduced
gOtaEraseWholePartitionOnInit_doption (KW43 only, disabled by default) to erase the whole OTA partition at start of image transfer.[wireless_mcu] Replaced the critical section in
PLATFORM_RemoteActiveReq()andPLATFORM_RemoteActiveRel()with a shared mutex to reduce critical section duration. These APIs must not be called from ISR anymore.[wireless_nbu] Updated the low power callback to check for pending RPMSG buffers so the NBU enters WFI only when a Tx message is pending, reducing main core latency.
Minor Changes
[platform][zephyr] Zephyr feature flag overrides are now owned by the framework repo in a per platform
configs/fwk_config_zephyr.h, included at the top offwk_config.hunder__ZEPHYR__, removing the dual maintenance with the Zephyr integration. Platforms: kw43_mcxw70, kw45_k32w1_mcxw71, kw47_mcxw72, mcxw23, rw61x.[NVS] Replaced
memcpy()byHAL_FlashRead()for internal flash reads so that HAL checks and Async Flash mode synchronization are not bypassed.[wireless_mcu] Added the missing
fwk_config.has first include in the kw43_mcxw70, kw45_k32w1_mcxw71 and kw47_mcxw72 platform files so that feature flag overrides are taken into account.[settings] Added IAR compiler support for iterable sections and disabled the
SETTINGS_NAME_ENDIAR warning.[SecLib_RNG] Added to
RNG_psa.cseed support including WorkQueue-based automatic reseedinggRngEnableAutoReseed_d, NBU seed forwarding viaPLATFORM_SendRngSeed(), reseed counter logicgRngMaxRequests_d, and new APIsRNG_NotifyReseedNeeded()andRNG_IsReseedNeeded().[OTA] Added a blank check of the OTA partition to avoid unnecessary erase operations and refactored
OTA_MakeHeadRoom().
Bug Fixes
[WorkQ] Increased the default
FWK_SYSWORKQ_STACK_SIZEfrom 608 to 640 bytes to fix a stack overflow on the system work queue thread.[platform][TSTMR] Fixed the 56 bit version of the timestamp, now reading the TSTMR instance base and testing only the base pointer validity.
[wireless_mcu] Fixed FRO6M calibration by replacing
FWK_MRCC_TSTMR0_CC/FWK_MRCC_TSTMR0_MUXmacros withMRCC_CC/MRCC_MUXfromfsl_clock.hand preserving the MUX clock selection inPLATFORM_StartFro6MCalibration().[zephyr][lib][crc] Fixed build conflict with EdgeFast OPN CRC by guarding CRC sources with the Zephyr common framework component check to avoid symbol redefinition.
[NVM] Fixed offset validation in
NvGetEntryFromDataPtr()and corrected the bottom record address calculation inNvGetPageFreeSpace()whengUnmirroredFeatureSet_dis undefined.[docs] Fixed Sphinx/docutils warnings and errors in the framework documentation.
[SFC] Prevent unnecessary SFA measurement retrieval when SFC is disabled by adding a check in the SFC ISR to verify that the SFC module is enabled before retrieving the SFA frequency measurement.
[Coverity] Various Coverity compliance fixes in SecLib (DHKey handling in
SecLib_GenerateBluetoothF5KeysSecure()) and OTA (replaced union with structure for callback/argument passing in message buffer).[MISRA][CERT-C] Various MISRA, CERT-C and Coverity compliance fixes gathered across platform, LowPower, ICS (wireless_mcu and wireless_nbu), OTA, FSCI, SFC, SecLib and NVM modules.
Known issues#
This section lists the known issues, limitations, and/or workarounds.
FRO6M Clock Stability Issue#
According to ERRATA ERR052742, the FRO6M clock is not stable on some parts. FRO6M outputs lower frequency signal instead of 6MHz when device is reset or wakes up from low power. It can impact peripherals using it as a clock source.
Impact on TSTMR Module#
The TSTMR (Time Stamp Timer) module exclusively uses the FRO6M clock source. Due to the aforementioned stability issues, avoid using TSTMR-related APIs if your application requires high-precision timing.
Recommendation#
For applications requiring precise timing, consider using alternative timer modules that support more stable clock sources.
New project wizard compile failure#
The following components request the user to manually select other components that they depend upon in order to compile. These components depend on several other components and the New Project Wizard (NPW) is not able to decide which one is needed by the user.
Note: xxx means core variants, such as, cm0plus, cm33, cm4, cm33_nodsp.
Also for low-level adapter components, currently the different types of the same adapter cannot be selected at the same time. For example, if there are two types of timer adapters, gpt_adapter and pit_adapter, only one can be selected as timer adapter in one project at a time. Duplicate implementation of the function results in an error.
Only FreeRTOS is tested for RTOS support#
This release only supports the FreeRTOS kernel and a bare-metal non-preemptive task scheduler.
Bluetooth LE#
Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h header file.
Bluetooth LE controller:#
The maximum Advertising data length is limited to:
800 bytes for KW45/KW47
31 bytes for KW43.
The scanner may sporadically miss some chained packets.
Periodic Advertising with Responses (PAwR):
Periodic Advertising with Response (PAwR) is not supported with the configuration “Subevent Interval = Number of Response Slots x Response Slot Spacing with Response Slot Spacing = 0x2”.
The feature is not functional with the Free-Running Oscillator (FRO32K); it requires a 32 KHz Crystal Oscillator with accuracy less than 50 ppm.
KW43:
CS performances are not yet guaranteed.
KW45 / MCXW 71: No specific issues.
KW47 / MCX W72: Channel Sounding (CS): Information:
RF Bandwidth Occupancy and Connections/Channel Sounding Activities: The RF bandwidth occupancy is tightly coupled with configured activities, including the number of connections, connection event durations, the number of Channel Sounding (CS) procedures, and related CS parameters (e.g., subevent length, repeat mode). The Link Layer Scheduler is responsible for allocating RF bandwidth to these activities, optimizing bandwidth utilization. However, because each activity operates on its own timing constraints, some RF collisions are expected. This is inherent to the Bluetooth LE protocol, particularly when peripheral roles are configured, as anchor placement is controlled by the central peer devices. The application controls several timing parameters, such as connection interval and subevent length. To optimize user experience, the Link Layer expects the application to adjust these parameters to achieve the best RF bandwidth occupancy with the lowest occurrence of RF collisions.
Limitations:
RTT with Sounding Sequence is not supported.
Maximum 6 Channel Sounding procedures are supported in parallel.
Phase measurement bias is within certification range (<1.7x2πns) with KW47 EVK board. However, if different PCB or antenna matching is used, some bias may appear due to increased delay.
For experimental feature IPT(Inline PCT Transfer), only 1x1 configuration is supported.
Channel Sounding Channel Map Update procedure may not function when high value of subrate factor and latency is used.
Known issues:
When CS Subevents are configured very close from each other (<700us), some Subevents may be aborted with reason 0x3.
When CS offset is configured too close from ACL anchor point, the anchor point may not be served (TX on central or RX on peripheral will not happen). Ideally, CS Offset should be configured greater than 1ms.
RTT bias compensation:
For parts not properly configured at production (IFR blank), RTT bias is not compensated properly. Consequently, an inaccuracy of +/-2m can be observed.
Pairing procedure fails to complete after connection is established. Affects digital_key sample applications. Increase
gHost_TaskStackSize_cto1900U.Channel Sounding measurement cannot start after handover. Affects digital_key sample applications.
For the digital_key_car_anchor_cs and digital_key_device_cs BM applications on KW47EVK and KW47LOC, and the loc_reader BM application on KW47EVK, MCXW72EVK, and FRDMMCXW72, increase stack_size in board_reconfig.cmake from 0x0CE4 to 0x1194 (4500 bytes). This change is required to avoid runtime stack overflow that can lead to a HardFault.
LIN New Project Wizard (NPW) issue#
The lin (LIN Driver) and lin_stack (LIN Stack Driver) drivers components should not be enabled at the same time while creating the new projects in MCUXpresso. Otherwise there will be the compiling issue.
The lin_stack (LIN Stack Driver) is not actually a driver. It is an adapt layer for LIN Stack middleware to adapt to the low level lpuart driver and cannot be used in NPW alone. So, select the LIN Stack middleware and then the lin_stack is selected automatically since it is required by LIN Stack middleware. Besides, customer need to add the lin_cfg.c/h in application layer for user definition of frame data and add FSL_SDK_LIN_STACK_ENABLE=1 in MCUXpresso preprocessor, otherwise the compiling of LIN Stack will report error.
Flash ROMAPI#
Note that:
If using ROM API for internal flash or SPI NOR operation, reserve RAM location 0x200030A0 - 0x200032CF (
0x300030A0-0x300032CF).If using kb API, reserve
0x20002000-0x200032FF(0x30002000-0x300032FF).
Other limitations#
The following Connectivity Framework configurations are Experimental and not recommended for mass production:
Power down on application power domain.
GenFSK
Connectivity_testapplication is not operational with Low Power enabled.Serial manager is only supported on UART (not I2C nor SPI).
If the FRO32K is configured as the clock source of the CM33 Core then the debug session will block in IAR CMSIS-DAP while debugging. Use a lower debug wire speed, for example 1 MHz instead of the default one.
In IAR, the option is in Runtime Checking -> Debugger -> CMSIS DAP -> Interface -> Interface speed.
Examples hello_world_ns, secure_faults_ns, and secure_faults_trdc_ns have incorrect library path in GUI projects#
When the affected examples are generated as GUI projects, the library linking the secure and non-secure worlds has an incorrect path set. This causes linking errors during project compilation.
Examples: hello_world_ns, hello_world_s, secure_faults_ns, secure_faults_s, secure_faults_trdc_ns, secure_faults_trdc_s
Affected toolchains: mdk, iar
Workaround: In the IDE project settings for the non-secure (_ns) project, find the linked library (named hello_world_s_CMSE_lib.o, or similar, depending on the example project) and replace the path to the library with <build_directory>/<secure_world_project_folder>/<IDE>/, replacing the subdirectory names with the build directory, the secure world project name, and IDE name.
El2go examples on kw45b41zevk#
The el2go examples are executed on socketed board with KW45 samples instead of actual EVKs.
Examples: el2go_blob_test, el2go_import_blob
Affected toolchains: All