MCUXpresso SDK Documentation

MCUXpresso SDK Release Notes#

Development tools#

The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.

  • MCUXpresso IDE, Rev. 25.06.xx

  • IAR Embedded Workbench for Arm, version is 9.70.4

  • Keil MDK, version is 5.43a

  • MCUXpresso for VS Code v26.06

  • GCC Arm Embedded Toolchain 14.2.x

Supported development systems#

This release supports board and devices listed in following table. The board and devices in bold were tested in this release.

Development boards

MCU devices

MCX-N5XX-EVK

MCXN546VAB, MCXN546VDF, MCXN546VKL,
MCXN546VNL, MCXN546VPB, MCXN547VAB,
MCXN547VDF, MCXN547VKL, MCXN547VNL,
MCXN547VPB

MCUXpresso SDK release package#

The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.

Device support#

The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.

Board support#

The boards folder provides the board-specific demo applications, driver examples, and middleware examples.

Demo application and other examples#

The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.

RTOS#

FreeRTOS#

Real-time operating system for microcontrollers from Amazon

Middleware#

CMSIS DSP Library#

The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.

Wireless EdgeFast Bluetooth PAL#

For more information, see the MCUXpresso SDK EdgeFast Bluetooth Protocol Abstraction Layer User’s Guide.

Wireless EdgeFast Bluetooth PAL will be deprecated starting with SDK v26.09.00.

SDK EdgeFast v26.06.00 is classified as a Long Term Support (LTS).

Ethermind BT/BLE Stack#

nxp_bt_ble_stack

coreMQTT#

Lightweight MQTT client library for IoT devices from the AWS IoT Device SDK.

coreJSON#

Strictly conforming RFC 8259 JSON parser library from the AWS IoT Device SDK.

coreHTTP#

coreHTTP

NXP Wi-Fi#

The MCUXpresso SDK provides driver for NXP Wi-Fi external modules. The Wi-Fi driver is integrated with LWIP TCPIP stack and demonstrated with several network applications (iperf and AWS IoT).

For more information, see Getting Started with NXP based Wireless Modules and i.MX RT Platform Running on RTOS (document: UM11441).

USB Type-C PD Stack#

See the MCUXpresso SDK USB Type-C PD Stack User’s Guide (document MCUXSDKUSBPDUG) for more information

USB Host, Device, OTG Stack#

See the MCUXpresso SDK USB Stack User’s Guide (document MCUXSDKUSBSUG) for more information.

Peripheral devices tested with USB Host stack#

Table 1 provides a list of USB devices tested with the USB Host stack.

Device type

Device

USB HUB

BELKIN F5U233BELKIN F5U304BELKIN F5U307BELKIN F4U040UNITEK Y-2151Z-TEK ZK032AHYUNDAI HY-HB608

USB flash drive

ADATA C008 32 GBADATA S102 8 GADATA S102 16 GVerbatim STORE N GO USB Device 8 GKingston DataTraveler DT101 G2SanDisk Cruzer Blade 8 GBUnisplendour 1 GImation 2 GBV-mux 2 GBSanmina-SCI 128 MCorporate Express 1 GTOSHIBA THUHYBS-008G 8 GTranscend JF700 8 GNetac U903 16 GSSK SFD205 8 GBRex 4 GBSAMSUNG USB3.0 16GB

USB card reader/adapter

SSK TF adapterKawau Multi Card ReaderKawau TF adapterKawau SDHC cardUSB Mouse DELL MS111-PDELL M066U0ADELL MUAVDEL8TARGUS AMU76APDELL MD56U0DELL MS111-TRAPOO M110

USB Keyboard

DELL SK8135DELL SK8115

NXP Touch Library#

NXP Touch Library

TinyCBOR#

Concise Binary Object Representation (CBOR) Library

TF-M#

Trusted Firmware - M Library

PSA Test Suite#

Arm Platform Security Architecture Test Suite

SDMMC stack#

The SDMMC software is integrated with MCUXpresso SDK to support SD/MMC/SDIO standard specification. This also includes a host adapter layer for bare-metal/RTOS applications.

PKCS#11#

The PKCS#11 standard specifies an application programming interface (API), called “Cryptoki,” for devices that hold cryptographic information and perform cryptographic functions. Cryptoki follows a simple object based approach, addressing the goals of technology independence (any kind of device) and resource sharing (multiple applications accessing multiple devices), presenting to applications a common, logical view of the device called a “cryptographic token”.

NXP IoT Agent#

NXP IoT Agent

Multicore#

Multicore Software Development Kit

MCU Boot#

Open source MCU Bootloader.

mbedTLS#

mbedtls SSL/TLS library v3.x

Voice intelligent technology library#

Voice Intelligent Technology (VIT) Library provides wake word and voice command engine for voice control

Audio Voice components#

Audio Voice components for MCU

Maestro Audio Framework for MCU#

Maestro Audio Framework library for MCU

mbedTLS#

mbedtls SSL/TLS library v2.x

lwIP#

The lwIP TCP/IP stack is pre-integrated with MCUXpresso SDK and runs on top of the MCUXpresso SDK Ethernet driver with Ethernet-capable devices/boards.

For details, see the lwIP TCPIP Stack and MCUXpresso SDK Integration User’s Guide (document MCUXSDKLWIPUG).

lwIP is a small independent implementation of the TCP/IP protocol suite.

eIQ#

The package contains several example applications using the eIQ TensorFlow Lite for Microcontrollers library.

eIQ machine learning SDK containing:

  • Arm CMSIS-NN library (neural network kernels optimized for Cortex-M cores)

  • Inference engines:

    • TensorFlow Lite Micro

    • DeepView RT

  • Example code for TensorFlow Lite Micro, Glow, and DeepView RT

LVGL#

LVGL Open Source Graphics Library

llhttp#

HTTP parser llhttp

LittleFS#

LittleFS filesystem stack

FreeMASTER#

FreeMASTER communication driver for 32-bit platforms.

File systemFatfs#

The FatFs file system is integrated with the MCUXpresso SDK and can be used to access either the SD card or the USB memory stick when the SD card driver or the USB Mass Storage Device class implementation is used.

emWin#

The MCUXpresso SDK is pre-integrated with the SEGGER emWin GUI middleware. The AppWizard provides developers and designers with a flexible tool to create stunning user interface applications, without writing any code.

NXP PSA CRYPTO DRIVER#

PSA crypto driver for crypto library integration via driver wrappers

NXP ELS PKC#

ELS PKC crypto library

Release contents#

Provides an overview of the MCUXpresso SDK release package contents and locations.

Deliverable

Location

Boards

INSTALL_DIR/boards

Demo Applications

INSTALL_DIR/boards/<board_name>/demo_apps

Driver Examples

INSTALL_DIR/boards/<board_name>/driver_examples

eIQ examples

INSTALL_DIR/boards/<board_name>/eiq_examples

Board Project Template for MCUXpresso IDE NPW

INSTALL_DIR/boards/<board_name>/project_template

Driver, SoC header files, extension header files and feature header files, utilities

INSTALL_DIR/devices/<device_name>

CMSIS drivers

INSTALL_DIR/devices/<device_name>/cmsis_drivers

Peripheral drivers

INSTALL_DIR/devices/<device_name>/drivers

Toolchain linker files and startup code

INSTALL_DIR/devices/<device_name>/<toolchain_name>

Utilities such as debug console

INSTALL_DIR/devices/<device_name>/utilities

Device Project Template for MCUXpresso IDE NPW

INSTALL_DIR/devices/<device_name>/project_template

CMSIS Arm Cortex-M header files, DSP library source

INSTALL_DIR/CMSIS

Components and board device drivers

INSTALL_DIR/components

RTOS

INSTALL_DIR/rtos

Release Notes, Getting Started Document and other documents

INSTALL_DIR/docs

Tools such as shared cmake files

INSTALL_DIR/tools

Middleware

INSTALL_DIR/middleware

Known issues#

This section lists the known issues, limitations, and/or workarounds.

New project wizard compile failure#

The following components request the user to manually select other components that they depend upon in order to compile. These components depend on several other components and the New Project Wizard (NPW) is not able to decide which one is needed by the user.

Note: xxx means core variants, such as, cm0plus, cm33, cm4, cm33_nodsp.

Also for low-level adapter components, currently the different types of the same adapter cannot be selected at the same time. For example, if there are two types of timer adapters, gpt_adapter and pit_adapter, only one can be selected as timer adapter in one project at a time. Duplicate implementation of the function results in an error.

Only FreeRTOS is tested for RTOS support#

This release only supports the FreeRTOS kernel and a bare-metal non-preemptive task scheduler.

Bluetooth LE#

Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h header file.

Bluetooth LE controller:#

  • The maximum Advertising data length is limited to:

    • 800 bytes for KW45/KW47

    • 31 bytes for KW43.

  • The scanner may sporadically miss some chained packets.

Periodic Advertising with Responses (PAwR):

  • Periodic Advertising with Response (PAwR) is not supported with the configuration “Subevent Interval = Number of Response Slots x Response Slot Spacing with Response Slot Spacing = 0x2”.

  • The feature is not functional with the Free-Running Oscillator (FRO32K); it requires a 32 KHz Crystal Oscillator with accuracy less than 50 ppm.

KW43:

  • CS testmode does not work.

  • CS works only over 1M ACL connection.

  • CS performances are not yet guaranteed.

KW45 / MCXW 71: No specific issues.

KW47 / MCX W72: Channel Sounding (CS): Information:

  • RF Bandwidth Occupancy and Connections/Channel Sounding Activities: The RF bandwidth occupancy is tightly coupled with configured activities, including the number of connections, connection event durations, the number of Channel Sounding (CS) procedures, and related CS parameters (e.g., subevent length, repeat mode). The Link Layer Scheduler is responsible for allocating RF bandwidth to these activities, optimizing bandwidth utilization. However, because each activity operates on its own timing constraints, some RF collisions are expected. This is inherent to the Bluetooth LE protocol, particularly when peripheral roles are configured, as anchor placement is controlled by the central peer devices. The application controls several timing parameters, such as connection interval and subevent length. To optimize user experience, the Link Layer expects the application to adjust these parameters to achieve the best RF bandwidth occupancy with the lowest occurrence of RF collisions.

Limitations:

  • RTT with Sounding Sequence is not supported.

  • Maximum 6 Channel Sounding procedures are supported in parallel.

  • Phase measurement bias is within certification range (<1.7x2πns) with KW47 EVK board. However, if different PCB or antenna matching is used, some bias may appear due to increased delay.

  • For experimental feature IPT(Inline PCT Transfer), only 1x1 configuration is supported.

Known issues:

  • When CS Subevents are configured very close from each other (<700us), some Subevents may be aborted with reason 0x3.

  • When CS offset is configured too close from ACL anchor point, the anchor point may not be served (TX on central or RX on peripheral will not happen). Ideally, CS Offset should be configured greater than 1ms.

  • RTT bias compensation:

    • For parts not properly configured at production (IFR blank), RTT bias is not compensated properly. Consequently, an inaccuracy of +/-2m can be observed.

  • Pairing procedure fails to complete after connection is established. Affects digital_key sample applications. Increase gHost_TaskStackSize_c to 1900U.

  • Channel Sounding measurement cannot start after handover. Affects digital_key sample applications.

  • For the digital_key_car_anchor_cs and digital_key_device_cs BM applications on KW47EVK and KW47LOC, and the loc_reader BM application on KW47EVK, MCXW72EVK, and FRDMMCXW72, increase stack_size in board_reconfig.cmake from 0x0CE4 to 0x1194 (4500 bytes). This change is required to avoid runtime stack overflow that can lead to a HardFault.

Zigbee#

  • OTA interruption is not resuming correctly (for example, when using a reset in the middle of the transfer).

  • Zigbee ZED RX OFF example application on FreeRTOS fails sometime.

  • Minor fixes and stability improvements for connectivity_test example application.

LIN New Project Wizard (NPW) issue#

  • The lin (LIN Driver) and lin_stack (LIN Stack Driver) drivers components should not be enabled at the same time while creating the new projects in MCUXpresso. Otherwise there will be the compiling issue.

  • The lin_stack (LIN Stack Driver) is not actually a driver. It is an adapt layer for LIN Stack middleware to adapt to the low level lpuart driver and cannot be used in NPW alone. So, select the LIN Stack middleware and then the lin_stack is selected automatically since it is required by LIN Stack middleware. Besides, customer need to add the lin_cfg.c/h in application layer for user definition of frame data and add FSL_SDK_LIN_STACK_ENABLE=1 in MCUXpresso preprocessor, otherwise the compiling of LIN Stack will report error.

Flash ROMAPI#

Note that:

  • If using ROM API for internal flash or SPI NOR operation, reserve RAM location 0x200030A0 - 0x200032CF (0x300030A0 - 0x300032CF).

  • If using kb API, reserve 0x20002000 - 0x200032FF (0x30002000 - 0x300032FF).

Other limitations#

  • The following Connectivity Framework configurations are Experimental and not recommended for mass production:

    • Power down on application power domain.

  • GenFSK Connectivity_test application is not operational with Low Power enabled.

  • Serial manager is only supported on UART (not I2C nor SPI).

  • If the FRO32K is configured as the clock source of the CM33 Core then the debug session will block in IAR CMSIS-DAP while debugging. Use a lower debug wire speed, for example 1 MHz instead of the default one.

    In IAR, the option is in Runtime Checking -> Debugger -> CMSIS DAP -> Interface -> Interface speed.

Examples hello_world_ns, secure_faults_ns, and secure_faults_trdc_ns have incorrect library path in GUI projects#

When the affected examples are generated as GUI projects, the library linking the secure and non-secure worlds has an incorrect path set. This causes linking errors during project compilation.

Examples: hello_world_ns, hello_world_s, secure_faults_ns, secure_faults_s, secure_faults_trdc_ns, secure_faults_trdc_s

Affected toolchains: mdk, iar

Workaround: In the IDE project settings for the non-secure (_ns) project, find the linked library (named hello_world_s_CMSE_lib.o, or similar, depending on the example project) and replace the path to the library with <build_directory>/<secure_world_project_folder>/<IDE>/, replacing the subdirectory names with the build directory, the secure world project name, and IDE name.

Example mbedtls_benchmark may hang on some targets on devices with ELS acceleration#

Some targets of ELS accelerated devices may experience runtime issues when run with the default configuration of the mbedtls_benchmark application.

Examples: mbedtls_benchmark

Affected toolchains: All

The iped example does not complete successfully#

The iped example fails at multiple points.

Examples: iped

Affected toolchains: All

TF-M secure and EL2GO examples incorrect path in “Download extra image” with iar and mdk IDEs with Kex package#

TF-M secure and EL2GO examples are missing the target path for ns binary in “extra download image” with iar and mdk IDEs

Examples: tfm_demo_s, tfm_psatest_s, tfm_regression_s, tfm_secureboot_s, el2go_agent_s, el2go_blob_test_s, el2go_import_blob_s, el2go_mqtt_demo_s Affected toolchains: mdk, iar Affected platforms: mcxn5xxevk, frdmmcxn947, mcxn9xxevk, rdrw612bga, frdmrw612 Workaround: There are two ways 1.) Flash secure and non secure bins via Jlink or SPSDK after the build with IDE and providing with correct paths of secure and non-secure binaries. or 2.) Add {target} debug/release in path of “Download extra image” for iar and for MDK in xxx_flashdownload.ini file.