46 #define MMA8652_COUNTSPERG 8192.0 47 #define MMA8652_ACCEL_FIFO_SIZE 32 111 #if (ACCEL_ODR_HZ <= 1) 113 #elif (ACCEL_ODR_HZ <= 6) 115 #elif (ACCEL_ODR_HZ <= 12) 117 #elif (ACCEL_ODR_HZ <= 50) 119 #elif (ACCEL_ODR_HZ <= 100) 121 #elif (ACCEL_ODR_HZ <= 200) 123 #elif (ACCEL_ODR_HZ <= 400) 142 sfg->Accel.iWhoAmI = reg;
155 sfg->Accel.isEnabled =
true;
165 uint8_t sensor_fifo_count = 1;
176 sensor_fifo_count = I2C_Buffer[0] & 0x3F;
185 MMA8652_DATA_READ[0].
numBytes = 6 * sensor_fifo_count;
189 for (j = 0; j < sensor_fifo_count; j++)
191 sample[
CHX] = (I2C_Buffer[6 * j ] << 8) | I2C_Buffer[6 * j + 1];
192 sample[
CHY] = (I2C_Buffer[6 * j + 2] << 8) | I2C_Buffer[6 * j + 3];
193 sample[
CHZ] = (I2C_Buffer[6 * j + 4] << 8) | I2C_Buffer[6 * j + 5];
218 sfg->Accel.isEnabled =
false;
225 #endif // F_USING_ACCEL The sensor_drv.h file contains sensor state and error definitions.
#define __END_WRITE_DATA__
void * bus_driver
should be of type (ARM_DRIVER_I2C* for I2C-based sensors, ARM_DRIVER_SPI* for SPI) ...
#define CHY
Used to access Y-channel entries in various data data structures.
The mma865x.h contains the MMA865xFC Digital Accelerometer Sensor register definitions, access macros, and device access functions.
int32_t Sensor_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerreadlist_t *pReadList, uint8_t *pOutBuffer)
Read register data from a sensor.
#define ACCEL_FIFO_SIZE
FXOS8700 (accel), MMA8652, FXLS8952 all have 32 element FIFO.
#define __END_READ_DATA__
The top level fusion structure.
int8_t MMA8652_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
#define MMA8652_COUNTSPERG
#define MMA8652_WHOAMI_VALUE
uint16_t addr
I2C address if applicable.
void addToFifo(union FifoSensor *sensor, uint16_t maxFifoSize, int16_t sample[3])
addToFifo is called from within sensor driver read functions
The sensor_fusion.h file implements the top level programming interface.
The FifoSensor union allows us to use common pointers for Accel, Mag & Gyro logical sensor structures...
#define CHZ
Used to access Z-channel entries in various data data structures.
uint16_t isInitialized
Bitfields to indicate sensor is active (use SensorBitFields from build.h)
registerDeviceInfo_t deviceInfo
I2C device context.
Provides function prototypes for driver level interfaces.
int8_t MMA8652_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
#define CHX
Used to access X-channel entries in various data data structures.
void conditionSample(int16_t sample[3])
conditionSample ensures that we never encounter the maximum negative two's complement value for a 16-...
#define MMA8652_ACCEL_FIFO_SIZE
int32_t Register_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
The interface function to read a sensor register.
This structure defines the Write command List.
This structure defines the Read command List.
#define F_USING_ACCEL
nominally 0x0001 if an accelerometer is to be used, 0x0000 otherwise
An instance of PhysicalSensor structure type should be allocated for each physical sensors (combo dev...
int8_t MMA8652_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
The sensor_io_i2c.h file declares low-level interface functions for reading and writing sensor regist...
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor.