![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The mpl3115_normal_interrupt.c file implements the ISSDK MPL3115 sensor driver example demonstration with interrupt mode. More...
#include "board.h"#include "pin_mux.h"#include "clock_config.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "gpio_driver.h"#include "mpl3115_drv.h"
Go to the source code of this file.
Macros | |
| #define | MPL3115_DATA_SIZE (5) /* 3 byte Pressure/Altitude and 2 byte Temperature. */ |
| #define | MPL3115_SAMPLING_EXPONENT (1) /* 2 seconds */ |
Functions | |
| void | mpl3115_int_data_ready_callback (void *pUserData) |
| This is the Sensor Data Ready ISR implementation. More... | |
| int | main (void) |
| This is the The main function implementation. More... | |
Variables | |
| const registerwritelist_t | cMpl3115ConfigNormal [] |
| Register settings for Interrupt (non buffered) mode. More... | |
| const registerreadlist_t | cMpl3115OutputNormal [] |
| Address and size of Raw Pressure+Temperature Data in Normal Mode. More... | |
| volatile uint8_t | gMpl3115DataReady |
The mpl3115_normal_interrupt.c file implements the ISSDK MPL3115 sensor driver example demonstration with interrupt mode.
Definition in file mpl3115_normal_interrupt.c.
Definition at line 64 of file mpl3115_normal_interrupt.c.
Referenced by main().
| #define MPL3115_SAMPLING_EXPONENT (1) /* 2 seconds */ |
In MPL3115 the Auto Acquisition Time Step (ODR) can be set only in powers of 2 (i.e. 2^x, where x is the SAMPLING_EXPONENT). This gives a range of 1 second to 2^15 seconds (9 hours).
Definition at line 68 of file mpl3115_normal_interrupt.c.
| int main | ( | void | ) |
This is the The main function implementation.
This function invokes board initializes routines, then then brings up the sensor and finally enters an endless loop to continuously read available samples.
| [in] | void | This is no input parameter. |
Initialize the MCU hardware.
Initialize MAG3110 pin used by FRDM board
Initialize RGB LED pin used by FRDM board
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize MPL3115 sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the MAG3110 sensor driver.
Clear the data ready flag, it will be set again by the ISR.
Read new raw sensor data from the MPL3115.
Process the sample and convert the raw sensor data to signed 16-bit container.
Definition at line 125 of file mpl3115_normal_interrupt.c.
References ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, Driver_GPIO_KSDK, gMpl3115DataReady, GPIO_DIRECTION_IN, GPIO_DIRECTION_OUT, GREEN_LED, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, int32_t(), MPL3115_DATA_SIZE, MPL3115_I2C_ADDR, MPL3115_I2C_Configure(), MPL3115_I2C_Initialize(), MPL3115_I2C_ReadData(), MPL3115_I2C_SetIdleTask(), MPL3115_INT1, mpl3115_int_data_ready_callback(), MPL3115_PRESSURE_CONV_FACTOR, MPL3115_TEMPERATURE_CONV_FACTOR, MPL3115_WHOAMI_VALUE, pGpioDriver, GENERIC_DRIVER_GPIO::pin_init, mpl3115_pressuredata_t::pressure, rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeWait(), status, mpl3115_pressuredata_t::temperature, and GENERIC_DRIVER_GPIO::toggle_pin.

| void mpl3115_int_data_ready_callback | ( | void * | pUserData | ) |
This is the Sensor Data Ready ISR implementation.
This function sets the flag which indicates if a new sample(s) is available for reading.
| [in] | pUserData | This is a void pointer to the instance of the user specific data structure for the ISR. |
Set flag to indicate Sensor has signalled data ready.
Definition at line 111 of file mpl3115_normal_interrupt.c.
References gMpl3115DataReady.
Referenced by main().

| const registerwritelist_t cMpl3115ConfigNormal[] |
Register settings for Interrupt (non buffered) mode.
Definition at line 74 of file mpl3115_normal_interrupt.c.
| const registerreadlist_t cMpl3115OutputNormal[] |
Address and size of Raw Pressure+Temperature Data in Normal Mode.
Definition at line 92 of file mpl3115_normal_interrupt.c.
| volatile uint8_t gMpl3115DataReady |
Definition at line 98 of file mpl3115_normal_interrupt.c.
Referenced by main(), and mpl3115_int_data_ready_callback().