46 #include "fsl_lptmr.h"    47 #include "clock_config.h"    48 #include "fsl_debug_console.h"    53 #include "Driver_I2C.h"    58 #include "issdk_hal.h"    59 #include "gpio_driver.h"    66 #define mma8491q_en_callback LPTMR0_IRQHandler    68 #define MMA8491Q_T_ODR_ms 100U    70 #define LPTMR_T_CORRECTION_ms 2    89         .interruptMode = kPORT_InterruptOrDMADisabled,
    91         .portPinConfig.mux = kPORT_MuxAsGpio,
   101     uint32_t delay, count, systemCoreClock;
   103     systemCoreClock = CLOCK_GetCoreSysClkFreq();
   105     for(count=0;count<delay;count++)
   114     LPTMR_ClearStatusFlags(LPTMR0, kLPTMR_TimerCompareFlag);
   121     lptmr_config_t lptmrConfig;
   123     LPTMR_GetDefaultConfig(&lptmrConfig);
   124     LPTMR_Init(LPTMR0, &lptmrConfig);
   125     LPTMR_EnableInterrupts(LPTMR0, kLPTMR_TimerInterruptEnable);
   126     EnableIRQ(LPTMR0_IRQn);
   129     LPTMR_SetTimerPeriod(LPTMR0, MSEC_TO_COUNT((samplingInterval-
LPTMR_T_CORRECTION_ms), CLOCK_GetFreq(kCLOCK_LpoClk)));
   150     PRINTF(
"\r\n ISSDK MMA8491Q sensor driver example demonstration with poll mode\r\n");
   163     if (ARM_DRIVER_OK != status)
   165         PRINTF(
"\r\n I2C Initialization Failed\r\n");
   170     status = pI2cDriver->PowerControl(ARM_POWER_FULL);
   171     if (ARM_DRIVER_OK != status)
   173         PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
   178     status = pI2cDriver->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   179     if (ARM_DRIVER_OK != status)
   181         PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
   193         PRINTF(
"\r\n Sensor Initialization Failed\r\n");
   196     PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
   227         if (ARM_DRIVER_OK != status)
   240         rawData.
accel[0] = ((int16_t)data[0] << 8) | (data[1]);
   241         rawData.
accel[0] /= 4;
   242         rawData.
accel[1] = ((int16_t)data[2] << 8) | (data[3]);
   243         rawData.
accel[1] /= 4;
   244         rawData.
accel[2] = ((int16_t)data[4] << 8) | (data[5]);
   245         rawData.
accel[2] /= 4;
   247         PRINTF(
"\r\n Tilt :  X = %d  Y = %d  Z = %d ", rawData.
tilt[0], rawData.
tilt[1], rawData.
tilt[2]);
   248         PRINTF(
"|| Accel : X = %5d  Y = %5d  Z = %5d \r\n", rawData.
accel[0], rawData.
accel[1], rawData.
accel[2]);
 
#define MMA8491Q_STATUS_ZYXDR_MASK
 
gpioConfigKSDK_t gGpioConfigInPins
 
const registerreadlist_t cMma8491qStatus[]
Address of Status Register. 
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
#define BOARD_BootClockRUN
 
#define MMA8491Q_DATA_SIZE
 
uint8_t data[FXLS8962_DATA_SIZE]
 
void(* toggle_pin)(pinID_t aPinId)
 
The GPIO Configuration KSDK. 
 
int32_t MMA8491Q_I2C_ReadData(mma8491q_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
void BOARD_InitDebugConsole(void)
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
#define mma8491q_en_callback
 
const registerreadlist_t cMma8491qOutput[]
Address and size of Raw Acceleration Data. 
 
#define __END_READ_DATA__
 
GENERIC_DRIVER_GPIO * pGpioDriver
 
uint32_t(* read_pin)(pinID_t aPinId)
 
gpioHandleKSDK_t GREEN_LED
 
void mma8491q_timer_fwk_init(uint32_t samplingInterval)
 
int32_t MMA8491Q_I2C_Initialize(mma8491q_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress)
The interface function to initialize the sensor. 
 
#define ASK_USER_TO_RESUME(x)
 
gpio_pin_config_t pinConfig
 
void(* set_pin)(pinID_t aPinId)
 
void(* clr_pin)(pinID_t aPinId)
 
void MMA8491Q_I2C_SetIdleTask(mma8491q_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
This defines the function pointers and sensor specific information. 
 
#define I2C_S_DEVICE_INDEX
 
int main(void)
Main function. 
 
#define LPTMR_T_CORRECTION_ms
 
The mma8491q_drv.h file describes the MMA8491Q driver interface and structures. 
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
#define MMA8491Q_T_ODR_ms
 
Access structure of the GPIO Driver. 
 
fxls8962_acceldataUser_t rawData
 
#define MMA8491Q_T_ON_TYPICAL
 
This structure defines the Read command List. 
 
This structure defines the mma8491q data buffer. 
 
volatile bool bMma849qDataReady
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features. 
 
#define I2C_S_SIGNAL_EVENT