44 #include "clock_config.h" 45 #include "fsl_debug_console.h" 48 #include "Driver_I2C.h" 51 #include "issdk_hal.h" 58 #define MMA865x_ACCEL_DATA_SIZE (6) 83 .bits = {.config = 1},
125 PRINTF(
"\r\n ISSDK Pedometer Example using MMA8652 sensor as the acceleration source\r\n");
129 if (ARM_DRIVER_OK != status)
131 PRINTF(
"\r\n I2C Initialization Failed\r\n");
136 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
137 if (ARM_DRIVER_OK != status)
139 PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
144 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
145 if (ARM_DRIVER_OK != status)
147 PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
156 PRINTF(
"\r\n Sensor Initialization Failed\r\n");
161 PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
171 PRINTF(
"\r\n MMA865x Sensor Configuration Failed, Err = %d\r\n", status);
176 PRINTF(
"\r\n Successfully Applied MMA865x Sensor Configuration\r\n");
196 if (ARM_DRIVER_OK != status)
202 rawData.
accel[0] = ((int16_t)data[0] << 8) | data[1];
203 rawData.
accel[1] = ((int16_t)data[2] << 8) | data[3];
204 rawData.
accel[2] = ((int16_t)data[4] << 8) | data[5];
void pedometer_init(pedometer_t *pPedometer)
The interface function initialize the pedometer.
#define MMA865x_ACCEL_DATA_SIZE
This defines the configuration structure of the pedometer.
#define MMA865x_XYZ_DATA_CFG_FS_MASK
The pedometer.h file contains the interface and structure definitions for pedometer application...
#define __END_WRITE_DATA__
int32_t MMA865x_I2C_Initialize(mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
#define PEDO_FREQHZ_DEFAULT
This structure defines the mma865x raw data buffer.
#define BOARD_BootClockRUN
const registerreadlist_t cMma865xDataReady[]
uint8_t data[FXLS8962_DATA_SIZE]
int32_t MMA865x_I2C_ReadData(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
This defines the acceleration input data for the pedometer.
void BOARD_InitDebugConsole(void)
#define PEDO_STEP_THRESHOLD_DEFAULT
This defines the sensor specific information.
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
#define MMA865x_CTRL_REG1_DR_MASK
#define __END_READ_DATA__
#define MMA865x_CTRL_REG1_DR_50HZ
This defines the pedometer instance.
const registerreadlist_t cMma865xOutputValues[]
void MMA865x_I2C_SetIdleTask(mma865x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
#define MMA8652_WHOAMI_VALUE
#define PEDO_SPEED_PERIOD_DEFAULT
debounce_count_t sleepcount_threshold
int32_t MMA865x_I2C_Configure(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
#define MMA865x_XYZ_DATA_CFG_FS_2G
#define MMA865x_CTRL_REG2_MODS_MASK
void pedometer_configure(pedometer_t *pPedometer, const pedometer_config_t *pConfig)
The interface function to configure the pedometer.
int32_t pedometer_run(pedometer_t *pPedometer, ped_accel_t *pData)
The interface function excutes the pedometer algorithm.
#define MMA865x_STATUS_ZYXDR_MASK
#define I2C_S_DEVICE_INDEX
The mma865x_drv.h file describes the MMA865x driver interface and structures.
struct pedometer_t::pedometer_status_tag status
fxls8962_acceldataUser_t rawData
#define PEDO_FILTER_STEPS_DEFAULT
#define MMA865x_CTRL_REG2_MODS_HR
This structure defines the Write command List.
This structure defines the Read command List.
int main(void)
Main function.
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
#define I2C_S_SIGNAL_EVENT
const registerwritelist_t cMma865xConfigNormal[]
#define PEDO_FILTER_TIME_DEFAULT