![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The mag3110_normal.c file implements the ISSDK MAG3110 sensor driver example demonstration with polling mode. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "mag3110_drv.h"
Go to the source code of this file.
Macros | |
| #define | MAG3110_DATA_SIZE (6) /* 2 byte X,Y,Z Axis Data each. */ |
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | cMag3110ConfigNormal [] |
| Register settings for Normal (non buffered) mode. More... | |
| const registerreadlist_t | cMag3110Status [] = {{.readFrom = MAG3110_DR_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| Address of Status Register. More... | |
| const registerreadlist_t | cMag3110OutputNormal [] |
| Address and size of Raw Pressure+Temperature Data in Normal Mode. More... | |
The mag3110_normal.c file implements the ISSDK MAG3110 sensor driver example demonstration with polling mode.
Definition in file mag3110_normal.c.
| #define MAG3110_DATA_SIZE (6) /* 2 byte X,Y,Z Axis Data each. */ |
Definition at line 37 of file mag3110_normal.c.
Referenced by main().
| int main | ( | void | ) |
Main function.
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize MAG3110 sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the MAG3110 sensor driver.
Wait for data ready from the FXAS21002.
Read the raw sensor data from the FXAS21002.
Process the sample and convert the raw sensor data to signed 16-bit container.
Definition at line 65 of file mag3110_normal.c.
References ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), mag3110_magdata_t::mag, MAG3110_CalibrateHardIronOffset(), MAG3110_DATA_SIZE, MAG3110_DR_STATUS_ZYXDR_MASK, MAG3110_I2C_ADDR, MAG3110_I2C_Configure(), MAG3110_I2C_Initialize(), MAG3110_I2C_ReadData(), MAG3110_I2C_SetIdleTask(), MAG3110_WHOAMI_VALUE, rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), and status.

| const registerwritelist_t cMag3110ConfigNormal[] |
Register settings for Normal (non buffered) mode.
Definition at line 43 of file mag3110_normal.c.
| const registerreadlist_t cMag3110OutputNormal[] |
Address and size of Raw Pressure+Temperature Data in Normal Mode.
Definition at line 56 of file mag3110_normal.c.
| const registerreadlist_t cMag3110Status[] = {{.readFrom = MAG3110_DR_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Address of Status Register.
Definition at line 53 of file mag3110_normal.c.