![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The dp5004_interrupt.c file implements the ISSDK MPXVDP5004 analog sensor driver example demonstration with interrupt mode. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_lptmr.h"#include "fsl_adc12.h"#include "fsl_debug_console.h"#include "issdk_hal.h"#include "gpio_driver.h"
Go to the source code of this file.
Macros | |
| #define | dp5004_odr_callback PWT_LPTMR0_IRQHandler |
| #define | adc12_irq_callback ADC0_IRQHandler |
| #define | MPXV5004DR_ODR_ms 1000U |
Functions | |
| void | dp5004_odr_callback (void) |
| void | adc12_irq_callback (void) |
| void | KE15Z_LPTMR0_ADC0_Initialize (void) |
| int | main (void) |
| Main function. More... | |
Variables | |
| volatile uint32_t | gAdcConversionValue |
| volatile bool | bAdcCompletedFlag = false |
| adc12_channel_config_t | gAdcChannelConfigStruct |
The dp5004_interrupt.c file implements the ISSDK MPXVDP5004 analog sensor driver example demonstration with interrupt mode.
Definition in file dp5004_interrupt.c.
| #define adc12_irq_callback ADC0_IRQHandler |
Definition at line 37 of file dp5004_interrupt.c.
| #define dp5004_odr_callback PWT_LPTMR0_IRQHandler |
Definition at line 35 of file dp5004_interrupt.c.
| #define MPXV5004DR_ODR_ms 1000U |
Definition at line 40 of file dp5004_interrupt.c.
Referenced by KE15Z_LPTMR0_ADC0_Initialize().
| void adc12_irq_callback | ( | void | ) |
Definition at line 61 of file dp5004_interrupt.c.
References bAdcCompletedFlag, gAdcConversionValue, and MPXVDP5004_ADC12_CHANNEL_GROUP.
| void dp5004_odr_callback | ( | void | ) |
Definition at line 53 of file dp5004_interrupt.c.
References gAdcChannelConfigStruct, and MPXVDP5004_ADC12_CHANNEL_GROUP.
| void KE15Z_LPTMR0_ADC0_Initialize | ( | void | ) |
Definition at line 68 of file dp5004_interrupt.c.
References gAdcChannelConfigStruct, MPXV5004DR_ODR_ms, and MPXVDP5004_ADC12_CHANNEL.
Referenced by main().

| int main | ( | void | ) |
Main function.
Initialize GREEN LED pin used by FRDM board
Definition at line 104 of file dp5004_interrupt.c.
References ASK_USER_TO_RESUME, bAdcCompletedFlag, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), Driver_GPIO_KSDK, gAdcConversionValue, GPIO_DIRECTION_OUT, GREEN_LED, KE15Z_LPTMR0_ADC0_Initialize(), MPXV5004DP_PRESSURE_FROM_ADC_VALUE, GENERIC_DRIVER_GPIO::pin_init, SMC, SMC_SetPowerModeWait(), and GENERIC_DRIVER_GPIO::toggle_pin.

| volatile bool bAdcCompletedFlag = false |
Definition at line 46 of file dp5004_interrupt.c.
Referenced by adc12_irq_callback(), and main().
| adc12_channel_config_t gAdcChannelConfigStruct |
Definition at line 47 of file dp5004_interrupt.c.
Referenced by dp5004_odr_callback(), and KE15Z_LPTMR0_ADC0_Initialize().
| volatile uint32_t gAdcConversionValue |
Definition at line 45 of file dp5004_interrupt.c.
Referenced by adc12_irq_callback(), and main().