![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
Provides init() and read() functions for the FXAS21002 gyroscope. More...
#include "board.h"#include "sensor_fusion.h"#include "sensor_drv.h"#include "sensor_io_i2c.h"#include "drivers.h"#include "fxas21002.h"
Go to the source code of this file.
Macros | |
| #define | FXAS21000_STATUS 0x00 |
| #define | FXAS21000_F_STATUS 0x08 |
| #define | FXAS21000_F_SETUP 0x09 |
| #define | FXAS21000_WHO_AM_I 0x0C |
| #define | FXAS21000_CTRL_REG0 0x0D |
| #define | FXAS21000_CTRL_REG1 0x13 |
| #define | FXAS21000_CTRL_REG2 0x14 |
| #define | FXAS21000_WHO_AM_I_VALUE 0xD1 |
| #define | FXAS21000_COUNTSPERDEGPERSEC 20 |
| #define | FXAS21002_COUNTSPERDEGPERSEC 16 |
| #define | FXAS21002_GYRO_FIFO_SIZE 32 |
| FXAX21000, FXAS21002 have 32 element FIFO. More... | |
Provides init() and read() functions for the FXAS21002 gyroscope.
Definition in file driver_FXAS21002.c.
| #define FXAS21000_COUNTSPERDEGPERSEC 20 |
Definition at line 29 of file driver_FXAS21002.c.
| #define FXAS21000_CTRL_REG0 0x0D |
Definition at line 25 of file driver_FXAS21002.c.
| #define FXAS21000_CTRL_REG1 0x13 |
Definition at line 26 of file driver_FXAS21002.c.
| #define FXAS21000_CTRL_REG2 0x14 |
Definition at line 27 of file driver_FXAS21002.c.
| #define FXAS21000_F_SETUP 0x09 |
Definition at line 23 of file driver_FXAS21002.c.
| #define FXAS21000_F_STATUS 0x08 |
Definition at line 22 of file driver_FXAS21002.c.
| #define FXAS21000_STATUS 0x00 |
Definition at line 21 of file driver_FXAS21002.c.
| #define FXAS21000_WHO_AM_I 0x0C |
Definition at line 24 of file driver_FXAS21002.c.
| #define FXAS21000_WHO_AM_I_VALUE 0xD1 |
Definition at line 28 of file driver_FXAS21002.c.
| #define FXAS21002_COUNTSPERDEGPERSEC 16 |
Definition at line 30 of file driver_FXAS21002.c.
| #define FXAS21002_GYRO_FIFO_SIZE 32 |
FXAX21000, FXAS21002 have 32 element FIFO.
Definition at line 32 of file driver_FXAS21002.c.