![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "fsl_irqsteer.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "mpl3115_drv.h"
Go to the source code of this file.
Macros | |
| #define | MPL3115_DATA_SIZE (5) /* 3 byte Pressure/Altitude and 2 byte Temperature. */ |
| #define | MPL3115_SAMPLING_EXPONENT (1) /* 2 seconds */ |
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | cMpl3115ConfigAltitude [] |
| Register settings for Altitude readings in Normal (non buffered) mode. More... | |
| const registerreadlist_t | cMpl3115Status [] = {{.readFrom = MPL3115_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| Address of Status Register. More... | |
| const registerreadlist_t | cMpl3115OutputNormal [] |
| Address and size of Raw Altitude+Temperature Data in Normal Mode. More... | |
Definition at line 33 of file mpl3115_altitude.c.
Referenced by main().
| #define MPL3115_SAMPLING_EXPONENT (1) /* 2 seconds */ |
In MPL3115 the Auto Acquisition Time Step (ODR) can be set only in powers of 2 (i.e. 2^x, where x is the SAMPLING_EXPONENT). This gives a range of 1 second to 2^15 seconds (9 hours).
Definition at line 37 of file mpl3115_altitude.c.
| int main | ( | void | ) |
Main function.
Initialize the MCU hardware.
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize MPL3115 sensor driver.
Configure the MPL3115 sensor.
Wait for data ready from the MPL3115.
Read new raw sensor data from the MPL3115.
Process the sample and convert the raw sensor data.
Definition at line 68 of file mpl3115_altitude.c.
References mpl3115_altitudedata_t::altitude, ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), MPL3115_ALTITUDE_CONV_FACTOR, MPL3115_DATA_SIZE, MPL3115_DR_STATUS_PTDR_MASK, MPL3115_I2C_ADDR, MPL3115_I2C_Configure(), MPL3115_I2C_Initialize(), MPL3115_I2C_ReadData(), MPL3115_TEMPERATURE_CONV_FACTOR, MPL3115_WHOAMI_VALUE, rawData, SENSOR_ERROR_NONE, status, and mpl3115_altitudedata_t::temperature.

| const registerwritelist_t cMpl3115ConfigAltitude[] |
Register settings for Altitude readings in Normal (non buffered) mode.
Definition at line 43 of file mpl3115_altitude.c.
| const registerreadlist_t cMpl3115OutputNormal[] |
Address and size of Raw Altitude+Temperature Data in Normal Mode.
Definition at line 59 of file mpl3115_altitude.c.
| const registerreadlist_t cMpl3115Status[] = {{.readFrom = MPL3115_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Address of Status Register.
Definition at line 56 of file mpl3115_altitude.c.