![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "fsl_irqsteer.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "mpl3115_drv.h"
Go to the source code of this file.
Macros | |
| #define | MPL3115_DATA_SIZE (5) /* 3 byte Pressure/Altitude and 2 byte Temperature. */ |
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | cMpl3115ConfigAltitude [] |
| Register settings for Altitude readings in One-Shot mode. More... | |
| const registerwritelist_t | cMpl3115SetOST [] |
| Register settings for Triggring One-Shot Sampling. More... | |
| const registerreadlist_t | cMpl3115GetOST [] = {{.readFrom = MPL3115_CTRL_REG1, .numBytes = 1}, __END_READ_DATA__} |
| Address of Register containing OST Bit. More... | |
| const registerreadlist_t | cMpl3115OutputNormal [] |
| Address and size of Raw Altitude+Temperature Data. More... | |
Definition at line 33 of file mpl3115_oneshot.c.
Referenced by main().
| int main | ( | void | ) |
Main function.
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize MPL3115 sensor driver.
We do not need to call MPL3115_I2C_Configure() in this case as we are going to read samples on demand. Instead we directly write register settings for One-Shot Mode...
The code contained withing the braces illustrate steps to read one-sample. These can be repated at desired intervals to acquire more samples.
Keep checking the OST FLAG for completion.
Read raw sensor data from the MPL3115.
Process the sample and convert the raw sensor data.
Definition at line 63 of file mpl3115_oneshot.c.
References mpl3115_altitudedata_t::altitude, ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, registerDeviceInfo_t::deviceInstance, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), MPL3115_ALTITUDE_CONV_FACTOR, MPL3115_CTRL_REG1_OST_MASK, MPL3115_DATA_SIZE, MPL3115_I2C_ADDR, MPL3115_I2C_Initialize(), MPL3115_I2C_ReadData(), MPL3115_TEMPERATURE_CONV_FACTOR, MPL3115_WHOAMI_VALUE, mpl3115_i2c_sensorhandle_t::pCommDrv, rawData, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_I2C_Write(), mpl3115_i2c_sensorhandle_t::slaveAddress, status, and mpl3115_altitudedata_t::temperature.

| const registerwritelist_t cMpl3115ConfigAltitude[] |
Register settings for Altitude readings in One-Shot mode.
Definition at line 39 of file mpl3115_oneshot.c.
| const registerreadlist_t cMpl3115GetOST[] = {{.readFrom = MPL3115_CTRL_REG1, .numBytes = 1}, __END_READ_DATA__} |
Address of Register containing OST Bit.
Definition at line 51 of file mpl3115_oneshot.c.
| const registerreadlist_t cMpl3115OutputNormal[] |
Address and size of Raw Altitude+Temperature Data.
Definition at line 54 of file mpl3115_oneshot.c.
| const registerwritelist_t cMpl3115SetOST[] |
Register settings for Triggring One-Shot Sampling.
Definition at line 45 of file mpl3115_oneshot.c.