Peripherals
Peripherals is a generic term referring to both core peripherals, for example the System Timer (SysTick) and SOC/MCU peripherals such as an ADC or UART. In both instances these hardware blocks are exposed within the MCUs address space (known as memory mapped peripherals) and so can be interrogated by accesses to their specific memory locations.
SVD files (provided by an SDK) include knowledge of an MCU’s peripheral set, which is made available via the Peripherals view within the bottom panel, once a debug connection is made.

In this view each peripheral is listed along with its value, base address, access, and a brief description. The view also exposes the inner peripheral registers and offers bit field enumerations to greatly simplify both reading existing configurations and setting new values.
A Refresh button is available in the top right corner for re-reading the memory values from the target.

Note: When an MCU powers up, many peripherals will be unavailable because they are unpowered/not clocked. Attempting to access a peripheral in this state will result in failure, and the peripheral view will simply display “???” as the value.
Warning: It is strongly advised that only peripherals that are well understood are accessed in this manner since attempting to view certain peripherals can break a debug connection or perform other unexpected actions. MCUXpresso for VS Code’s debug features cannot offer protection from such occurrences.
Custom SVD File
MCUXpresso for VS Code tries to automatically detect the appropriate SVD from the information provided in the software repository. The extension can also retrieve the SVD file from the public MCUXpresso SoC SVD repository. In various situations, like initiating a debug session, you might be offered the option to automatically retrieve the SVD file, or to manually browse to a local SVD file. The notification allows ignoring future prompts for specific debug configurations available inside the project. In the screenshot below, you can see the quick pick notification shown once a debug session is initiated when there’s no SVD file already specified inside .vscode/launch.json, and further more, no SVD was identified in the SDK linked to the project being debugged.

Note: If the hardware information (board ID, device ID, core ID) associated to the project can be used to identify a single SVD file, you will not be further asked for any other input. However, if no exact match is identified, you will be required to choose the appropriate file from a list of SVD files available in the remote MCUXpresso SoC SVD repository. Once the SVD is retrieved and configured, this will be reused for subsequent debug sessions.
The path to the SVD can also be manually provided (or override the default SVD) by setting the svdPath property in the launch configuration present in .vscode/launch.json:
"svdPath": "C:/sdks/mcux-sdk/svd/MIMXRT1176/MIMXRT1176_cm7.xml"
The automatically downloaded SVD files are stored inside the project, under the svd folder. When "Don't ask again" is selected in the notification, the current debug configuration is added in the settings to prevent future prompts for that specific debug configuration.
Note: The configuration setting is intended to be used at workspace folder level and can be manually changed via the
Settingspage inside VS Code.