MCUXpresso Installer troubleshooting
The MCUXpresso Installer troubleshooting guide is designed to help users quickly identify and resolve common issues encountered during the installation of development software tools dependencies.
Table of Contents
Python Virtual Environment
Issues can be encountered during the creation, updating, activation, or usage of the Python virtual environment.
Common causes
Corrupted Python installation
Corrupted virtual environment
The existing virtual environment is tied to a missing Python installation
Recommended solutions
1. If the virtual environment does not exist
Make sure that the correct version of Python is installed and functional under
%USERPROFILE% (or $HOME on Unix systems)/.mcuxpressotools/python-<version>.Retry the creation of the virtual environment using the MCUXpresso Installer:
Open MCUXpresso Installer.
Perform a check for newer versions of components.
Install the Python environment for the desired package.
2. If the virtual environment exists
Remove the existing virtual environment from
%USERPROFILE%(or $HOME on Unix systems)/.mcuxpressotools/.venv.Retry the creation of the virtual environment using the MCUXpresso Installer.
Open MCUXpresso Installer.
Perform a check for newer versions of components.
Install the Python environment for the desired package.
Wget utility
Issues regarding the installation of Wget can occur on systems where network connectivity is restricted or proxy configurations are modified.
Common causes
Incomplete or misconfigured network settings
Proxy server restrictions
Firewall blocking download connections
Invalid or outdated SSL/TLS certificates
Recommended solution
Manual wget download and configuration
Download Wget from an official mirror site
Add Wget to the PATH environment variable
Verify the installation by running
wget --versionin a new instance of the command prompt or terminalTo ensure that the new configuration takes effect, you have to restart the MCUXpresso Installer application
Windows Developer Mode
Some development tools require Windows Developer Mode to be enabled for proper functionality, particularly for debugging and development features.
Recommended solutions
1. Enable Developer Mode through Settings
Steps:
Open Settings (Windows key + I)
Navigate to System → For developers (Windows 11) or Update & Security → For developers (Windows 10)
Select Developer mode
Click Yes when prompted to confirm the change
Restart your computer if prompted
2. Enable Developer Mode through Registry (if the Settings method fails)
Steps:
Press Windows key + R and type
regeditNavigate to
HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\AppModelUnlockCreate a DWORD (32-bit) Value named
AllowDevelopmentWithoutDevLicenseSet the value to 1
Restart your computer
3. Verify that Developer Mode is enabled
Steps:
Open Command Prompt as administrator
Run the command:
reg query "HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\AppModelUnlock" /v AllowDevelopmentWithoutDevLicenseVerify that the value is set to 0x1